This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0340: 图像输出挑显示器

Part Number: LMH0340

SDI接口输出图像,使用SDI串行器为LMH0340;

发现接不同品牌的显示器,有的成像,有的不成像;

经过测试发现:显示器接入端的输入接口对地阻值为高阻的可以成像;

显示器接入端的输入接口对地阻值为75欧姆的不成像;

如何解决这个问题,谢谢!

  • LMH0340驱动电路完成按照规格书推荐电路设计,几个项目都有同样的问题,是这个片子对接收端有要求不?

  • 显示器的输入引脚对地阻值只有75ohm吗?有没有这个显示器的spec,附上我这边看下。

  • 已经确认接收端使用的是semtech GS2971A, 参考这个片子spec,接收端的电路如下图所示。这个接收芯片与LMH0340是不是不匹配,还是有其他方式可以解决?

  • 您好,关于GS2971A不能正常显示的问题,我这边需要去确认一下。

  • 好的,感谢,有相关结论还麻烦回复下,谢谢!

  • 您好,下面这是美国工程师的回复:

    We cannot comment or do not know why Semtech GS2971A cannot display the image.

    LMH0340 is a serializer and it is being driven by the FPGA. So the SDI image framing actually gets generated by the FPGA. As long as the FPGA can support this video monitor, LMH0340 should be able able to display the image. LMH0340 performs serialization and FPGA does all the SDI video image framing and support for different monitors

    我们无法评论或不知道 Semtech GS2971A 为何无法显示图像。 LMH0340是一款串行器, 是由 FPGA 驱动。 因此、SDI 图像组帧实际上由 FPGA 生成。 只要 FPGA 能够支持该视频监控器、LMH0340就应该能够显示图像。 LMH0340执行串行化、FPGA 执行所有 SDI 视频图像组帧并支持不同的显示器。