Other Parts Discussed in Thread: LMH0030, LMH0031
Hi TI teams:
I'm surverying a SDI output solution, and found LMH0340 might suit for our usage. But I need to confirm with you about the requirement of input LVDS frequncy(data rate) first.
The colock frequency of slected LVDS transistor can support up to 80~157MHz(Another one can reach to 105MHz), can it transmit 1080p@60Hz (3G) signal as input to LMH0340?
You can refer to the detail desctiption in the following links.
Conditions:
Max. resolution: 1920*1080@60Hz
Color depth: 10-bit
Thanks for the support and wait for your reply.