Request a Solution: Eliminating Bounce When Using SN74LVC1G125DBVR to Drive a Rotary Encoder
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simpli… |
The period of the waveform output at the DQ signal terminal is not 16 times that of the CLKO terminal.The RC parameters are as follows:R1=56KΩ,R2=240KΩ,C=3400pF.The supply voltage is 5.3V.
我需要做如此应用,实现一个单线总线的1.2V--1.8V双向电平转换。
单线总线:
1.只有1根信号线
2.master和slave都只有驱动高的能力
仅靠下拉电阻输出低电平
3.下拉电阻<=10KΩ
4.频率<=1MHz
总线3个状态:
1. master输出,slave输入,总线高电平
2. master输入,slave输出,总线高电平
3. master输入,slave输入,总线依靠下拉电阻拉到低…
我有一个线路需要用同样大管脚,实现SPI和IIC通讯,我是否可以用他来实现(SPI 模式下不上拉, IIC模式下通过两边上拉实现),如果说有问题,是否有其他型号替换? 例如TXS01XX, 另外如果用TXS01系列是不是在IIC通讯的时候也要两边上拉,如果可以,上拉电阻多大合适?请帮忙
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
您好:
我打算选用SN74AHC1G08该与门芯片。看到它最小工作电压为2V,但电源上电会有上升时间,不会一下子到2V。
我的问题是,2V之前,它的逻辑输出默认是高压还是低呢?这在我的应用中非常重要,我希望是低。
非常感谢!
hello!
I have purchased the model TXS0108ENMER of your company.
When I measured the volume, I found that the thickness was not consistent with the PDF. I also found that the thickness was not consistent with the PDF when I bought…
OAM小板SN74AXC4T774RSVR布板在连接器旁边,需要评估应力变形对IC的影响。
请帮忙确认以下两个问题:
1. SN74AXC4T774RSVR UQFN16封装的Die占整个IC封装面积的比例是多少。
2. 是否有IC应力测试报告,IC是否可以耐受450微应变。
谢谢!