• TXB0108: drive relay

    Part Number: TXB0108
    Other Parts Discussed in Thread: LSF0108

    Dear teams,

    I used TXB0108 drive relay,the circuit diagram is as follows:

    I cannot drive the relay in actual use, and I feel that the driving ability is insufficient.

    I was able to drive relays…

  • LSF0108-Q1: 1.8V转3.3V失败--Description Failed to convert 1.8V to 3.3V

    Part Number: LSF0108-Q1
    Other Parts Discussed in Thread: LSF0108

    如题,下图为我的电路设计图。我想使用LSF0108进行1.8v(a侧)到3.3v(b侧)的转换,但当我使用示波器测量时,b侧电压仍保持1.8v。请大家帮我看看电路或者器件使用有什么问题吗?

    As the subject, the following is my circuit design drawing. I wanted to convert 1.8v (A side…

  • LSF0108: 求助LSF0108输出无法到0V

    Part Number: LSF0108

    使用推荐电路,Vref_B和EN通过200K链接到5V,B输出口上拉5V,但是当控制输出低是,输出有1.3V

  • LSF0108: 双向通信,速率提高到50MHz时出现写入数据和读取数据不一致的问题

    Part Number: LSF0108
    Other Parts Discussed in Thread: TXB0304

           hi 你好,使用LSF0108进行1.2V和3.3V电平信号转换,用于QSPI信号双向通信,目标速率是50MHz,但当速率提高到50MHz会出现写入数据和读取数据不一致的问题,目前实测最大速率只能支持到33.33MHz时数据和读取数据是一致的,参考电路图如下,实测时A侧的上拉是去掉的,为了增大驱动能力B侧的上拉换成了330Ω,还请看下什么原因导致的速率提高到50MHz时出现写入数据和读取数据不一致…

  • LSF0108: 请问LSF系列电平转换芯片是否能支持推挽的自动双向转换应用?例如3WIRE的SPI。

    Part Number: LSF0108

    如果可以的话,原理图需要如何连接?

  • TXS0108E: TXS0108的VCCA端口输出电压是否支持1.2V。

    Part Number: TXS0108E
    Other Parts Discussed in Thread: TXB0108, LSF0108, TXB0304, TXB0302

    TXS0108在Datasheet中描述VCCA的Input Power最小为1.4V,在TXS0108的ibis模型中有VCCA为1.2V的模型,请问VCCA是否支持1.2V?

  • LSF0108: about convert the LSF0108's IBIS model to pspice model

    Part Number: LSF0108

     i convert the LSF0108's IBIS model to pspice model,found that LSF0108's each pin is one single component,makes me can't use it to draw schematic,and run function simulate.how can i solve it?

  • LSF0108: uart信号波形异常

    Part Number: LSF0108

    Hi,team

    我们在调试LSF0108的时候遇到了一个问题。原理图如图所示。

    UART1是主板传输过来的串口信号,1.8V电平,位于左边的A端口。希望转换为3.3V后从B端口输出。下图是U10没有上电,在A端口测出的UART1原始波形——

    下图是U10上电后,在A端口测出的UART1波形——

    可以发现,U10没有上电时,UART原始波形是正常的,但U10上电后,低电平就拉不下来了,按道理低电平应该…

  • LSF0108: 硬件设计问题咨询

    Part Number: LSF0108

    The LSF0108 automatic bidirectional level conversion IC is used in the new project , and I would like to ask about its design. The circuit is shown in the figure.

    Question 1: Handling of EN pins

    Now it is the combination of EN and…

  • LSF0108: 芯片内部工作原理

    Part Number: LSF0108

    在application report中看到LSF010x的基本框图,但是框图中没有标明MOSFET的源极和漏极,请问和vrefA相连的是源极还是漏极?VBPU是起到什么作用?芯片是如何通过两个MOSFET实现了自动双向电压转换?

  • LSF0108: 使用LSF0108 在50MHz频率下波形失真较大

    Part Number: LSF0108

    LSF0108RKSR做信号的电平转换器,效果不太理想,在50MHz频率下波形失真较大. 请问有解决方案吗?或者是有其他型号推荐!!

    要求:

    1.时钟频率最高达208MHz

    2.支持1.8V3.3V电平转换,双向数据传输

  • LSF0108: 3.3V/5V电平转换,3.3V被拉高至3.9V

    Part Number: LSF0108

    搭建了一个5V和3.3V的双向电平转换电路,如图显示,调试过程中发现3.3V被拉高到3.9V,断开EN控制脚后,电压恢复正常的3.3V,5V供电电压正常,请问问题出在哪里?