请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TMS320F28335 尊敬的 TI 团队:
有两个 ADC 功率为28335、3.3V 和1.8V。 如何知道哪些 ADC 为3.3V、哪些是1.8V?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的 TI 团队:
有两个 ADC 功率为28335、3.3V 和1.8V。 如何知道哪些 ADC 为3.3V、哪些是1.8V?
谢谢!