This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
我正尝试使用手册《C2000 微控制器串行闪存编程》(SPRABV4F–2021年10月–2023年7月修订)通过串行方式向 TMS320微控制器发送固件。 当我使用闪烁示例使过程一切正常时、但当我尝试使用我的代码执行此操作时、我会得到" 不正确的数据缓冲区长度 " 在执行 DFU CPU1 [1]操作后出现错误。
我注意到十六进制(ASCII)文件格式似乎错误。 我正在使用手册中编写的命令:
serial_flash_programr.exe -d f2837xD -k F2837xD_sci_flash_kernels_cpu01.txt -a output_of_my_program.txt -p COM7 -v
运行命令后内核正确加载
在此之后、我选择选项1 (DFU CPU1)并且会显示此错误(0x122 -不正确的数据缓冲区长度)
这是2837x_FLASH_Ink _CPU1.cmd 文件
MEMORY { PAGE 0 : /* Program Memory */ /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */ RAMM0 : origin = 0x000122, length = 0x0002DE RAMD0 : origin = 0x00B000, length = 0x000800 RAMLS0 : origin = 0x008000, length = 0x000800 RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS3 : origin = 0x009800, length = 0x000800 RAMLS4 : origin = 0x00A000, length = 0x000800 RESET : origin = 0x3FFFC0, length = 0x000002 #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 20012000 GROUP { /* GROUP memory ranges for crc/checksum of entire flash */ #endif #endif /* BEGIN is used for the "boot to Flash" bootloader mode */ BEGIN : origin = 0x080000, length = 0x000002 /* Flash sectors */ FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */ FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */ FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */ FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */ FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */ FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */ FLASHG : origin = 0x098000, length = 0x007FF0 /* on-chip Flash */ FLASHG_DO_NOT_USE : origin = 0x09FFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 20012000 } crc(_ccs_flash_checksum, algorithm=C28_CHECKSUM_16) #endif #endif PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */ BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ RAMD1 : origin = 0x00B800, length = 0x000800 RAMLS5 : origin = 0x00A800, length = 0x000800 RAMGS0 : origin = 0x00C000, length = 0x001000 RAMGS1 : origin = 0x00D000, length = 0x001000 RAMGS2 : origin = 0x00E000, length = 0x004000 /* RAMGS3 : origin = 0x00F000, length = 0x001000 RAMGS4 : origin = 0x010000, length = 0x001000 RAMGS5 : origin = 0x011000, length = 0x001000*/ RAMGS6 : origin = 0x012000, length = 0x001000 RAMGS7 : origin = 0x013000, length = 0x001000 RAMGS8 : origin = 0x014000, length = 0x001000 RAMGS9 : origin = 0x015000, length = 0x001000 RAMGS10 : origin = 0x016000, length = 0x001000 RAMGS11 : origin = 0x017000, length = 0x001000 CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400 CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400 } SECTIONS { /* Allocate program areas: */ .cinit : > FLASHB PAGE = 0, ALIGN(4) .pinit : > FLASHB, PAGE = 0, ALIGN(4) .text : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0, ALIGN(4) codestart : > BEGIN PAGE = 0, ALIGN(4) ramfuncs : > RAMM0, PAGE = 0 #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 15009000 .TI.ramfunc : {} LOAD = FLASHD, RUN = RAMLS0 | RAMLS1 | RAMLS2 ,//|RAMLS3, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(4) #else ramfuncs : LOAD = FLASHD, RUN = RAMLS0 | RAMLS1 | RAMLS2,// |RAMLS3, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(4) #endif #endif /* Allocate uninitalized data sections: */ .stack : > RAMM1 PAGE = 1 //.ebss : >> RAMLS4 | RAMGS0 | RAMGS1 PAGE = 1 //.esysmem : > RAMLS4 PAGE = 1 //modificacao // .ebss : >> RAMGS3, PAGE = 1 //.ebss : >> RAMGS0 | RAMGS1 | RAMGS2, PAGE = 1 .ebss : >> RAMGS2 , PAGE = 1 // .ebss : >> RAMLS5 | RAMGS0 | RAMGS1, PAGE = 1 .esysmem : > RAMLS5 PAGE = 1 /* Initalized sections go in Flash */ .econst : >> FLASHF | FLASHG PAGE = 0, ALIGN(4) .switch : > FLASHB PAGE = 0, ALIGN(4) .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ Filter_RegsFile : > RAMGS0, PAGE = 1 SHARERAMGS0 : > RAMGS0, PAGE = 1 SHARERAMGS1 : > RAMGS1, PAGE = 1 /* The following section definitions are required when using the IPC API Drivers */ GROUP : > CPU1TOCPU2RAM, PAGE = 1 { PUTBUFFER PUTWRITEIDX GETREADIDX } GROUP : > CPU2TOCPU1RAM, PAGE = 1 { GETBUFFER : TYPE = DSECT GETWRITEIDX : TYPE = DSECT PUTREADIDX : TYPE = DSECT } /* crc/checksum section configured as COPY section to avoid including in executable */ .TI.memcrc : type = COPY } /* //=========================================================================== // End of file. //=========================================================================== */
有些人能帮忙吗?
谢谢!!
Leonardo、
您能否将链接器文件中的参数更改为"align 指令"、并再次尝试加载?
我想知道引导加载程序需要的是128位对齐的地址还是64位对齐的地址。 将所有 Align 参数更改为8将解决此问题。
如果您的反馈有所帮助、我们将寻找您的反馈。
此致!
马修