工具/软件:
您好、
我在电路中使用 TPS563300 降压 IC、
观察到开关频率降至接近 27~35kHz。 但需要增加到 500kHz 以减少推理。
我们强烈建议提高开关频率的方法。
输入电压:12V
Vo:3.3V
电感器:33uH
最大负载:200mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.