请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS62867 你(们)好
TPS62867的 VIN 下降压摆率低于 Vulvo、有特别的建议。 如红色框。 -10mV/us、转换为-10000V/s、斜率非常陡。

(1)在这里、最小值为-10mV/us、这是否意味着电源以低于-10mV/us 的斜率关闭?
(2)如果不符合规格、会发生什么情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.