请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ24650 您好!
我想知道、即使电池电压低于1.5V、充电也能正常工作吗?
根据电池检测时序,如果电池电压过低(VLOWV 为1.55V),如果电池电压低至3V,
VFB 将低于1.55V。
电源接通时、电池是否可以进入预充电模式?
感谢你的帮助。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.