This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

280049c CLA影响PWM中断运行



我使用了一个pwm中断,用pwm2触发,不触发cla时运行时间为400ns,触发cla后pwm中断运行时间是13us,感觉是cla影响了pwm中断。pwm中断配置如下:

        EALLOW;
        EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;
        EPwm2Regs.ETSEL.bit.INTEN  = 1;               
        EPwm2Regs.ETPS.bit.INTPRD  = 1;           
        EDIS;

    EALLOW;  //
    PieVectTable.EPWM2_INT=&EPWM1ISR;
    EDIS;
    IER |= M_INT3; // Enable CPU Interrupt 3
    PieCtrlRegs.PIEACK.bit.ACK3   = 1;
    PieCtrlRegs.PIEIER3.bit.INTx2 = 1;  
cla配置如下:
void CLA_configClaMemory(void)
{
    #define _FLASH
    extern uint32_t Cla1ProgRunStart, Cla1ProgLoadStart, Cla1ProgLoadSize,Cla1ProgLoadEnd;
    EALLOW;
#ifdef _FLASH
    //
    // Copy over code from FLASH to RAM
    //
//    MemCopy(&Cla1ProgLoadStart, &Cla1ProgLoadEnd, &Cla1ProgRunStart);
//        asm("   RPT #3 || NOP");
    memcpy((uint32_t *)&Cla1ProgRunStart, (uint32_t *)&Cla1ProgLoadStart,
            (uint32_t)&Cla1ProgLoadSize);
#endif //_FLASH
    //
    // Initialize and wait for CLA1ToCPUMsgRAM
    //
    MemCfgRegs.MSGxINIT.bit.INIT_CLA1TOCPU = 1;
    while(MemCfgRegs.MSGxINITDONE.bit.INITDONE_CLA1TOCPU != 1){};
    //
    // Initialize and wait for CPUToCLA1MsgRAM
    //
    MemCfgRegs.MSGxINIT.bit.INIT_CPUTOCLA1 = 1;
    while(MemCfgRegs.MSGxINITDONE.bit.INITDONE_CPUTOCLA1 != 1){};
    //
    // Select LS4RAM and LS5RAM to be the programming space for the CLA
    // First configure the CLA to be the master for LS4 and LS5 and then
    // set the space to be a program block
    //
    MemCfgRegs.LSxMSEL.bit.MSEL_LS0 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS0 = 1;
    MemCfgRegs.LSxMSEL.bit.MSEL_LS1 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS1 = 0;
    EDIS;
}
//
// CLA_initCpu1Cla1 - Initialize CLA1 task vectors and end of task interrupts
//
void CLA_initCpu1Cla1(void)
{
    //
    // Compute all CLA task vectors
    // On Type-1 CLAs the MVECT registers accept full 16-bit task addresses as
    // opposed to offsets used on older Type-0 CLAs
    //
    EALLOW;
    Cla1Regs.MVECT1 = (uint16_t)(&Cla1Task1);
    Cla1Regs.MVECT2 = (uint16_t)(&Cla1Task2);
    Cla1Regs.MVECT3 = (uint16_t)(&Cla1Task3);
    Cla1Regs.MVECT4 = (uint16_t)(&Cla1Task4);
    Cla1Regs.MVECT5 = (uint16_t)(&Cla1Task5);
    Cla1Regs.MVECT6 = (uint16_t)(&Cla1Task6);
    Cla1Regs.MVECT7 = (uint16_t)(&Cla1Task7);
    Cla1Regs.MVECT8 = (uint16_t)(&Cla1Task8);
    //
    // Enable the IACK instruction to start a task on CLA in software
    // for all  8 CLA tasks. Also, globally enable all 8 tasks (or a
    // subset of tasks) by writing to their respective bits in the
    // MIER register
//    EALLOW;
    Cla1Regs.MCTL.bit.IACKE = 1;
    Cla1Regs.MIER.all = (M_INT8 | M_INT1);
    //
    DmaClaSrcSelRegs.CLA1TASKSRCSEL1.bit.TASK1 = CLA_TRIG_EPWM3INT;
}
请问是哪里出了问题,导致cla影响了pwm中断的正常运行??非常感谢!!
  • 所以您现在是EPWM3触发CLA task? PieVectTable.EPWM2_INT=&EPWM1ISR;

    您的EPWM3是如何配置的呢?能否简要说一下您的程序?
  • 您好,我用EPWM3触发cla task1,软件强制触发task8一次。关于cla的配置如下:
    Cla1ForceTask8();
    EPwm3Regs.ETSEL.bit.INTSEL = ET_CTR_PRD; // Select INT on Zero event
    EPwm3Regs.ETSEL.bit.INTEN = 1; // 使能Enable INT,外设级中断允许
    EPwm3Regs.ETPS.bit.INTPRD = 1;//ET_1ST; // Generate INT on 1rd event

    void CLA_configClaMemory(void)
    {
    #define _FLASH

    // extern uint32_t Cla1ProgRunStart, Cla1ProgLoadStart, Cla1ProgLoadSize,Cla1ProgLoadEnd;

    EALLOW;
    #ifdef _FLASH
    //
    // Copy over code from FLASH to RAM
    //
    // MemCopy(&Cla1ProgLoadStart, &Cla1ProgLoadEnd, &Cla1ProgRunStart);
    // asm(" RPT #3 || NOP");
    memcpy((uint32_t *)&Cla1ProgRunStart, (uint32_t *)&Cla1ProgLoadStart,
    (uint32_t)&Cla1ProgLoadSize);
    #endif //_FLASH

    //
    // Initialize and wait for CLA1ToCPUMsgRAM
    //
    MemCfgRegs.MSGxINIT.bit.INIT_CLA1TOCPU = 1;
    while(MemCfgRegs.MSGxINITDONE.bit.INITDONE_CLA1TOCPU != 1){};

    //
    // Initialize and wait for CPUToCLA1MsgRAM
    //
    MemCfgRegs.MSGxINIT.bit.INIT_CPUTOCLA1 = 1;
    while(MemCfgRegs.MSGxINITDONE.bit.INITDONE_CPUTOCLA1 != 1){};

    //
    // Select LS4RAM and LS5RAM to be the programming space for the CLA
    // First configure the CLA to be the master for LS4 and LS5 and then
    // set the space to be a program block
    //
    MemCfgRegs.LSxMSEL.bit.MSEL_LS0 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS0 = 1;
    MemCfgRegs.LSxMSEL.bit.MSEL_LS1 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS1 = 0;

    EDIS;
    }

    //
    // CLA_initCpu1Cla1 - Initialize CLA1 task vectors and end of task interrupts
    //
    void CLA_initCpu1Cla1(void)
    {
    extern Uint16 Cla1Prog_Start;
    //
    // Compute all CLA task vectors
    // On Type-1 CLAs the MVECT registers accept full 16-bit task addresses as
    // opposed to offsets used on older Type-0 CLAs
    //
    EALLOW;
    Cla1Regs.MVECT1 = (uint16_t)(&Cla1Task1);
    Cla1Regs.MVECT2 = (uint16_t)(&Cla1Task2);
    Cla1Regs.MVECT3 = (uint16_t)(&Cla1Task3);
    Cla1Regs.MVECT4 = (uint16_t)(&Cla1Task4);
    Cla1Regs.MVECT5 = (uint16_t)(&Cla1Task5);
    Cla1Regs.MVECT6 = (uint16_t)(&Cla1Task6);
    Cla1Regs.MVECT7 = (uint16_t)(&Cla1Task7);
    Cla1Regs.MVECT8 = (uint16_t)(&Cla1Task8);


    // Enable the IACK instruction to start a task on CLA in software
    // for all 8 CLA tasks. Also, globally enable all 8 tasks (or a
    // subset of tasks) by writing to their respective bits in the
    // MIER register
    // EALLOW;
    Cla1Regs.MCTL.bit.IACKE = 1;
    Cla1Regs.MIER.all = (M_INT8 | M_INT1);

    //
    DmaClaSrcSelRegs.CLA1TASKSRCSEL1.bit.TASK1 = CLA_TRIG_EPWM3INT;
    EDIS;

    }
  • 我用EPWM2触发PWM中断EPWM1_ISR,具体配置如下:
    EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;
    EPwm2Regs.ETSEL.bit.INTEN = 1;
    EPwm2Regs.ETPS.bit.INTPRD = 1;

    EALLOW; //
    PieVectTable.EPWM2_INT=&EPWM1ISR;
    EDIS;

    IER |= M_INT3; // Enable CPU Interrupt 3
    PieCtrlRegs.PIEACK.bit.ACK3 = 1;
    PieCtrlRegs.PIEIER3.bit.INTx2 = 1;
  • 不触发PWM中断时,EPWM3触发cla单独运行正常;不触发cla,EPWM2触发PWM中断单独运行正常,运行时间为400ns。同时用EPWM3触发cla、EPWM2触发PWM中断,PWM中断运行时间为13us。
  • 请问可以公开解决方案吗?
  • 你好,请问如何解决的呢?我的配置类似于楼主,我是测试PWM中断次数及CLA运行次数,CLA的运行次数不对。另外请问.cla文件中能清除触发中断标志吗?比如我是EPWM1触发的CLA, EPwm1Regs.ETCLR.bit.INT =1;
    谢谢