This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位好:
我在運行手把手教你學DSP的例程PWM,出現警告
This project was created using a version of compiler that is not currently installed: 5.2.3 [C2000]. Another version of the compiler will be used during build: 6.4.6. Please go to <a href="liveaction:OpenAppCenter">CCS App Center</a> to install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties.
這個警告我去查詢過往詢問過的問題都無法解決
compiler5.2.3在舊提問中下載都已失效
請各位幫忙,先謝謝大家回覆
请不要勾选下面的2项
编译器的选择安装的话,请参考文档
http://software-dl.ti.com/ccs/esd/documents/ccs_compiler-installation-selection.html
我用的ccs版本 Version: 6.1.1.00022
我之前的截图就是使用CCS 6.2和 CCS10,理论上都是包含的。若是可以的话,您可以尝试更新CCS版本
Code Generation Tools Updates - http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/codegen/Updates/p2win32/
您不要选择help,而需要选下面的
您好,我去嘗試編譯是可以成功的,但是請注意他有三角形的黃色警告,
This project was created using a version of compiler that is not currently installed: 5.2.3 [C2000]. Another version of the compiler will be used during build: 6.4.6. Please go to <a href="liveaction:OpenAppCenter">CCS App Center</a> to install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties.
我認為會導致我連接F28335時,板子亮紅燈LD2