This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
新手一枚,想请大神看一下我的adc采样配置有没有问题。代码已上传:
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File // Prototype statements for functions found within this file. __interrupt void adc_isr(void); void Adc_Config(void); // Global variables used in this example: Uint16 LoopCount; Uint16 ConversionCount; Uint16 Voltage1[10]; Uint16 Voltage2[10]; Uint16 Voltage3[10]; Uint16 Voltage4[10]; main() { // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2803x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initialize GPIO: // This example function is found in the DSP2803x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2803x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2803x_DefaultIsr.c. // This function is found in DSP2803x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected register PieVectTable.ADCINT1 = &adc_isr; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize all the Device Peripherals: // This function is found in DSP2803x_InitPeripherals.c // InitPeripherals(); // Not required for this example InitAdc(); // For this example, init the ADC // Step 5. User specific code, enable interrupts: // Enable ADCINT1 in PIE PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable INT 1.1 in the PIE IER |= M_INT1; // Enable CPU Interrupt 1 EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM LoopCount = 0; ConversionCount = 0; // Configure ADC // Note: Channel ADCINA4 will be double sampled to workaround the ADC 1st sample issue for rev0 silicon errata EALLOW; AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //ADCINT1 trips after AdcResults latch AdcRegs.INTSEL1N2.bit.INT1E = 1; //Enabled ADCINT1 AdcRegs.INTSEL1N2.bit.INT1CONT = 0; //Disable ADCINT1 Continuous mode AdcRegs.INTSEL1N2.bit.INT1SEL = 2; //setup EOC2 to trigger ADCINT1 to fire AdcRegs.ADCSOC0CTL.bit.CHSEL = 1; //set SOC0 channel select to ADCINA1(dummy sample for rev0 errata workaround) AdcRegs.ADCSOC1CTL.bit.CHSEL = 1; //set SOC1 channel select to ADCINA1 AdcRegs.ADCSOC2CTL.bit.CHSEL = 2; //set SOC2 channel select to ADCINA2 AdcRegs.ADCSOC3CTL.bit.CHSEL = 4; //set SOC3 channel select to ADCINA4 AdcRegs.ADCSOC4CTL.bit.CHSEL = 6; //set SOC4 channel select to ADCINA6 AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 9; //set SOC0 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2 AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 9; //set SOC1 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2 AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 9; //set SOC2 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2 AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 9; //set SOC1 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2 AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 9; //set SOC2 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2 AdcRegs.ADCSOC0CTL.bit.ACQPS = 9; //set SOC0 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1) AdcRegs.ADCSOC1CTL.bit.ACQPS = 9; //set SOC1 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1) AdcRegs.ADCSOC2CTL.bit.ACQPS = 9; //set SOC2 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1) AdcRegs.ADCSOC3CTL.bit.ACQPS = 9; //set SOC1 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1) AdcRegs.ADCSOC4CTL.bit.ACQPS = 9; //set SOC2 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1) EDIS; // Assumes EPwm3 clock is already enabled in InitSysCtrl(); EPwm3Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group EPwm3Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount EPwm3Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event EPwm3Regs.CMPA.half.CMPA = 0x0080; // Set compare A value EPwm3Regs.TBPRD = 0xFFFF; // Set period for EPwm3 EPwm3Regs.TBCTL.bit.CTRMODE = 0; // count up and start // Wait for ADC interrupt for(;;) { LoopCount++; } } __interrupt void adc_isr(void) { Voltage1[ConversionCount] = AdcResult.ADCRESULT1; //discard ADCRESULT0 as part of the workaround to the 1st sample errata for rev0 Voltage2[ConversionCount] = AdcResult.ADCRESULT2; Voltage3[ConversionCount] = AdcResult.ADCRESULT3; Voltage4[ConversionCount] = AdcResult.ADCRESULT4; // If 20 conversions have been logged, start over if(ConversionCount == 9) { ConversionCount = 0; } else ConversionCount++; AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //Clear ADCINT1 flag reinitialize for next SOC PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE return; }
其中关于adc的设置有疑问的点在于:
下面附上程序刷进F28035后,调试时voltage1至voltag4的采样截图和Expressions截图:
voltage1:
voltage2:
voltage3:
voltage4:
Expressions:
问题是:
1.我的adc配置是否有问题。
2.为什么voltage1和voltage2的数值分别在25和17上下浮动,而voltage3和voltage4的数值分别在1255和1830上下浮动。
3.为什么每组adc采样的voltage数值浮动范围都不一样,到底voltage的数值应该是多少。
程序是官方例程改的,只是我模仿voltage1和voltage2的配置加了voltage3和voltage4。另外还想问一下触发源的选择,代码是:
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 9;
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 9;
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 9;
AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 9;
AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 9;
9是代表epwm3,是所有的soc都可以集中到epwm3的trigger上吗,还是说epwm3的trigger接收数量是有一个上限的呢,求解答,谢谢。
这几行代码里的ADCRESULT1至ADCRESULT4的数字1至4是怎么来的
参照下图:
程序是官方例程改的,只是我模仿voltage1和voltage2的配置加了voltage3和voltage4
使用的哪个例程以及改动的位置具体是哪里?
建议参考下user guide ADC相关章节,你的大部分疑问可以在其中找到答案。
使用的例程叫Example_2803xAdcSoc。改动的地方就是模仿voltage1和voltage2的配置加了voltage3和voltage4,具体来说就是:
Uint16 Voltage3[10];
Uint16 Voltage4[10];
AdcRegs.ADCSOC3CTL.bit.CHSEL = 4; //set SOC3 channel select to ADCINA4
AdcRegs.ADCSOC4CTL.bit.CHSEL = 6; //set SOC4 channel select to ADCINA6
AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 9;
AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 9;
AdcRegs.ADCSOC3CTL.bit.ACQPS = 9;
AdcRegs.ADCSOC4CTL.bit.ACQPS = 9;
Voltage3[ConversionCount] = AdcResult.ADCRESULT3;
Voltage4[ConversionCount] = AdcResult.ADCRESULT4;
就这几行,别的没有了。
我就想知道调试的时候为什么voltage1和voltage2的数值分别在25和17上下浮动,而voltage3和voltage4的数值分别在1255和1830上下浮动。
还有就是为什么每组adc采样的voltage数值浮动范围都不一样,到底voltage的数值应该是多少。
你好我试了一下,发现voltage2的值基本准确,voltage3和voltage5的值跟真实电压值差很多。
真实电压值调大,voltage3和voltage5会变大;真实电压值调小,voltage3和voltage5也会变小,但是数值上差很多。
这是为啥,我感觉我的配置没问题呀,麻烦您看一下,谢谢。
建议您先检查一下输入IO口以及对应的输出IO口是否正确,都正确的话那么可能是硬件上的问题。
建议先使用未修改的官方例程测试一下(有TI官方板更好),一般情况下例程是不会出错的。
device_support/f2803x/v126/DSP2803x_examples_ccsv4/adc_soc,按照这个路径就能找到soc的官方例程,这个文件夹有很多官方例程,都可以学习看看,我也是这样过来的
您可以在C2000ware中找到:
C:\ti\c2000\C2000Ware_5_00_00_00\device_support\f2803x\examples\c28\adc_soc
device_support/f2803x/v126/DSP2803x_examples_ccsv4/adc_soc,按照这个路径就能找到soc的官方例程,
这个是在controlsuite中的路径。