Other Parts Discussed in Thread: C2000WARE, CONTROLSUITE
新手一枚,想请大神看一下我的adc采样配置有没有问题。代码已上传:
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
// Prototype statements for functions found within this file.
__interrupt void adc_isr(void);
void Adc_Config(void);
// Global variables used in this example:
Uint16 LoopCount;
Uint16 ConversionCount;
Uint16 Voltage1[10];
Uint16 Voltage2[10];
Uint16 Voltage3[10];
Uint16 Voltage4[10];
main()
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2803x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initialize GPIO:
// This example function is found in the DSP2803x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2803x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2803x_DefaultIsr.c.
// This function is found in DSP2803x_PieVect.c.
InitPieVectTable();
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected register
PieVectTable.ADCINT1 = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2803x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
InitAdc(); // For this example, init the ADC
// Step 5. User specific code, enable interrupts:
// Enable ADCINT1 in PIE
PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable INT 1.1 in the PIE
IER |= M_INT1; // Enable CPU Interrupt 1
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
LoopCount = 0;
ConversionCount = 0;
// Configure ADC
// Note: Channel ADCINA4 will be double sampled to workaround the ADC 1st sample issue for rev0 silicon errata
EALLOW;
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //ADCINT1 trips after AdcResults latch
AdcRegs.INTSEL1N2.bit.INT1E = 1; //Enabled ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 0; //Disable ADCINT1 Continuous mode
AdcRegs.INTSEL1N2.bit.INT1SEL = 2; //setup EOC2 to trigger ADCINT1 to fire
AdcRegs.ADCSOC0CTL.bit.CHSEL = 1; //set SOC0 channel select to ADCINA1(dummy sample for rev0 errata workaround)
AdcRegs.ADCSOC1CTL.bit.CHSEL = 1; //set SOC1 channel select to ADCINA1
AdcRegs.ADCSOC2CTL.bit.CHSEL = 2; //set SOC2 channel select to ADCINA2
AdcRegs.ADCSOC3CTL.bit.CHSEL = 4; //set SOC3 channel select to ADCINA4
AdcRegs.ADCSOC4CTL.bit.CHSEL = 6; //set SOC4 channel select to ADCINA6
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 9; //set SOC0 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 9; //set SOC1 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 9; //set SOC2 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 9; //set SOC1 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 9; //set SOC2 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC0CTL.bit.ACQPS = 9; //set SOC0 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
AdcRegs.ADCSOC1CTL.bit.ACQPS = 9; //set SOC1 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
AdcRegs.ADCSOC2CTL.bit.ACQPS = 9; //set SOC2 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
AdcRegs.ADCSOC3CTL.bit.ACQPS = 9; //set SOC1 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
AdcRegs.ADCSOC4CTL.bit.ACQPS = 9; //set SOC2 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
EDIS;
// Assumes EPwm3 clock is already enabled in InitSysCtrl();
EPwm3Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm3Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount
EPwm3Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm3Regs.CMPA.half.CMPA = 0x0080; // Set compare A value
EPwm3Regs.TBPRD = 0xFFFF; // Set period for EPwm3
EPwm3Regs.TBCTL.bit.CTRMODE = 0; // count up and start
// Wait for ADC interrupt
for(;;)
{
LoopCount++;
}
}
__interrupt void adc_isr(void)
{
Voltage1[ConversionCount] = AdcResult.ADCRESULT1; //discard ADCRESULT0 as part of the workaround to the 1st sample errata for rev0
Voltage2[ConversionCount] = AdcResult.ADCRESULT2;
Voltage3[ConversionCount] = AdcResult.ADCRESULT3;
Voltage4[ConversionCount] = AdcResult.ADCRESULT4;
// If 20 conversions have been logged, start over
if(ConversionCount == 9)
{
ConversionCount = 0;
}
else ConversionCount++;
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //Clear ADCINT1 flag reinitialize for next SOC
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
return;
}
其中关于adc的设置有疑问的点在于:
下面附上程序刷进F28035后,调试时voltage1至voltag4的采样截图和Expressions截图:
voltage1:

voltage2:

voltage3:

voltage4:

Expressions:

问题是:
1.我的adc配置是否有问题。
2.为什么voltage1和voltage2的数值分别在25和17上下浮动,而voltage3和voltage4的数值分别在1255和1830上下浮动。
3.为什么每组adc采样的voltage数值浮动范围都不一样,到底voltage的数值应该是多少。