汇集牛人原创电路图,值得赏读。
1、去年做的一个扩展板卡,用于“C2000 LaunchPad”外扩。实现单相交流电压电流表采样及显示。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
汇集牛人原创电路图,值得赏读。
1、去年做的一个扩展板卡,用于“C2000 LaunchPad”外扩。实现单相交流电压电流表采样及显示。
10、本产品电路设计核心采用了DSP+ARM控制器的控制板卡,该控制板卡采用6层板设计,搭载一颗TMS320VC33 150MHZ的DSP器件,一颗LM3S8962的cortex-m3器件,采用了多种供电方式,既可以支持USB接口供电,也可以采用外部7V-12V 供电,搭载一颗CY37064CPLD和一片FT245BM USB转串口芯片,可以方便实现和电脑端的上位机通信。同时,作为主控制核心的DSP,主要负责算法处理。可以加载U盘模块,外加SRAM模块,板上外扩 4M位的FLASH,可在其上运行DSP程序。当时采用LM3S8962,主要是考虑其带有网络功能,可以实现远程控制。