This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的振荡电路参考了Launch_Pad,与芯片手册推荐相同但波形不同,无法烧录。
你好,谢谢你的解答,使用JTAG时TRST引脚约为2V,我将有片外电源引脚逐一测试均正常,但是使用PLECS仿真(配置如下)时出现以下错误,无法连接cpu
Error in build step #15 (Make): Make process exited with code 2: copy /Y "E:\plecs\support_package\tsp_ti_c2000\demos\simple_model\simple_model_codegen\ControlCard_TMS320F28379D.ccxml" ".\output_TI2837x_cpu1\pl_28379D.ccxml" Ѹ 1 ļ "C:/ti/uniflash_8.5.0/dslite.bat" --flash --config=.\output_TI2837x_cpu1\pl_28379D.ccxml .\output_TI2837x_cpu1\pl_28379D.out -u Executing the following command: > "C:\ti\uniflash_8.5.0\deskdb\content\TICloudAgent\win\ccs_base\DebugServer\bin\DSLite" flash --flash --config=.\output_TI2837x_cpu1\pl_28379D.ccxml .\output_TI2837x_cpu1\pl_28379D.out -u For more details and examples, please refer to the UniFlash Quick Start guide. C28xx_CPU1: GEL Output: Memory Map Initialization Complete info: C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed. error: C28xx_CPU1: Error: (Error -1135 @ 0xC095) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.13.0.00201) fatal: C28xx_CPU1: Trouble Halting Target CPU: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.13.0.00201) error: C28xx_CPU1: Error: (Error -1135 @ 0xC095) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.13.0.00201) error: C28xx_CPU1: Unable to determine target status after 20 attempts error: C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging error: C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected error: C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected error: C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected error: C28xx_CPU1: Error occurred during flash operation: Could not read 0x000130@Program: target is not connected error: C28xx_CPU1: Error executing PLL configuration algorithm. Operation cancelled. (0x0) error: C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D200@Data: target is not connected error: C28xx_CPU1: File Loader: Memory write failed: Unknown error pl_28379D.mk:170: recipe for target 'download' failed Failed: File: .\output_TI2837x_cpu1\pl_28379D.out: Load failed. make: *** [download] Error 1
您好,
PLECS不是TI的软件,这个软件的调试问题我们无法支持更多。
请问TI的 XDS系列调试器+CCS/UNIFLASH是可以编程成功吗?
如果可以,说明就是PLECS与匹配的调试器的驱动问题。