• TMS320F28379D: 导入例程出现故障Description Resource Path Location Type gmake: *** [gridconnectedinvlclfltr.obj] Error 1 gridConnectedInverterLCLFltr C/C++ Problem

    Part Number: TMS320F28379D
    Other Parts Discussed in Thread: CONTROLSUITE, SFRA

    故障详情:
    **** Build of configuration F2837x_RAM for project gridConnectedInverterLCLFltr ****

    "C:\\ti\\ccs1260\\ccs\\utils\\bin\\gmake" -k all

    Building file: "../F2837xD_CodeStartBranch…

  • TMS320F28377D: 设计并网逆变器或电机驱动

    Part Number: TMS320F28377D
    Other Parts Discussed in Thread: CONTROLSUITE

    尊敬的TI技术支持,我现在需要使用28379d设计并网逆变器控制程序。想咨询一下TI官方有没有可以参考的官方例程。

    关于电机驱动的也行。

    我以前在ControlSuite中找到一个SVPWM的例程,但是现在找不到了,您能不能提示一下具体在那个文件夹。

  • TMS320F28335: 伺服驱动三环位置环+速度环+扭力环设计的PI参数问题

    Part Number: TMS320F28335
    Other Parts Discussed in Thread: CONTROLSUITE

    Dear TI  supports:

    我现在用TI的TMS320F28335做一款电动工具,采用HPWM_LON,有感方波,位置环(三相霍尔反馈)+速度环(三相霍尔反馈)+扭力环(扭力传感器反馈)

    参考了《C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v2.1\HVPM_Sensored_Servo…

  • TMS320F28035: Using the function in CLAmath compiles with a warning “Data is being written to auto-generated file 28035 NIMI CLA.i10”

    Part Number: TMS320F28035
    Other Parts Discussed in Thread: CONTROLSUITE

    I added the .lib file “ cla0 math library.lib” and the .h file “CLAmath” to the project. Both files are found in “D:\CONTROLSUITE\controlSUITE\libs\math\CLAmath\v4_02_00_00” and I…

  • TMS320F28027: Flash2802x_API_V200.lib谁能提供给我一份,万分感谢!

    Part Number: TMS320F28027
    Other Parts Discussed in Thread: C2000WARE, CONTROLSUITE Flash2802x_API_V200.lib
  • TMS320F28379D: 如何在28379D实现biss-c通信

    Part Number: TMS320F28379D
    Other Parts Discussed in Thread: BOOSTXL-POSMGR, LAUNCHXL-F28379D, C2000WARE, CONTROLSUITE

    想在28379D实现biss-c,已经购买了BOOSTXL-POSMGR和launchxl-F28379D,但是没有配套开发板的28379biss例程,在c2000ware moter control sdk中关于biss的只有F28P65X的例程,请问是否提供LAUNCHXL…

  • LAUNCHXL-F28379D: 对solar库的sogi锁相环应用的问题

    Part Number: LAUNCHXL-F28379D
    Other Parts Discussed in Thread: CONTROLSUITE

    Ti的工程师们你们好!

    我想要在控制板的CLA上应用solar库的sogi锁相环,但是我在按照里面的步骤进行后运行代码出现了问题。

    在官方文档中一共有五步,其中第一步是添加library库,但是在运行过程中ccs软件好像并没有识别到我的Solar_CLA.h这个文件,但是我应该已经将文件链接上去了,想问问看TI的工程师们问题是出现在哪个地方?

  • TMS320F2800155: 在配置MCAN功能时出现问题

    Part Number: TMS320F2800155

    参照TI例程配置完成MCAN后,烧录程序进行仿真发现message ram没有初始化,无法写入数据。

  • TMS320F28069: 我在使用069上面的CSM模块,目前想单独使能此模块保护特定的ram区域,但我参考controlSUITE中的文件并没有提及这个

    Part Number: TMS320F28069
    Other Parts Discussed in Thread: CONTROLSUITE

    应该如何编写.asm模块来使能csm保护特定的ram区?我参考了07x系列,它有.syscfg文件可以手动配置要保护的RAM,但是06x系列没有这个文件来手动配置

  • TMDSHVMTRINSPIN: 关于TMDSHVMTRINSPIN的硬件支持

    Part Number: TMDSHVMTRINSPIN
    Other Parts Discussed in Thread: CONTROLSUITE

    你好

    Ti的工程师们

    我之前从TI这里采购了一套TMDSHVMTRINSPIN套件,不知道TI这边是否能提供相关的PCB,或者说在哪里可以下载

  • TMS320F280025: controlsuite一直显示下载失败

    Part Number: TMS320F280025
    Other Parts Discussed in Thread: CONTROLSUITEWe are sorry but your transaction has been denied.

    我选择了民用,而且选择了yes,为什么还是下载失败controlsuite。

  • TIDM-BIDIR-400-12: 申请SDK源码

    Part Number: TIDM-BIDIR-400-12
    Other Parts Discussed in Thread: CONTROLSUITE

    TI工程师,您好,

       申请TIDM-BIDIR-400-12相关SDK 源码,麻烦提供一下,谢谢!

  • TMS320F28377D: IPC无法进入中断

    Part Number: TMS320F28377D
    Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE

    TMS320F28377D IPC无法进中断

    CPU1设置IPC的中断0,CPU2相应该中断,查看CPU1的IPC_FLAG的bit0和CPU2的IPC_STS的bit0,都置位为1,但是CPU2无法进入中断

    我用TI的例程,也不能进入中断

    C:\ti\controlSUITE\device_support\F2837xD\v210…

  • TMS320F28335: 如何使用片外RAM进行快速傅里叶变换运算?

    Part Number: TMS320F28335
    Other Parts Discussed in Thread: CONTROLSUITE

    想使用片外RAM进行傅里叶变换,即调用RFFT_32(),RFFT_32_mag()实现。可是输出数据都是+Inf和-Inf,这是为什么? 

    可以用指针对片外RAM正常进行读写。

  • TMS320C28344: 历程库要在哪里寻找

    Part Number: TMS320C28344

    我刚刚入门TMS320C28344,这款芯片的历程库要在哪里寻找。

  • TMS320F28335: 使用controlsuit软件往CCS软件里引入solar库报错,已经把solar库放在项目properties中但还是报错。Using the controlsuit software to import the solar library into the CCS software gives an error, and the solar library has been placed in the project properties but the error...

    Part Number: TMS320F28335
    Other Parts Discussed in Thread: CONTROLSUITE

    代码内容(Code content):

    #include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
    #include "DSP2833x_Examples.h" // DSP2833x Examples Include File
    #include <math…

  • TMS320F28377D: 是否有关 USBHCDC 的代码例程或库

    Part Number: TMS320F28377D
    Other Parts Discussed in Thread: CONTROLSUITE

    您好:

    项目开发中,需要使用DSP与一个 以太网模块通信。二者通信方式使用USB。以太网模块作为USB-CDC设备。需要DSP作为USB主机。

    但是 TI controlSUITE 的host例程中并没有 有关CDC的例程或 CDC类驱动程序库。

    请问 是否有 USB主机 控制CDC设备的例程,哪里可以找到?

    或者说 CDC的驱动类程序需要自行编写?自行编写是否有指导手册可以参考…

  • TMS320F28377D: 有关于 USB虚拟串口 例程一些的问题

    Part Number: TMS320F28377D
    Other Parts Discussed in Thread: CONTROLSUITE

    专家您好:

    项目需要使用 USB虚拟串口功能,所以在研究 TI例程: C:\ti\controlSUITE\device_support\F2837xD\v210\F2837xD_examples_Cpu1\usb_dev_serial\cpu01

    有几个疑问需要解答:

    1、我看到例程中,除了初始化USB之外还初始化了SCIA,请问 这里串口与USB 是什么对应关系…

  • TMS320F280049C: TMS320F280049C

    Part Number: TMS320F280049C
    Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE-DIGITALPOWER-SDK

    您好,

        请问一下DCL_runDF22_C4,DCL_runDF22_C5,DCL_runDF22_C6与下面的2P2Z在使用时有什么区别呢,参数ek使用时必须进行标幺化吗?下面的代码来自controlSUITE。(C:\ti\controlSUITE\libs\app_libs\solar\v1…

  • TMS320F28335: controlSUITE中DSP库关于rfft输出相位的数据怎么理解和使用?

    Part Number: TMS320F28335
    Other Parts Discussed in Thread: CONTROLSUITE

    controlSUITE中DSP库的函数void RFFT_f32_phase (RFFT_F32_STRUCT *),其输出应该在RFFT_F32_STRUCT结构体中的float32 *PhaseBuf指针中,但是需要多大的数组去存储结果?(FPU DSP Software Library USER’S GUIDE 5.16 Real Fast Fourier…

  • CONTROLSUITE: C2000™︎ 微控制器论坛

    Part Number: CONTROLSUITE

    麻烦请问一下,如何下载CONTROLSUITE:?谢谢

    选了civil

    下载失败,提示:

    TI Request
     
    We are sorry but your transaction has been denied.

    If you feel you have been denied incorrectly, please contact the TI Customer Support Center at https://www.ti.com/…

  • LAUNCHXL-F28379D: 例程

    Part Number: LAUNCHXL-F28379D
    Other Parts Discussed in Thread: DRV8302, CONTROLSUITE, C2000WARE

    用上述控制板配合DRV8302驱动板来驱动电机,请问有没有PWM发波和AD采样相关的适配例程

  • TMS320F280049C: DCL_runDF22

    Part Number: TMS320F280049C
    Other Parts Discussed in Thread: CONTROLSUITE

    您好,

        请问一下DCL_runDF22_C4,DCL_runDF22_C5,DCL_runDF22_C6与下面的2P2Z在使用时有什么区别呢,参数ek使用时必须进行标幺化吗?下面的代码来自controlSUITE。(C:\ti\controlSUITE\libs\app_libs\solar\v1.2\float\source)

  • TMS320F28377D: C2000和controlSuite关于cmd中BOOT_RSVD长度定义不同

    Part Number: TMS320F28377D
    Other Parts Discussed in Thread: CONTROLSUITE

    文件都是2837xD_FLASH_CLA_lnk_cpu1.cmd

    下面是C2000中

    下面是controlSuite中

    关于BOOT_RSVD的长度,是0x000121还是0x000120呢?请问有人知道哪一个是正确的呢?

    或者帮我转到英文论坛呢?我在英文论坛发不了,说要有公司邮箱什么的。

    诚挚感谢!

  • CONTROLSUITE: 关于I-TOTAL的疑问

    Part Number: CONTROLSUITE

    上图为controlSUITE\development_kits\DRV830x-HC-C2-KIT_v105\~DRV830x-HC-EVM-HWdevPkg\DRV830x_RevD_HWDevPKG原理图

    问题1. 请问该设计中的I-TOTAL是等于三相桥母线供电直流电源的电流吗,也就是母线电流。

    问题2.如上图所示,是我目前设计的母线电流采集电路,麻烦大家帮我看下有问题吗?目前调试发现母线电流采集值波动很大。

    PWM波的产生方式是CAD_SET…

1 2 3 4 5 »