This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2433的TA0R计数器问题

Other Parts Discussed in Thread: MSP430FR2433

Hi TI team:

1、在使用MSP430FR2433的TA0R不计数,发现如果执行延时函数,TA0R能够正常计时,但是其他的语句无法让TA0R计时;

2、想了解下在主频配置或者定时器初始化有什么不一样的地方?现在用的是16M主频,对输入时钟进行了8分频,8s中断唤醒一次

3、又测试发现如果定时器时钟源选择ACLK只有经过延时函数定时器可以正常计时,其他语句指令不计时,时钟源选择SMCLK时,所有指令都可以正常计时。附件是测试程序。

main()
{
  _DINT(); 
  WDTCTL = WDTPW | WDTHOLD;

  PortInit();  
  
  Ucs_Init_16M();
//  Ucs_Init_1M();
  
  TimerA0CounterSetup();

while(1)  
  {
    __bis_SR_register(LPM3_bits | GIE);     // Enter LPM3

    WDTCTL = WDTPW | WDTCNTCL | WDTSSEL0_L | WDTIS_2;

    UCA1IE |= UCRXIE;    
    
    APP_RTCPro_Delay_ms(2);


    uiTranceiver=TA0R;
    do
    {
      __bis_SR_register(LPM3_bits | GIE);     // Enter LPM3

      if(TA0R>=uiTranceiver)uiTemp=TA0R;
      else uiTemp=TA0R+0x8000;
      if((uiTemp-uiTranceiver)> T50ms) //400ms
      {
        P1OUT |= BIT3;
       P3OUT |=BIT3;;
        break;
      }
    }while((uiTemp-uiTranceiver)<(T200ms+T200ms));
    
    P1OUT |= BIT3;
    UCA1IE &= ~UCRXIE; 
  }
}


void Ucs_Init_16M(void)
{
  FRCTL0 = FRCTLPW | NWAITS_1;
  P2SEL0 |= BIT0 | BIT1; 
  do
  {
    CSCTL7 &= ~(XT1OFFG | DCOFFG);           // Clear XT1 and DCO fault flag
    SFRIFG1 &= ~OFIFG;
   } while (SFRIFG1 & OFIFG);                   // Test oscillator fault flag

  __bis_SR_register(SCG0);                           // disable FLL

  CSCTL3 |= SELREF__XT1CLK;
  CSCTL0 = 0;                                        // clear DCO and MOD registers
  CSCTL1 &= ~(DCORSEL_7);                            // Clear DCO frequency select bits first
  CSCTL1 |= DCORSEL_5;                               // Set DCO = 16MHz

  CSCTL2 = FLLD_0 + 487;                             // DCOCLKDIV = 16MHz

  __delay_cycles(3);
  __bic_SR_register(SCG0);                           // enable FLL
  while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1));         // FLL locked

  CSCTL4 = SELMS__DCOCLKDIV | SELA__XT1CLK;  // MCLK=SMCLK=DCO; ACLK=XT1

  PM5CTL0 &= ~LOCKLPM5;
}


void TimerA0CounterSetup(void)
{
  TA0CCTL0 |= CCIE;     // CCR0 interrupt enabled
  TA0CCR0 = 0x8000;
  TA0CTL = TASSEL_1 | TACLR | ID_3 | MC_1;            // ACLK, clear TAR,8��Ƶ��Up to CCR0
}

  • 您的源码是不是不全?编译后有很多未定义

    请给出完整代码,我会在测试后回复

  • Susan:
    主频配置或者定时器初始化和flash型单片机有什么不一样的地方?
  • 这个建议您看一下移植指南内的 7.2 Clock System 以及 8.5 Timer and IR Modulation Logic

    file.elecfans.com/.../o4YBAFnLh0OAMZjZAANywuLNynU627.pdf
  • 您这边测试跑例程是否会有出现同样情况。
  • 我测试了下例程 MSP430FR243x Demo - Timer0_A3, PWM TA0.1-2, Up Mode, 32KHz ACLK ,可以计数的·

  • Susan:
    时钟源为SMCLK的可以正常计数,时钟源为ACLK时计数有问题。可以测试ACLK为时钟源的嘛
  • 测试的是 MSP430F55xx_ta0_04.c                              Timer0_A5, Toggle P1.0, Overflow ISR, 32kHz ACLK

    也是可以计数的。请您使用例程测试一下

  • Susan:
    我拿例程测试时单步执行还是无法计数;您可以将您测试例程发我一下。另外我测试程序如下。

    main()
    {
      _DINT(); 
      WDTCTL = WDTPW | WDTHOLD;
    
      PortInit();  
      
      Ucs_Init_16M();
      
      TimerA0CounterSetup();
    
    while(1)  
      {
        __bis_SR_register(LPM3_bits | GIE);     // Enter LPM3
    
        WDTCTL = WDTPW | WDTCNTCL | WDTSSEL0_L | WDTIS_2;
    
        UCA1IE |= UCRXIE;    
        
        APP_RTCPro_Delay_ms(2);
        
        unsigned int uiTemp=0;
        unsigned int uiTranceiver=0;
    
        uiTranceiver=TA0R;
        do
        {
          __bis_SR_register(LPM3_bits | GIE);     // Enter LPM3
    
          if(TA0R>=uiTranceiver)uiTemp=TA0R;
          else uiTemp=TA0R+0x8000;
          if((uiTemp-uiTranceiver)> T50ms) //400ms
          {
            P1OUT |= BIT3;
            P3OUT |= BIT3;
            break;
          }
        }while((uiTemp-uiTranceiver)<(T200ms+T200ms));
        
        P1OUT |= BIT3;
        UCA1IE &= ~UCRXIE; 
      }
    }
    
    
    void PortInit(void)
    {      
      _DINT();
          
    //  P1DIR=0xff;     P1OUT=0x00;  
    //  P2DIR=0xff;     P2OUT=0x00; 
    //  P3DIR=0xff;     P3OUT=0x00;
    
      P1DIR=0;  P2DIR=0;  P3DIR=0;
     
      P1OUT |= BIT3;
      P3OUT &= ~BIT3;
          
      _NOP();  
    }
    
    
    void Ucs_Init_16M(void)
    {
      FRCTL0 = FRCTLPW | NWAITS_1;
      P2SEL0 |= BIT0 | BIT1; 
      do
      {
        CSCTL7 &= ~(XT1OFFG | DCOFFG);           // Clear XT1 and DCO fault flag
        SFRIFG1 &= ~OFIFG;
       } while (SFRIFG1 & OFIFG);                   // Test oscillator fault flag
    
      __bis_SR_register(SCG0);                           // disable FLL
    
      CSCTL3 |= SELREF__XT1CLK;
      CSCTL0 = 0;                                        // clear DCO and MOD registers
      CSCTL1 &= ~(DCORSEL_7);                            // Clear DCO frequency select bits first
      CSCTL1 |= DCORSEL_5;                               // Set DCO = 16MHz
    
      CSCTL2 = FLLD_0 + 487;                             // DCOCLKDIV = 16MHz
    
      __delay_cycles(3);
      __bic_SR_register(SCG0);                           // enable FLL
      while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1));         // FLL locked
    
      CSCTL4 = SELMS__DCOCLKDIV | SELA__XT1CLK;  // MCLK=SMCLK=DCO; ACLK=XT1
    
      PM5CTL0 &= ~LOCKLPM5;
    }
    
    
    void TimerA0CounterSetup(void)
    {
      TA0CCTL0 |= CCIE;     // CCR0 interrupt enabled
      TA0CCR0 = 0x8000;
      TA0CTL = TASSEL_1 | TACLR | ID_3 | MC_1;            // ACLK, clear TAR,8��Ƶ��Up to CCR0
    }
    
    void APP_RTCPro_Delay_ms(unsigned int iTimes)
    {
      for(unsigned int i=0;i<iTimes;i++)
      { 
        unsigned int uiTemp0=0; 
        unsigned int uiTranceiver0=TA0R; 
        do
        { 
          _NOP(); 
          if(TA0R>=uiTranceiver0) uiTemp0=TA0R; 
          else uiTemp0=TA0R+0x8000;   
        }while((uiTemp0-uiTranceiver0)<0x21 ); 
      }
    }
    
    
    /***********************************************************
    �������ƣ�
    �������ܣ���ʱ��TA0�жϷ����������ж�
    ��ڲ�����
    ���ڲ�����
    ������
    ************************************************************/
    #pragma vector=TIMER0_A0_VECTOR
    __interrupt void Timer_A0_Counter (void)
    {
      TA0CTL=TA0CTL&(~TAIFG);
      _BIC_SR_IRQ(LPM3_bits);	
      
    }
    

  • 对于MSP430,查看定时器寄存器的话,建议不要单步,您可以设置断点或者全速运行后暂停查看

    测试例程如下

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2014, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     *
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //  MSP430FR24xx Demo - Timer0_A3, Toggle P1.0, Overflow ISR, 32kHz ACLK
    //
    //  Description: Toggle P1.0 using software and the Timer0_A overflow ISR.
    //  In this example an ISR triggers when TA overflows. Inside the ISR P1.0
    //  is toggled. Toggle rate is exactly 0.5Hz. Proper use of the TAIV interrupt
    //  vector generator is demonstrated.
    //
    //  ACLK = TACLK = 32768Hz, MCLK = SMCLK = 8MHz/2
    //
    //
    //                MSP430FR2433
    //             -----------------
    //         /|\|                 |
    //          | |                 |
    //          --|RST              |
    //            |                 |
    //            |             P1.0|--> LED
    //
    //
    //  Wei Zhao
    //  Texas Instruments Inc.
    //  Jan 2014
    //  Built with IAR Embedded Workbench v6.20 & Code Composer Studio v6.0.1
    //******************************************************************************
    #include <msp430.h>
    
    int main(void)
    {
        WDTCTL = WDTPW | WDTHOLD;                    // Stop WDT
    
        // Configure clock
        __bis_SR_register(SCG0);                     // disable FLL
        CSCTL3 = SELREF__REFOCLK;                    // Set REFOCLK as FLL reference source
        CSCTL0 = 0;                                  // clear DCO and MOD registers
        CSCTL1 &= ~(DCORSEL_7);                      // Clear DCO frequency select bits first
        CSCTL1 |= DCORSEL_3;                         // Set DCOCLK = 8MHz
        CSCTL2 = FLLD_1 + 121;                       // FLLD = 1, by default, DCODIV = DCO/2 = 4MHz
        __delay_cycles(3);
        __bic_SR_register(SCG0);                     // enable FLL
        while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1));   // Poll until FLL is locked
    
        CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK;   // set ACLK = REFOCLK = 32768Hz, DCOCLK as MCLK and SMCLK source
        CSCTL5 |= DIVM0 | DIVS0;                     // SMCLK = MCLK = DCODIV = 4MHz
    
        // Configure GPIO
        P1DIR |= BIT0;
        P1OUT |= BIT0;
    
        // Disable the GPIO power-on default high-impedance mode to activate
        // previously configured port settings
        PM5CTL0 &= ~LOCKLPM5;
    
        // Configure Timer_A
        TA0CTL = TASSEL_1 | MC_2 | TACLR | TAIE;      // ACLK, count mode, clear TAR, enable interrupt
    
        __bis_SR_register(LPM3_bits | GIE);           // Enter LPM3, enable interrupts
        __no_operation();                             // For debugger
    }
    
    // Timer0_A3 Interrupt Vector (TAIV) handler
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=TIMER0_A1_VECTOR
    __interrupt void TIMER0_A1_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(TIMER0_A1_VECTOR))) TIMER0_A1_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
        switch(__even_in_range(TA0IV,TA0IV_TAIFG))
        {
            case TA0IV_NONE:
                break;                               // No interrupt
            case TA0IV_TACCR1:
                break;                               // CCR1 not used
            case TA0IV_TACCR2:
                break;                               // CCR2 not used
            case TA0IV_TAIFG:
                P1OUT ^= BIT0;                       // overflow
                break;
            default:
                break;
        }
    }
    

  • Susan:
    谢谢。之前用FXX的单片机可以单步调试可以看得到。这个是FR系列和FXX系列的区别么。
  • 这个确实没太注意过。我会在确认后给您回复