This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
/*********************************************************
此为flash_writechar() 的子函数,将infoA段的数据复制到RAM中
********************************************************/
void flash_backup2RAM_char(unsigned int segment,unsigned char *array,int segsize)
{
unsigned char *ptr=(unsigned char *)segment;
int i;
for(i=0;i<segsize;i++)
{
array[i]=ptr[i];
}
}
void flash_writechar(unsigned int addr,unsigned char data)
{
unsigned char *flash_ptra;
unsigned char *flash_ptrb;
unsigned char backuparray[32];
int i;
flash_ptra=(unsigned char *)0x1080;
flash_ptrb=backuparray;
flash_backup2RAM_char(flash_saveaddr,backuparray,32);
FCTL1=FWKEY+ERASE;
FCTL3=FWKEY;
_DINT();
*flash_ptra=0;
while(FCTL3&BUSY);
FCTL1=FWKEY+WRT;
for(i=0;i<MAX_DATA_NUM;i++)
{
if(i==addr)
{
*flash_ptra++=data;
while(FCTL3&BUSY);
flash_ptrb++;
}
else
{
*flash_ptra++=*flash_ptrb++;
while(FCTL3&BUSY);
}
}
FCTL1=FWKEY;
FCTL3=FWKEY+LOCK;
_EINT();
}
例如:
void main()
{
flash_writechar(addr_gaoya,0x02);
}
调试的时候,全速运行以上主函数,能成功在0x1080偏移量为addr_gaoya的地址上写入0x02 ;
但
void main()
{
flash_writechar(addr_gaoya,0x02);
flash_writechar(addr_default,0x05);
_NOP();
}
调试的时候,全速运行以上主函数,则无法在以上两个任意一个地址写入任意一个数(即0x1080,infoA段上仍然全是FF)。如果在下一句的_NOP();处设置断点,
全速运行后到达不了该断点处。
PS: IAR里的opinion里的FET Debugger里的“erase main memory” 与“erase main and information memory”选项 都已尝试过。
求解惑
waterank join, 每次对Flash写入内容之前,需要先erase.即每erase一次,在同一地址只可写入一次。这是flash的特性。举个例子,erase后,某个地址是0xFFFF, 后对该地址写入0x0000, 如果你再在这一地址写入0x0001,那是肯定不会成功的。当然此例子有些极端。
你可以参考一下TI MSP430Ware中flash write的例程看看。
附件是MSP430F149在MSP430Ware中的例子,你可以看看,每次写之前,都进行了erase。希望对你有帮助!O(∩_∩)O~
/* --COPYRIGHT--,BSD_EX * Copyright (c) 2012, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //**************************************************************************** // MSP-FET430P140 Demo - Flash In-System Programming, Copy SegA to SegB // // Description: This program first erases flash seg A, then it increments all // values in seg A, then it erases seg B, then copies seg A to seg B. // Assumed MCLK 550kHz - 900kHz. // //* Set Breakpoint on NOP in the Mainloop to avoid Stressing Flash *// // // MSP430F149 // ----------------- // /|\| XIN|- // | | | // --|RST XOUT|- // | | // // M. Mitchell // Texas Instruments Inc. // Feb 2005 // Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.21A //****************************************************************************** #include <msp430.h> char value; // 8-bit value to write to segment A // Function prototypes void write_SegA (char value); void copy_A2B (void); int main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer FCTL2 = FWKEY + FSSEL0 + FN0; // MCLK/2 for Flash Timing Generator value = 0; // Initialize value while(1) // Repeat forever { write_SegA(value++); // Write segment A, increment value copy_A2B(); // Copy segment A to B _NOP(); // SET BREAKPOINT HERE } } void write_SegA (char value) { char *Flash_ptr; // Flash pointer unsigned int i; Flash_ptr = (char *) 0x1080; // Initialize Flash pointer FCTL1 = FWKEY + ERASE; // Set Erase bit FCTL3 = FWKEY; // Clear Lock bit *Flash_ptr = 0; // Dummy write to erase Flash segment FCTL1 = FWKEY + WRT; // Set WRT bit for write operation for (i=0; i<128; i++) { *Flash_ptr++ = value; // Write value to flash } FCTL1 = FWKEY; // Clear WRT bit FCTL3 = FWKEY + LOCK; // Set LOCK bit } void copy_A2B (void) { char *Flash_ptrA; // Segment A pointer char *Flash_ptrB; // Segment B pointer unsigned int i; Flash_ptrA = (char *) 0x1080; // Initialize Flash segment A pointer Flash_ptrB = (char *) 0x1000; // Initialize Flash segment B pointer FCTL1 = FWKEY + ERASE; // Set Erase bit FCTL3 = FWKEY; // Clear Lock bit *Flash_ptrB = 0; // Dummy write to erase Flash segment B FCTL1 = FWKEY + WRT; // Set WRT bit for write operation for (i=0; i<128; i++) { *Flash_ptrB++ = *Flash_ptrA++; // Copy value segment A to segment B } FCTL1 = FWKEY; // Clear WRT bit FCTL3 = FWKEY + LOCK; // Set LOCK bit }
Lina Lian,你好!这个flash_writechar()函数里,已有对infoA段进行erase的操作。 先将infoA段的数据复制到RAM里,然后擦除infoA段,然后将复制到RAM的数据与需要更改的数据一并写入infoA段里。
FCTL1=FWKEY+ERASE;
FCTL3=FWKEY;
_DINT();
*flash_ptra=0;
while(FCTL3&BUSY);
这个是flash_writechar()函数里,对infoA段进行erase的代码。
补充:
void flash_init(void)
{
FCTL2=FWKEY+FSSEL_2+FN4+FN2+FN1;
}
这是对flash的时钟进行设置的函数
弄好了
因为是FLASH时钟频率设置这个函数我写在后面去了,所以一开始erase写入什么的,都还没有对FLASH时钟频率进行设定
自然出了问题