#include <stdint.h> #include <stdbool.h> #include "inc/hw_memmap.h" #include "inc/hw_types.h" #include "inc/hw_gpio.h" #include "inc/hw_ints.h" #include "driverlib/gpio.h" #include "driverlib/pin_map.h" #include "driverlib/sysctl.h" #include "driverlib/interrupt.h" #include "driverlib/eeprom.h" #include "utils/uartstdio.h" #define E2PROM_TEST_ADRES 0x0000 struct E2PROM { uint8_t value1; uint8_t value2; uint16_t value3; uint8_t value4[12]; }; struct E2PROM e2prom_write_value = {5,7,9826, "Hello World"}; /* Write struct */ struct E2PROM e2prom_read_value = {0,0,0,""}; /* Read struct */ int main(void) { uint32_t e2size,e2block; SysCtlClockSet(SYSCTL_SYSDIV_2_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ); // islemcimizi 80 Mhz'e ayarlıyoruz. /* UART SETTINGS */ SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); GPIOPinConfigure(GPIO_PA0_U0RX); GPIOPinConfigure(GPIO_PA1_U0TX); GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); UARTStdioConfig(GPIO_PORTA_BASE,115200,SysCtlClockGet()); /*******************************/ /* EEPROM SETTINGS */ SysCtlPeripheralEnable(SYSCTL_PERIPH_EEPROM0); // EEPROM activate EEPROMInit(); // EEPROM start /*******************************/ UARTprintf("EEPROM Test Program ,, Teknikyazi.com\r\n"); e2size = EEPROMSizeGet(); // Get EEPROM Size UARTprintf("EEPROM Size %d bytes\n", e2size); e2block = EEPROMBlockCountGet(); // Get EEPROM Block Count UARTprintf("EEPROM Blok Count: %d\n", e2block); UARTprintf("Write Try > Address %u: Struct : {%u,%u,%u,%s}\n", E2PROM_TEST_ADRES, e2prom_write_value.value1, e2prom_write_value.value2, e2prom_write_value.value3, e2prom_write_value.value4); EEPROMProgram((uint32_t *)&e2prom_write_value, E2PROM_TEST_ADRES, sizeof(e2prom_write_value)); //Write struct to EEPROM start from 0x0000 EEPROMRead((uint32_t *)&e2prom_read_value, E2PROM_TEST_ADRES, sizeof(e2prom_read_value)); //Read from struct at EEPROM start from 0x0000 UARTprintf("Read Try > Address %u: Struct : {%u,%u,%u,%s}\n", E2PROM_TEST_ADRES, e2prom_read_value.value1, e2prom_read_value.value2, e2prom_read_value.value3, e2prom_read_value.value4); while(1) { } }