This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8825: 实际电流与VREF和转速的关系

Part Number: DRV8825


DRV8825相关问题

  • 相电流峰值(Aout1)和Vref(模块上的电位器)设置电压不匹配
    实验初始设置条件:VREF:0.93V;2.负载:空载;3.Mode:1/16;4.电源电压:24V
    实验过程数据:

step信号频率和相电流峰值数据

PWM/Hz

相电流峰值/A

电源电流/A

0

1.1

0.4

6400

1.08

0.46

8000

1.24

0.48

9600

1.34

0.5

10667

1.38

0.5

11200

1.4

0.5

12800

1.34

0.46

14400

1.26

0.41

16000

1.16

0.37

17600

1.02

0.33

21333

0.82

0.27


根据实验设置和实验数据,有如下问题:

问题1:在无负载,Vref参考电压为0.93V,电机转动情况下,为什么相电流峰值没达到设定值(设定值计算公式:current limit=(100%)=相电流峰值=2*VREF(=0.1Ω)=0.93V*2=1.86A)?
问题2:在无负载,参考电压为0.93V,电机转动情况下,随step频率逐步增加的情况下(数据如上表所示)为什么相电流峰值先上升后下降?
问题3:电源电流与电机相电流关系,在电机转动情况下,相电流随时间正弦波式变化,其相电流有效值(幅值除以)为什么会大于电源的电流?其是否有相应的解算或者逻辑映射关系?

问题4:在固定脉冲step的输入和步进电机不失步的条件下,不同负载情况下步进电机输出扭矩变化,如何计算步进电机输出扭矩,或者说步进电机输出扭矩与电机哪些参数相关?具体关系是什么?