This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用BQ25703A设计1CELL 锂电池充电方案,目前使用TypeC接普通充电器(5V)可以充电,但是接带PD的适配器就无法充电,log显示pd disable,量测CHRG_OK在插入PD适配器后拉高,但很快就拉低了,请教下要使用PD快充,需要从哪方面来看,谢谢!2514.BQ25703A TypeC charge design.pdf
您好
Let's start by debugging why CHRG_OK is pulled low shortly after the USB PD adapter is plugged in. CHRG_OK should stay high as long as the VBUS voltage is valid (VVBUS_CONVEN < VBUS < VACOV) and there are no faults.
Can you please capture a waveform showing VBUS, CHRG_OK, REGN, and VSYS on the same graph, similar to Figure 48 in the datasheet?