This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355: 低温-40℃下输出不稳定

Part Number: TPS53355


使用TPS53355,Vin=12V,Vout=1.03V,Iout max =20.4A,设计原理如下:

现在问题是低温-40℃下,输出有跌落,波形如下:(黄色为Vout,蓝色为Pgood)

常温下TPS53355的Vout上有与LX同频的毛刺,如下:

请问:

1、低温下TPS53355的动态响应与哪些参数有关?造成低温下Vout跌落的原因可能有哪些?

2、Vout上的与LX同频的毛刺是如何产生的,应怎么去除?

3、测试中发现空焊LX上的RC电路,会导致输出为0.39V左右,达不到设定值,原因为何?

期待回复,谢谢!