This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355: 低温-35℃下输出异常

Part Number: TPS53355


我们电路中TPS53355的使用条件是:Vin=12VVout=1.03VIout max =20.4A,设计原理如下:

注:

1、上图中所有电容均为陶瓷电容

2L1DCR1.06mΩ

3fsw=750KHz

现在遇到的问题有:

1、部分芯片低温-40℃下,上电输出只有0.5V左右,过几秒才会输出标称电压1.03V,波形如下:(常温下芯片输出正常)

2、部分芯片低温-35℃下,上电一段时间后有跌落,波形如下:此芯片低温-30℃下可以正常启动。

TPS53355输出电压不正常,导致系统低温下无法启动。

3、测试中发现芯片LL引脚的CsnubRsnub如果不焊接,或者参数不对,芯片输出只有0.39V左右,无法输出标称电压1.03V

现在已经尝试了以下方法:

1、修改纹波注入电路RrCr参数,使其接近L1/DCR(L1=330nHDCR=1.06mΩ),或者减小Cac680pF

2、修改电感值为550nH或者160nH,其他参数不变

3、增大电容,将Cbst增大为220nFCreg增大为10uFCin增加两个22uF电容,Cout增加两个100uF电容

以上方法测试均无改善

我的疑问是:

1、低温会影响TPS53355哪些参数,我应该如何应对这些影响

2、以我的应用来看,电路中哪些参数需要修改?

3、芯片LL引脚的CsnubRsnub作用是?为什么不焊接或参数不对,会影响输出?