This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28782: VDD维持13V无法启动问题

Part Number: UCC28782

UCC28782_65W_V1.0-0227.pdf

您好,上面是我的原理图,在使用UCC28782制作65W反激电源时,遇到初级电容电压为45V再往上增加时,UCC28782VDD无法启动的问题。

下面是我的图:黄色VDD,蓝色SWS,红色VSW,蓝色PWML

上面示波器的图是快要无法启动的时候,一旦VSW到达比45v更高电压时,VDD就会在13V间波动,无法正常地在17.5V和10.5V间跳动。

从SWS引脚上来看,应该是芯片内部的SWS到VDD的补电开关依然开着,使VDD和SWS引脚的电压波形一致。

请问这种情况怎么解决呢?期待您的回答谢谢