This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: CAN FD Controller and Test

Part Number: TDA4VM

Hello TI TDA4VM team

Could you provide the following information?

1.Successful passing of the CAN conformance test shall be confirmed through provision of a certificate/confirmation document  of a 3rd party test house or the semiconductor manufacturer;

2.Type number(s) of the used CAN FD controller product(s);

3.Was the CAN FD controller tested against the complete ISO 16845-1 Conformance Test Plan?

4.Did the controller product(s) described in #2 pass the ISO 16845-1 Conformance Test Plan with 100% OK status? If not, please specify the influence of the failed test case;

x 出现错误。请重试或与管理员联系。