This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI TDA4VM team
Could you provide the following information?
1.Successful passing of the CAN conformance test shall be confirmed through provision of a certificate/confirmation document of a 3rd party test house or the semiconductor manufacturer;
2.Type number(s) of the used CAN FD controller product(s);
3.Was the CAN FD controller tested against the complete ISO 16845-1 Conformance Test Plan?
4.Did the controller product(s) described in #2 pass the ISO 16845-1 Conformance Test Plan with 100% OK status? If not, please specify the influence of the failed test case;
Hi, sorry for the late reply!
Please see the document below and check if it's helpful: