PROCESSOR-SDK-AM62A: PROCESSOR-SDK-AM62A

Part Number: PROCESSOR-SDK-AM62A

1. AM62A seems to lack PROCESSOR-SDK-RTOS-J721E (environment SDK that supports onnx/tensorflow model transformation and deployment to TI hardware) similar to J721E.
2. Learned from the forum that FIRMWARE-BUILDER-AM62A exists, not sure whether this is the environment SDK for model transformation and deployment.
3. Is the operation of FIRMWARE-BUILDER-AM62A similar to that of PROCESSOR-SDK-RTOS-J721E?
Can I directly use PROCESSOR-SDK-RTOS-J721E and set the SOC compilation to AM62A for model transformation and deployment?
Someone who can answer questions about whether AM62A can be transformed and deployed using a development process similar to J721E. 

  • Thanks! for reading the following link, I seem to understand it, but I still lack the tidl-tools library and firmware builder, which seems to be under application. Could you please pass it? Are the tidl_model_import.out and tidl_model*.so libraries also compiled based on edgeai-tidl-tools? I'm still conflicted about it.

  • thanks! I seem to know how to convert this model to the AM62A platform, but I have a problem that the operator is not supported. A721A and tdA4 can be transferred normally before, how do I deal with it? What documents do I need to provide to help you troubleshoot this problem?

  • Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    (am62a) docker@8084c2d7f6f9:/ti-am62a/tools/AM62
    A/tidl_tools$ bash run.sh
    00eyeclose Start to transform
    01eyeclose Start to transform
    ========================= [Model Compilation Started] =========================
    Model compilation will perform the following stages:
    1. Parsing
    2. Graph Optimization
    3. Quantization & Calibration
    4. Memory Planning
    ============================== [Version Summary] ==============================
    -------------------------------------------------------------------------------
    | TIDL Tools Version | 10_01_04_00 |
    -------------------------------------------------------------------------------
    | C7x Firmware Version | 10_01_00_01 |
    -------------------------------------------------------------------------------
    ONNX model (Proto) file : ./model/eye.onnx
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX
    This is the overall log

x 出现错误。请重试或与管理员联系。