• PROCESSOR-SDK-AM62X: AM6234

    Part Number: PROCESSOR-SDK-AM62X
    Other Parts Discussed in Thread: TPS65219

    我们在使用最新的SDK11 调试我们的自制板时,通过SD卡启动,编译出来的tiboot3.bin tispl.bin uboot.img 无法正常启动,在R5的配置中添加了tps65219的配置后,上电运行后打印 alloc space exhausted ,请问如何在R5的配置中设置R5 spl的内存空间大小。

  • TDA4VM: 在我的自定义板子上我使用SDK版本10.01.00.04的Yocto生成的 tiboot3.bin出现不能正常刷写的错误

    Part Number: TDA4VM

    在我的自定义板子上我使用SDK版本10.01.00.04的Yocto生成的 tiboot3.bin出现不能正常刷写的错误,错误如下;

    tiboot3.bin刷写完成后刷写sysfw.itb

    此时本来应该出现但是dfu设备已经没有了。

    tda4vm的串口终端出现提示:

    我已经确定了我的自定义设备在ti-processor-sdk-linux-j7-evm-08_06_00_11也就是sdk的08_06_00_11版本可以的刷写但是我现在升级了到了10_01_00_04却不能正常刷写…

  • AM625: 如何构建生成ti-processor-sdk-linux-am62xx-evm-09.02.01.09-Linux-x86-Install.bin

    Part Number: AM625

    如题所说,因为该开发SDK里面没有我需要的开发库,想单独构建Install.bin

    尝试使用yocto去构建Install.bin但是编译参数并没有生成Install.bin的

    问题:如何构建生成Install.bin?

  • AM3358: ti-processor-sdk-linux-am335x-evm-09.03.05.02 内核编译报错

    Part Number: AM3358

    AM335X SDK (ti-processor-sdk-linux-am335x-evm-09.03.05.02)编译内核(make linux)报错:

    In file included from /home/xxx/am335x/ti-processor-sdk-linux-am335x-evm-09.03.05.02/external-toolchain-dir/arm-gnu-toolchain-11.3.rel1-x86_64-arm-none…

  • SK-AM62P-LP: AM62P-LP-EVM, 如何使用OPENOCD + GDB调试代码?

    Part Number: SK-AM62P-LP
    Other Parts Discussed in Thread: AM62P

    想使用openocd 调试下内核,找不到openocd相关的配置文件 openocd -f /ti_am62x.cfg。 官方会提供吗?

  • AM3354: AM335串口启动卡住

    Part Number: AM3354

    我们目前遇到了一个AM3354串口启动失败的问题。

    详细描述如下:

    我们刚打样了一批板子回来,CPUAM3354,我们启动顺序如下:

    SPI0->MMC0->USB0->UART0

    由于新板SPI0 FLASH没内容,MMC0USB0没用,所以最终会跳到UART0串口启动,此时终端不停打印CCCCC

    此时通过Xmodem协议往串口发送SPLu-boot-spl.bin),但是发送过程中总是卡住,终端提示如如下:

    分析:于是我们…

  • AM62A7: Executing edgeai-tiovx-apps-test with [ownContextSendCmd:875] Command ack message returned failure cmd_status: -1

    Part Number: AM62A7

    HI experts,

    The version of the SDK used is:10.1.8--v10.01.08

    Linux version 6.6.58-ti (aarch64-oe-linux-gcc (GCC) 13.3.0

    When I use the above version, I get the following error when executing the edgeai-tiovx-apps-test program:

    Here…

  • PROCESSOR-SDK-AM335X: beaglebone black Uboot SPL spi flash 启动失败, 报告: SPI probe failed.

    Part Number: PROCESSOR-SDK-AM335X
    Other Parts Discussed in Thread: TPS65217, TPS65910

    硬件环境: BBB / W25Q64 (Flash , 连接SPI0)

    软件环境: ti-processor-sdk-linux-am335x-evm-09.01.00.001

    配置:  am335x_evm_spiboot_defconfig

    CONFIG_ARM=y CONFIG_ARCH_CPU_INIT=y CONFIG_ARCH_OMAP2PLUS…

  • AM6422: change ethernet to switch mode

    Part Number: AM6422

    Is there a way just change DTS file to  achieve switch mode?

    we want to use netifd.service to config our bridge and ip address, the devlink command seems doesn't work after run netifd service.

  • AM3352: ti ccs12.8 报错 program “arm-linux-gnueabihf-gcc” not found in PATH

    Part Number: AM3352

    专家你好!

    我现在使用ti ccs12.8 编译自己程序,编译的结果没有问题,但是会报一个

    program “arm-linux-gnueabihf-gcc” not found in PATH   的错误。

    实际上我使用的  : arm-none-linux-gnueabihf-

    我仔细查看了CCS的各种配置,没有发现有:arm-linux-gnueabihf-

    还请这种问题怎么定位?

    非常感谢!

    秦龙

  • AM3352: AM335x 启动Linux内核时停止

    Part Number: AM3352
    Other Parts Discussed in Thread: TPS65910

    专家你好!

    我之前升级到ti-processor-sdk-linux-am335x-evm-09.03.05.02-Linux-x86-Install报错后提交问题,目前还没有得到回复。

    现在使用ti-processor-sdk-linux-am335x-evm-08.02.00.24-Linux-x86-Install,启动内核时停止了,具体的信息如下。

    U-Boot SPL…

  • AM3352: AM335x U-boot时报错

    Part Number: AM3352

    专家好!

    我目前使用ti-processor-sdk-linux-am335x-evm-09.03.05.02-Linux-x86-Install.bin

    u-boot和kernel编译已经通过,但是放到板子上执行的时候报:不能初始化定时器,

    具体错误如下:

    U-Boot SPL 2023.04 (Jan 03 2025 - 14:14:26 +0800)
    Trying to boot from MMC1


    U-Boot 2023.04 (Jan 03 2025…

  • AM6528: AM6528

    Part Number: AM6528

    Hi,

    Can the AM6528 be configured with a cache switch?

    Looking forward to a reply

  • AM3352: ti-processor-sdk-linux-am335x-evm-09.01.00.001内核编译报错

    Part Number: AM3352

    各位专家好!

    我在使用ti-processor-sdk-linux-am335x-evm-09.01.00.001编译Linux内核时,报如下错误。

    error: cannot load plugin ./scripts/gcc-plugins/arm_ssp_per_task_plugin.so: ./scripts/gcc-plugins/arm_ssp_per_task_plugin.so: undefined symbol: _ZN8opt_pas…

  • AM3358: 移植waland/weston 到AM335X 在运行的时候运行不成功,求解

    Part Number: AM3358

    我是利用Processor SDK Linux for AM335X 09_01_00_001 文件寫的yocto去抓weston跟wayland, 然後放我的檔案系統裡面跑wetston指令,

    卻發生下面的狀況

    root@am335x-evm:/run# weston
    Date: 2024-11-01 UTC
    [05:32:44.839] weston 10.0.2
    wayland.freedesktop.org
    Bug reports to: gitlab…

  • AM6442: sd卡接口提速

    Part Number: AM6442

    您好,我查了6442的数据手册支持SDR104,我尝试修改DTS,但是没有成功,请问怎么修改能支持SDR104,谢谢

    红框里面是我新增的,没有效果,我用的创龙的开发板,谢谢!

  • PROCESSOR-SDK-J722S: DCC tool ip address

    Part Number: PROCESSOR-SDK-J722S

    Hi;

    I would like to know how to obtain the IP address of the DCC Tuning tool.

  • BYTES-3P-BE-AM6254: 如何提高程序运行性能?

    Part Number: BYTES-3P-BE-AM6254

    工程师好:

    硬件环境:自研开发板  TI AM6254A TCGGAALW  8G+1G。

    问题描述:

    我有一段c程序,主要工作是int32_t data[2048]接收网络传输的数据。使用此数据的每个元素去用二分法在全局二维数组即表单数组int32_t table[2049][256]中查找对应的点,然后进行一些double计算。主要程序如下:

    #include....

    int32_t table[2049][256];//必须是全局变量…

  • TDA4VM: linux 下 配置与操作GPIO

    Part Number: TDA4VM

    按照官方给出的步骤,[FAQ] TDA4VM/DRA829/AM65xx: Linux: Configuring GPIOs - Processors forum - Processors - TI E2E support forums我在设备树下做了如下变动
    mygpio { compatible = "myesp32io"; pinctrl-names = "default"; pinctrl-0 = <&esp32_ctl1_pins_default…

  • AM3352: 长期运行后死机

    Part Number: AM3352

    我们用AM3352的一款产品在长期使用(一年半)的过程中,有一批(12个)出现访问EMMC后死机的现象,具体log如附件

    root@am335x-evm:/# [43946.836954] Unable to handle kernel paging request at virtual address f08f4314 [43946…

  • TDA4VM: How to implement CAN reception in the A72 core of TDA4 VM Eco

    Part Number: TDA4VM

    SOC: TDA4

    Description: I want to receive CAN data directly through the A72 core. How to configure it?

    Below is the CAN PIN definition

  • AM625: AM6254有无硬件H264解码和vpe模块

    Part Number: AM625

    目前使用gstreamer软件解码avdec_h264和videoconvert模块发现播放MP4只有20fps

    0:00:33.708014055 2127 0xacf9450 LOG fpsdisplaysink fpsdisplaysink.c:380:display_current_fps:<fpsdisplaysink0> Signaling measurements: fps:20.007778 droprate:0.000000 avg-fps…

  • AM625: AM6254执行modetest失败

    Part Number: AM625

    SDK:PROCESSOR-SDK-LINUX-RT-AM62X 

    Version: 08.06.00.42

    参考文档modetest的使用:3.8.1. Introduction — Processor SDK AM62x Documentation

    出现no device found,如下log信息:

    root@AM62x-Tronlong:~# modetest [ 909.127193] PVR_K: 1292: RGX Firmware…

  • AM3352: 升级至Processor SDK Linux for AM335X 09_01_00_001 在AM3352 BBB上无法启动, 可能与cpsw以及SDK版本有关

    Part Number: AM3352
    Other Parts Discussed in Thread: AM3359

    硬件板卡: AM3359 BBB 和 AM3352 BBB(仅处理器区别)

    软件环境: ti-processor-sdk-linux-am335x-evm-09.01.00.001 和 ti-processor-sdk-linux-am335x-evm-06.03.00.106

    场景:

    A. 使用ti-processor-sdk-linux-am335x-evm-09.01.00…

  • AM625: 这颗芯片的datasheet给出支持的分辨率是每通道1920x1080 @ 60fps

    Part Number: AM625

    这颗芯片的datasheet给出支持的分辨率是每通道1920x1080 @ 60fps,但是我的屏是1920*1200的,请问这个芯片能否达到1920*1200的分辨率,哪怕牺牲点帧率也可以?

1 2 3 4 5 »