• SK-TDA4VM: 如何使用DSP开发

    Part Number: SK-TDA4VM
    Other Parts Discussed in Thread: TDA4VM

    查看资料SK-TDA4VM开发板不支持RTOS SDK,现在我们需要在SK-TDA4VM板子上开发C66/C71 DSP核相关代码,请教一下是否有相关资料进行指导。希望得到编译调用等相关资料,感谢~

  • SK-TDA4VM: SDK选择

    Part Number: SK-TDA4VM
    Other Parts Discussed in Thread: TDA4VM

    我购买的是SK-TDA4VM,官方提供的是PROCESSOR-SDK-LINUX-SK-TDA4VM  Linux SDK for edge AI applications on TDA4VM Jacinto 但是我想进行MCU开发,但是这个sdk没有mcu开发相关内容,但是其他的sdk官方回答说并不能用于SK-TDA4VM,比如PROCESSOR-SDK-RTOS…

  • SK-TDA4VM: SDK选择

    Part Number: SK-TDA4VM
    Other Parts Discussed in Thread: TDA4VM

    您好

      我购买的是SK-TDA4VM,官方提供的是PROCESSOR-SDK-LINUX-SK-TDA4VM  Linux SDK for edge AI applications on TDA4VM JacintoTm processors SDK,我想使用该套件进行MCU开发,但是似乎需要下载SDK-RTOS包

    于是我在官方文档中发现PROCESSOR-SDK-RTOS…

  • TDA4VM: 搭配OX03C10,在WDR模式下画面全黑

    Part Number: TDA4VM

    现象:出图后,画面黑,只能看见灯光 ,当前曝光增益均在限制的最小值,无法自动变化

    我们在IMX390的驱动上移植的OX03C10的驱动代码

    生成GCC profile的config

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    SENSOR_ID 390
    PRJ_DIR ../imx390_output
    SENSOR_NAME imx390
    SENSOR_DCC_NAME IMX390-UB953_D3
    SENSOR_WIDTH 1920
    SENSOR_HEIGHT 1080
    # 0…
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • TDA4VM: product board output is different from X86 simulation

    Part Number: TDA4VM

    parkNet3dEcoTv_post_ptq_0_tidl_net.binparkNet3dEcoTv_post_ptq_0_tidl_io_1.binpost_input_116.bin
    hello,
        we found the model  output is different between X86 simulation and product board. we share the model and input. we use tidl 0902 to…

  • TDA4VEN-Q1: TDA4VEN底层支持MCAL配置吗,如何获取MCAL配置工具?

    Part Number: TDA4VEN-Q1
    Other Parts Discussed in Thread: TDA4VM

    TDA4VEN底层支持MCAL配置吗,如何获取MCAL配置工具?

    Does the TDA4VM support MCAL(AUTOSAR) configuration at the lower level? How to obtain the MCAL configuration tool?

  • TDA4VM: YOLOV8 分类模型部署报错, 同工程模型切换为检测、分割都无此报错

    Part Number: TDA4VM

    app_create_graph_pre_proc_od done! app_create_graph_tidl done! app_create_graph!
     10984.669661 s:  VX_ZONE_ERROR:[ownContextSendCmd:822] Command ack message returned failure cmd_status: -1
     10984.669706 s:  VX_ZONE_ERROR:[ownContextSendCmd…

  • TDA4VM: IPC between A72 and mcu2_0 send data failed using new added char* type data interface

    Part Number:

    SDK vertion:

    10_00_00_27

    Discription:

    IPC (between a72 and mcu2_0)  when sending and receiving ipc data  add char* type data interface   failed.

    The IPC sending and receiving supported by the TI-supported library only work with data of the…

  • TDA4VM: IMX390点亮两路画面

    Part Number: TDA4VM

    您好,

    我现在在实现两路摄像头画面拼接,由于我只有两个摄像头,所以我暂时点亮两路,请问我为什么输入GStreamer命令后,无画面出现呢?一路摄像头是正常的,支持两路摄像头点亮吗?

    这是我的GStreamer命令,谢谢!

    Fullscreen
    1
    2
    3
    gst-launch-1.0 \
    v4l2src device=/dev/video-imx390-cam0 io-mode=5 ! queue max-size-buffers=1 leaky=2 ! \
    video/x-bayer…
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • TDA4VM: QNX SDK许可

    Part Number: TDA4VM

    TDA4vm和TDA4vh下使用QNX SDK还需要购买商业许可吗?包括开发阶段和商用阶段。如果需要购买,许可可以通过那些渠道获取?

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw Romanian
    Chinese Simplified Hungarian Russian
    Chinese…
  • TDA4VM: IMX390驱动调整AE

    Part Number: TDA4VM

    您好,

    我有个程序要实时修改IMA390驱动中的AE,最终写入到寄存器中,请问我应该调用那个函数,可以达到实时修改AE的效果,谢谢!

  • TDA4VM: TDA4VM的电子眼图工具

    Part Number: TDA4VM

    你好,我在TI官网找到一篇关于电子眼图工具的文章《 适用于 JacintoTM7 系列 的 LPDDR 4 电子眼图工具》,请问该文章中所提及的相应源码文件和工具在哪里可以获取?文章下载链接如下:

    www.ti.com.cn/.../zhcadl8.pdf

  • TDA4VM: 在SK板子上使用RTOS 新增sensor配置时出错

    Part Number: TDA4VM

    我们仅仅希望使用到摄像头相关功能,所以希望在SK上开发,目前出现问题如下:

    我使用0806版本的RTOS SDK,在imaging目录下加了0x08b40以及美信串行接串器的驱动代码。通过vision_app中的 single app进行测试;结果出现如下错误:

    Querying sensor [X8B_CAMERA] ... !!!

    ERROR: Querying sensor [X*B_CAMERA] failed !!!

    appQueryImageSensor…

  • TDA4VM: The problem of using Main domain UART 3 in MCU 1_0

    Part Number: TDA4VM

    Hello,

          I referred to the demo and used PDK for functional development, and I have some problems of using the Main domain uart3 (using rx levle interrupt triger,DMA was not used) in mcu1_0.  (Note: It is possible to read data using…

  • TDA4VM: The MCU1_0 program failed to start properly, and the following error was output: Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted.

    Part Number: TDA4VM

    Regarding the issue in the link below, I tried compiling several programs for MCU1_0, but all of them failed to start. The answer to this problem mentions the need to integrate sciserver. Is there a relevant manual or guide available…

  • TDA4VM: How to use Uart3 MCU in Mcu domain

    Part Number: TDA4VM

    Hello,I want to use Uart3 in main domain(baudRate is 460800,use interrupt mode). Is it possible to use it in the following way?

    1、Set Pinmux V28 UART3_RXD,V29 UART3_TXD

    2、use UART_socSetInitCfg()function set  operMode is UART13x_OPER_MODE…

  • TDA4VM: DA4VM: How to use Main domain I2c in Mcu domain

    Part Number: TDA4VM

    Hello,I want to use Main domain I2c(CSL_I2C2 bitRate 400khz) in Mcu domain. Is it possible to use it in the following way?

    1、Set pinmux  U23 as I2c SCL, U26 as I2c SDA

    2、Preventing access to I2c2 by changing the base address

          #define…

  • TDA4VM: tda4 SPL模式启动MCU1_0应用问题

    Part Number: TDA4VM
    我们使用的是10_00_00_05的BSP和SDK,目前想使用TDA4的SPL启动模式,在MCU1_0上启动can_profile_app_freertos_mcu1_0_debug.xer5f应用。
    请问有什么文档可以参考吗,请指点,多谢!~
  • TDA4VM: TDA4或AM62是否支持RCCG bayer patter raw sensor调试

    Part Number: TDA4VM

    Dear TI experts,

    I have two questions,please help with confirm it,thanks.

    1.Does TDA4 or AM62 platform support RCCG raw sensor ISP tuning by now?

    2.If not support,we develop it by ourself, include driver bring up, ae、demosaic、awb.…

  • TDA4VM: DCC Tuning Tools issue

    Part Number: TDA4VM

    May I ask if DCC Tuning Tools(v3.20) supports j722s-evm-10_00_00_05?

  • TDA4VH-Q1: TDA4VH盒子

    Part Number: TDA4VH-Q1
    Other Parts Discussed in Thread: TDA4VM

    我们公司希望基于TDA4VH以及TDA4VM设计一些产品,我们公司缺少硬件能力,所以希望贵司能推荐一些基于TDA4VH,TDA4VM做的盒子,能直接使用,不需要画PCB板的

  • TDA4VM: 我的RTC时间出现了偏差

    Part Number: TDA4VM

    我目前正在做一项测试工作,测试TDA4VM的RTC时间是否正常,我在测试的过程中,发现了它会出现时间上的偏差,我是使用的"i2ctransfer -f -y 0 w1@0x32 0x00 r7"命令来获取RTC存储的日期及时间,白天的测试是正常的,每次都是到晚上会出现时间异常,其中存储的小时会出现不增反减的现象。

    我讲一下的测试过程:我是用的两个硬件板进行时间的测试,其中时间异常的硬件板简称为181,时间正确的硬件板简称为195,我在195上执行测试脚本…

  • TDA4VM: MIPI CSI_1 RX 软件取帧卡住,有没有排查步骤确定故障点?

    Part Number: TDA4VM

    TI专家:

        你们好!背景如下:

    SDK版本:

    ti-processor-sdk-linux-j7-evm-08_05_00_08

    ti-processor-sdk-rtos-j721e-evm-08_05_00_11

    硬件示意图:

    摄像头规格完全一样,3M 像素,UYVY输出。

    我已经参考 app_multi_cam 例程,实现 4路摄像头 max96724 CSI0输入,通过马赛克 4分屏由 CSI-TX输出。

    现在我希望通过 max9296 从 cam5…

  • AM62A7-Q1: can的波特率设置和采样点位置设置

    Part Number: AM62A7-Q1

    你好,请问这个CAN配置的波特率和采样点是怎么计算的,我采用网上的计算公式计算了一下然后对照CAN 的demo的默认值,得出的跟demo是结果不一样的。还有就是CAN的NBTP寄存器在手册中被忽略了,没有提供具体寄存器的信息,如下文件中内容。

    请求解答(感谢!):

    1、与我按照公式计算值不同,麻烦提供一个按照文件中的配置计算实际波特率和采样点位置的方式公式。

    2、麻烦提供一下NBTP的寄存器相关内容,技术手册中没有相关寄存器的具体内容。

    我的问题.d…

  • J721EXCPXEVM: TDA4VM J721EXCPXEVM SD BOOT 不開機

    Part Number: J721EXCPXEVM
    Other Parts Discussed in Thread: TDA4VM

    Hi 

    我這裡使用 TI J721E + TDA4VM 平台

    要測試 Vision_apps

     

    從 ti 官網下載了 

    ti-processor-sdk-rtos-j721e-evm-10_00_00_05.tar.gz

    ti-processor-sdk-rtos-j721e-evm-10_00_00_05-prebuilt.tar.gz

    照線上 RTOS 的說明…

1 2 3 4 5 »