如题,google player中国上不去,镜像也不能访问
你好:
我在使用LP-XDS110调试版连接CC2745R10-Q1后,电脑无法识别串口指示灯变红。如果只连接XDS110时正常,电脑可以正常识别端口,并且使用XDS110连接CC2340R5也是可以工作的的,电脑能正常识别串口。请问这是什么原因导致的的这个问题?该如何解决。
Hi Team,
CC2541F256RHAR Can you tell me if this model will come with a bluetooth name, we now find it has a different bluetooth name, what is this kind of situation?
Hi,
改用改用8.40版本后,CC2340R5接收200多条手表通知后,就再也接收不到手表的心率通知,怀疑是内存泄露触发了BLE STACK异常。在case ATT_HANDLE_VALUE_NOTI:语句中增加GATT_bm_free((gattMsg_t*)pMsgData, ATT_HANDLE_VALUE_NOTI);后,有时CC2340接收200多条手表心率通知后就再也接收不到了,有时CC2340接收手表1000多条的心率通知后仍可继续接收…
SDK版本:simplelink_lowpower_f3_sdk_8_10_01_02
CCS:Version: 12.7.1.00001
示例:basic_ble_LP_EM_CC2340R5_freertos_ticlang
情况1:
基于basic_ble_LP_EM_CC2340R5_freertos_ticlang示例开发应用程序,当串口收到某些特定字符串时,需要调用osal_snv_write将一些信息保存在flash中,或者调用osal_snv_read从flash中读取信息进行比对校验…
您好,想问一下关于CC2340R5,工程中创建定时器,定时器中断中将MainTaskFunction通过BLEAppUtil_invokeFunction传递给BLEAppUtil_Task,在MainTaskFunction中调用osal_snv_write函数,发现前两次osal_snv_write函数可正常调用,第三次会进入ICall_abort函数导致while(1)无法退出,具
体是由什么原因导致的
void MainTaskFunction…
请问下TI BLE CC2340R52 能做Host 的吗? 可以的话, 它最多能连多少外设?
还请帮忙确认下 客户需要BLE scan 周围蓝牙设备并收集数据, 我们需要确认CC2340 最大连接ble设备数量
有相关的说明资料请提供,谢谢!
您好,自己用CC2340R52E0RGE设计了电路板,图纸如下问题(1)目前下载程序及运行程序都正常,电感L20换的10uh,外部供电VDD_BT=3.3V, VDDD=1.28V正常, 但是DCDC 输出端口VDCDC用万用表测量只有1.49V,跟手册描述的不一样,
,手册里面的是3.0v,低于2。2v会自动切换到LDO,模式,而且例程里面已经开启配置位DCDC模式,
,请问这个问题VDCDC=1.49V的原因是什么?问题(2)用xds110下载程序部正常…
I hope my LP_EM_CC2340R5 will work with coded S8 PHY, but I can only see Coded PHY in syscfg, how can I set it ?
基于CC2340R5+simplelink_lowpower_f3_sdk_8_20_00_119,修改rtos\LP_EM_CC2340R5\ble5stack\basic_ble以接收智能手表的心率通知数据。CC2340R5 Central在接收手表心率通知数据约80-300条之间数量后,无法再接收到心率通知数据。使用手机App 蓝牙调试助手测试,发现智能手表在发送一段时间心率通知数据后,会暂停几十秒钟的时间后,再重新发送心率通知数据,怀疑是不是因为智能手表会暂停心率通知数据发送…
When I use basic_ble in SimpleLink Low Power F3 SDK (8.20.00.119), the Terminal has no print about BLE ID Address.
Hi,
我目前使用SDK8.10,应用修改是基于SDK的示例data_stream。
在syscfg的GUI界面中的部分参数,现在需要蓝牙启动后从串口接收配置参数并修改,例如tx_power和pdu_size,tx_power在hci.h中找到了HCI_EXT_SetTxPowerCmd,但是pdu_size没有找到对应的设置方法。
请问我该如何在蓝牙启动后修改pdu最大值?
Hi,
I need to create a clock product. After the CC2340 connects with a smartphone, how can I get the system time of the phone. It’s not possible to send the time through an app, as we are not developing an app for the product. How…
I want to use the RCT clock for some urgent project tasks and hope to provide a routine soon, thanks
https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/,Android版本链接失效