i find an question talked about CC1352P 20dBm, but the question is locked, and some important link can not be opened, could you pls reopen this link?
i find an question talked about CC1352P 20dBm, but the question is locked, and some important link can not be opened, could you pls reopen this link?
Hello, all
we want use the cc1352P to build our product by it's 20 dBm Tx Power which worked on the 433MHz Frequency.
but i can't find any existing hardware solution on the TI web, just an image like this, ply help me and give…
请教各位开发者,我使用两块CC1352P1_LAUNCHXL搭建 rfAudioTx rfAudioRx测试,使用CCS 加载simplelink_audio_plugin_3_30_00_06里的参考程序,如果用最新的SDK是会提示导入错误的,
1、后来重新下载simplelink_cc13x2_26x2_sdk_5_20_00_52,可又找不到CC1352P1_LAUNCHXL的相关内容,
2、于是继续下载simplelink_cc13x2_26x2_sdk_4_20_00_35这个版本SDK…
你好!
我们目前正在使用TI15.4协议栈中的collector和sensor例程,现在想使用其中的NVS对用户设置参数进行存储,所以想深入了解一下NVS的整个机制,请问有相对应的文档可以进行学习吗?
我有个需求是 要实现1对10个节点的数据通信,1为主10个从
1、主到从大概5Kbps的实际有效数据量
2、每个节点有大概20kbps的实际有效数据量传输到主节点,共200kbps
3、要求整个网络基于主实现时间同步
4、实现跳频功能
5、在复杂电磁环境中实现200m的实际有效距离
6、上电10秒完成整个网络的所有节点链接
7、目前暂定使用433MHZ这个频段,CC1352@20dBm
问:
1、能用TI15.4STACK实现吗? 如果不能可以使用什么方式及思路…
参考设计射频前端模式中,无论使用单端(仅使用RF_P或者RF_N引脚)或差分模式(巴伦将信号旋转90度)都没有采用双工器器件。那么,公共的一个 π/T 型阻抗匹配电路如何同时满足RX和TX两个相反信号方向的阻抗匹配?
在“ Application NoteCC13xx/CC26xx 硬件配置和 PCB 设计注意事项”中,第九页(2.3 CC13xx单端模式)里面,“仅单端TX”和“仅单端RX”中阴角处阻抗不同已经给出,后面如何综合成(方法) TX和RX为一个电路的、单端的实际应用的射频电路?
我們利用CC1352P開發智能穿戴手錶,PCB完成后發現射頻部份不能正常接收及發送,軟件在LAUNCHXL-CC1352P是能正常運行的,估計是射頻部份設計問題,請協助審核原理圖是否出錯
在TI培训中一个视频看到,cc1352p支持在sub1G组网的情况下,同时支持2.4G BLE进行通信,请问具体如何配置和实现?
视频链接TI 15.4 协议栈,以及低功耗远距离传感器到云端解决方案介绍-多协议产品 - 德州仪器(TI)官方视频课程培训 (21ic.com)
rfEchoTx和rfEchoRx的分别会有一个接收信号强度,我用这个接收信号强度为条件,控制一个IO口的输出值作为射频开关的切换条件,当接收信号强度降低一定阈值后,缩短发送时间,并变换IO值,一共进行四次,选择四次中接收信号强度最高的那次IO输出值作为继续正常发送状态的开关值,我对rfEchoTx代码进行了以下改动:
需求:实现射频传输数据时,一个数据包可以达到4KB的大小。
现实:我遍历了所有的RF和easylink例程,发现例程中数据包的大小一般不超过128个字节。与发射有关的指令rfc_CMD_PROP_TX_ADV_t.pktLen的数据类型是uint16_t,也就是说,此值可以被设为4096;同理,与接收有关的指令rfc_CMD_PROP_RX_ADV_t.maxPktLen的数据类型也是uint16_t,也可以被设为4096。
问题:1. 将rfc_CMD_PROP_TX_ADV_t…
1. CC1352P在正常使用过程中,偶尔会发生了RF Core死机的情况,此时如果reset整个设备,一切恢复正常;
2. 但reset整个设备,需要很大的额外开支;
3. 所以,想咨询一下,有没有单独reset RF core的方法?
我在使用CC1352P的时遇到了一个问题,在采用SUB1G模式(设置为:200kbps,50kHz Deviation,2-GFSK,311kHz RX Bandwith),高功率口采用巴伦,低功率口是单端外偏接收,在采用射频线缆连接时,接收灵敏度小于-95dBm,但是用天线发射接收,灵敏度就在-70~-80dBm之间,放在屏蔽箱中测试也是如此。2.4G测试都是正常的。下面是原理图:
TI达人:
collector_sm_CC1352P_4这个工程如何修改管脚?试过只要芯片不带P的工程都没有问题,collector.syscfg这个文件我只要修改为Use Custom Board,编译就会错误!我按照之前的经验,不编译collector.syscfg文件,将ti_devices_config.c、ti_drivers_config.c、ti_radio_config.c等7个文件手动导入引用,我只修改GPIO之类的内容,编译错误更多…
你好,我们量产了一批设备,使用的是CC1352P1F3芯片,主要用到射频传输和UART串口通信。在使用中一段时间后出现个别设备的CC1352P芯片不工作的现象,检查发现:万用表测量芯片的烧录口VCC和GND出现短路,然后单独将CC1352P芯片取下来, 测量发现第44引脚VDDS和GND短路。请问:1、出现短路现象可能是什么原因?2、44引脚VDDS是给CC1352P内部的哪些功能模块供电的?
参考开发板设计的1352P1的射频模块模块工作在200k空速,软件用的SmartRF Studio 7,灵敏度测试能测到-100dbm,但在距离测试时RSSI在-50时就开始出现乱码,开发板测试效果很好rssi在-90时才会有乱码出现,感觉是模块抗干扰能力比开发板差,可能是哪里的问题,
ps,我把信号发生器通过天线接出来,模块也用天线,空旷环境下灵敏度测到-60dbm就有乱码,屏蔽房里能测到-100dbm。
谢谢支持