Other Parts Discussed in Thread: UNIFLASH
我参考swrc330制作了一块CC1310F128RHBR开发板,原理图如下。
关于CC1310的部分我是按照着swrc330的要求设计的,元器件也尽可能按照BOM表进行购买。测试下来射频以及串口这些外设都能正常使用,但却如标题所述,其有着一个奇怪的问题,大体表现为程序可以烧录进芯片,但硬件复位或断电后程序不再运行。
接下来我将描述这个问题的细节。
这块板子在第一次下载时就会在下载进行到某个阶段时报错…
我用的官方的例程 编译后 用XDS110无法下载 是需要配置吗? 报错如下图
Cortex_M4_0: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
CC1310 DEMO板有问题,能否帮忙指导下,怎么维修?现在插上USB后,供电正常,但是U5工作异常,指示灯不亮?芯片也无法识别,是什么原因呢?
新画的板子,芯片CC1310 F128RHBR,调试时会断开连接。
断开错误如下:
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Board Reset Complete.
Cortex_M3_0: Error: (Error…
1. 板子上没有接iic设备时,调用iic接口会卡死,在调试模式是正常的,断开调试器,直接上电会卡死!rfPacketTx_CC1310_LAUNCHXL_nortos_ccs.zip
2.
CC1310 有对应的离线烧录器吗,量产时要怎么烧录大量芯片?
ccs and uniflash can't load progarm on cc1310 launch borad,and use flash program to force mass erase won't help