• CC3551E: 使用CCS12.7.1编译示例工程CC35xx_network_terminal时出现的3条warnings

    Part Number: CC3551E

    你好,

    我按照Quickstart CC35XX User's Guide8.21.00.x里CCS下载和安装及设置步骤之后编译工程时出现了如下三个warning:

    "../linker.cmd", line 107: warning #10068-D: no matching section;

    warning #10247-D: creating output section ".ramVecs" without a SECTIONS…

  • BP-CC3351: tm4c129exl增加wifi

    Part Number: BP-CC3351
    Other Parts Discussed in Thread: CC3351, CC3200, LP-AM243

    我們目前tm4c129exl是使用SPI溝通其他 wifi module

    最近需要更換wifi module,目前有借到BP-CC3351

    我從Mcu CC33XX User's Guide R4看應該同樣用spi與其通訊

    但我未找到SPI通訊協定內容

    請問我要如何進行測試

    另外CC3351是否能像CC3200一樣進行編輯

  • CC3351: cc33xx驱动加载过程中,报错,未成功创建wlan0平台设备。

    Part Number: CC3351

    [ 216.265354] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [ 216.333703] cfg80211: Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
    [ 216.342853] cfg80211: Loaded X.509 cert 'sforshee…

  • CC2564C: 怎么和CE6.0系统连接

    Part Number: CC2564C

    你好!正在用CC2564C连接安卓系统上的蓝牙正常,但与win ce6.0系统的蓝牙2.0(使用的是TI WL1271)连接不上呢,请问下CC2564C哪个参数有关系

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw Romanian
    Chinese Simplified Hungarian
  • CC3235S: 关于SPI通信

    Part Number: CC3235S

    您好,我想知道CC3235S SPI通信过程中数字,SPI接口的电平标准和供电电压,由0-1变换时的电压

    ******************************************************************************************************************************************************************************…

  • CC2564C: Wi-Fi 论坛

    Part Number: CC2564C

    Hi ,

    I want confirm whether the CC2564C 's related stack 

    CC2564CSTBTBLESW  for STM32F4 has already be certificated with Bluetooth 5.1, because our product will use CC2564C and CC2564CSTBTBLESW as a BT 5.1 product.

    this question is…

  • CC3235S: 无效的工程路径:包含路径无法找到

    Part Number: CC3235S
    Other Parts Discussed in Thread: SIMPLELINK-CC32XX-SDK,

    导入官方例程network_terminal出现警告,Invalid project path: Include path not found (E:\CCS_Project\CC32XX_5_30_SDK\simplelink_cc32xx_sdk_5_30_00_08\.;D::\CCS_12_8_1\xdctools_3_62_01_16_core…

  • CC3200-LAUNCHXL: P2P例程无法通过wifi Direct连接手机

    Part Number: CC3200-LAUNCHXL
    Other Parts Discussed in Thread: CC3200SDK, UNIFLASH

    CCS:8.3.0

    SDK:1.5.0,CC3200SDK_1.5.0\cc3200-sdk\example\p2p

    手机型号:华为Mate60

    程序停在这个while中了,例程一点没改,直接debug或者uniflash下载都连接不上,一直显示正在连接,连接一会之后在可用设备列表中,cc3200-p2p-device消失了。请问需要手机进行设置吗…

  • CC3235S: 用CC3235S做了个WIFI的中继器,但是中继器反复链接手机热点后,出现链接失败阻塞,程序不执行,OStimer停止的问题

    Part Number: CC3235S
    Other Parts Discussed in Thread: SYSCONFIG, , UNIFLASH,

    To:大家

       各位好,我现在使用的CPU是CC3235S,原有工程使用的是CCS10.4.0+simplelink_cc32xx_sdk_5_20_00_06+sysconfig_1.8.0+xdctools_3_62_01_15_core,

    工程可以编译通过,程序可以用uniflash_6.4.0烧写到板子上并执行。但是板子链接自己手机的无线网络时…

  • CC3220S: 我使用官方範例 tcpecho build 的時候出現問題

    Part Number: CC3220S
    Other Parts Discussed in Thread: SYSCONFIG

    subdir_rules.mk:9: recipe for target 'build-67265087' failed
    Error: Exception occurred calling addInstance()

    **** Build of configuration MCU+Image for project tcpecho_CC3220S_LAUNCHXL_freertos_ticlang…

  • WL1837MOD: SDIO output timing

    Part Number: WL1837MOD

    Is Response and output data sampled during clock fall edge on default speed mode?

    how to set sample edge to rise edge?

  • CC3235S: 固定IP设置

    Part Number: CC3235S

    请问CC3235S以STA模式工作,在通过SSID连接到网络前,可否给CC3235S设置一个固定IP地址呢?

  • CC3220SF-LAUNCHXL: CC3220SF的与移动设备无法连接

    Part Number: CC3220SF-LAUNCHXL
    Other Parts Discussed in Thread: CC3220SF

    CC3220SF一直显示有AP接入点模式初始化无法连接,在连接之后点击start显示failed无法连接,提示ap接入点模式错误

  • CC3220R: MQTT无法连接,报错

    Part Number: CC3220R

    如图所示,SDK使用的版本为5.30.0.08版本,连接MQTT服务器时出现错误码-2005,请问这个错误码代表的是什么意思?我该如何修改我的工程?

  • CC3235S: CC3235S PCB铺铜

    Part Number: CC3235S

    如下图所示,CC3235 Launchpad的PCB在蓝色线圈出的区域中并未铺铜,请问这里为什么不需要铺铜?

  • CC3235SF: 关于cc3235 RTOS线程

    Part Number: CC3235SF

    我使用CC3235SF的SPI SLAVE 例程发现,每次接收 主机的数据 时间间隔是2MS 一次,这个2MS 在这里是默认的RTOS 的轮询功能吗?  怎么改成RTOS 的

    SCHED_FIFO 模式?
  • CC3235MODS: 初始上电的Reset波形不满足规格书要求

    Part Number: CC3235MODS

    问题:初始上电的Reset波形无法满足规格书要求,是需要客户处理(如并联大电容)满足此要求还是模组本身已满足要求?

    实测初始上电的rest 波形如下图所示:

      

    规格书要求:

  • CC3100MOD: 例程Lab_cc3100例程错误

    Part Number: CC3100MOD
    Other Parts Discussed in Thread: CC3100, , CC3135, CC3120, CC3200, CC3120MOD, BOOSTXL-CC3120MOD

    板子是MSP432P401R,用的例程是Lab20_cc3100,在运行时,configureSimpleLinkToDefaultState函数,返回数值-100

  • CC3220SF: SPI传输和Socket传输同时进行容易触发SL_DEVICE_EVENT_FATAL_DRIVER_ABORT

    Part Number: CC3220SF

    您好!

          我有一个程序,开了两个线程,A线程发起SPI传输Master,20000000Mhz,Block方式,SPI传输完成后通知B线程发起Socket传输,同时A线程再启动一次SPI传输。

    这样很容易引发SL_DEVICE_EVENT_FATAL_DRIVER_ABORT错误,查不到任何文档说明这样使用有冲突。

    当我在一个线程里按顺序使用SPI和Socket就不会有这个问题,但这样无法完全利用网络带宽,只能是SPI和Socket并发才能提高效率…

  • CC3220SF-LAUNCHXL: UART2_read或UART2_readTimeout都收不到UART2_STATUS_ECANCELLED

    Part Number: CC3220SF-LAUNCHXL

    环境:simplelink_cc32xx_sdk_6_10_00_05

    CCS Version: 12.2.0.00009 

    UART2,BLOCKING模式下,A线程调用UART2_readCancel,B线程UART2_read或UART2_readTimeout都收不到UART2_STATUS_ECANCELLED,UART2_readTimeout可以收到UART2_STATUS_ETIMEOUT

    void uart2_in…
  • WL1807MOD: WL1807MOD的特性

    Part Number: WL1807MOD

    请问TI的工程师一个问题:我现在需要在一个10000平的空间桥接多个WIFI基站,然后终端在这个空间内移动。当终端和当前链接基站的信号强度较低时,切换至下一个信号强度合适的基站,并与之通信。请问TI WIFI模块的这个切换时间是多少?

    谢谢!

  • LAUNCHXL-CC3235SF: 关于OTA的问题

    Part Number: LAUNCHXL-CC3235SF
    Other Parts Discussed in Thread: CC3235SF, CC3200, UNIFLASH

    我想使用Internal Update方式进行OTA,但是不知道如何将.tar文件写入到SimpleLink文件系统,以前的CC3200项目是通过tcp接收bin文件原始数据通过sl_FsWrite()写入文件系统,更改mcubootinfo重启MCU,这样很方便就完成了OTA,现在使用CC3235SF也能这样操作吗…

  • CC3235S: 关于out of box例程,该例程中为什么读出的加速度x轴数据、加速度y轴数据、加速度z轴数据都是-1呢?

    Part Number: CC3235S

    尊敬的TI工程师您好

    我是LAUNCHXL-CC3235S,我烧录的使out of box 例程,我在代码中设置了断点,经编译查看,读出的加速度x轴数据、加速度y轴数据、加速度z轴数据为什么都是-1呢?

  • CC3235MODSF: SPI主机模式下,启动TX和RX通道DMA,调用sl_send后卡死

    Part Number: CC3235MODSF
    Other Parts Discussed in Thread: CC3200, CC3200MOD

    CC3235MODSF开发板,SPI采用master模式,数据宽度两个字节,发射和接收通道都连接上DMA,双DMA通道,用的tirtos系统上跑WIFI-AP模式,调用sl_Recv接收上位机数据通过DMA到SPI发射出去,SPI DMA接收到的数据通过sl_Send发送到上位机。问题来了,当我发送和接收的数据包很小的时候没有问题,整个过程很流畅…

  • CC3200: CC3200的下载问题

    Part Number: CC3200

    你好:

             我看了CC3200的官方的板子原理图里面使用UART下载的管脚是连接的PIN55(CC_GPIO_01)(UART0_TX)和PIN57(CC_GPIO_02)(UART0_RX),是不是也可以使用PIN53(CC_GPIO_30)(UART0_TX)和PIN45(GPIO31)(UART0_RX)?使用的时候需要注意什么?

1 2 3