Other Parts Discussed in Thread: PCM5142, , PCM5242
hello
We found that when using PCM1860 and PCM5142, the output audio amplitude of PCM5142 decreased by half compared to the input audio amplitude when the output was set to 0dB. Both…
新增加的R228和R229这两个电阻可以把偏置电压上拉到-0.2V,不知道会不会有什么影响?
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hungarian | Russian |
Chinese Traditional | Indon… |
你好,我想请问一些关于TLV320ADC5120的技术实现问题, 我们在使用TLV320ADC5120做音频产品设计时,有一些技术我们并不确定。
1、我们希望 能使用TLV320ADC5120做ADC输入检测,既:当我的设备长时间无音频输出时,我希望TLV320ADC5120能做延时检测长时间无输入时进入省电休眠,当外部有输入时能唤醒。这两者是否可以实现,或者我能从一些寄存器配置中能获取输入状态…
现在我们3104做一块核心板,线性差分输入到差分输出,如图是原理图和PCB:
用AP做音频测试,测试出来只有72dB的信噪比,采样率是22050,麻烦帮忙看一下如何做才能提高信噪比到92dB
我现在遇到了个问题,我TLV320ADC3140设置的4通道,I2S-32bit数据传输格式,我STM32H7单片机这边也是设置的32位采样,但是我这边采样到的数据一个32位数据里面却是通道一和通道二的数据且两个通道的数据都是16位的。下面我展示一下我的配置。
TLV320ADC3140:配置如下:
模拟音频差分输入,IN M为什么也需要接上拉偏置?以前项目是接电阻下地
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hungarian | Russian |
Chinese Traditional | Indonesian |
I'm currently using an STM32F407ZGT6 to control a TLV320ADC5140 using SPI communication to receive audio using I2S, but I'm unable to capture the audio data. Acquisition method: analog dual channel input。
STM32 as host…
1、一个AES音频信号的处理需求,接口输入输出采用XLR的平衡方式,请问在输入和输出部分如果不使用音频的变压器的话,如下的设计是否正确?2、如果不使用音频变压器的话,是否需要ESD防护器件,有没有推荐的型号?
I used STM32L431 as the master to receive audio signals from TLV320. The test found that the trend of the data is right, as the input becomes larger, the output also becomes larger. But the amplitude of the signal seems to…
TPA3255是否可以AB通道输入的音频信号由AB输出通道输出,CD通道输入的音频信号由CD输出通道输出。即两路互不影响,可独立使用。
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hungarian | Russian |
Chinese… |
想請教一下DSP Sub address read/write問題,我們有看過data sheet 試著切換book 和page.
nvidia@tegra-ubuntu:~$ sudo i2cset -f -y 0 0x2c 0x00 0x00 切換到page0
PCM1809芯片做主时钟,BCLK(6.1M)和LRCLK(96K)输出正常,但是DATA无输出,麻烦帮忙协助分析一下;
1、IOVDD和AVDD供电正常均为3.3V;
2、14引脚:1.5V电压正常;
3、16引脚:3.3V电压正常;
4、17引脚:1.8V电压正常;
5、18引脚:2.6V电压正常
Recently we received three customer claims, and we noticed that the 6584 powerstage was not working propery due to loss of 12c communication.And we further noticed that the loss of l2c communication happened right after a chip…
Hi TI team,
In a project, when the TAS6584 module is in normal playback mode, if the speaker is short circuited or open circuited, the detection status of registers 0xC0 and 0xC1 will not be updated in real time. TAS6584…
电视通过HDMI线连功放,ARC传音频,EP950接收,输出SPDIF到PCM9211.有些电视连接时,功放会出现声音断续。帮忙看看是否有碰到这个问题,谢谢!
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hungarian | Rus… |
你好,我使用tlv320aic3204的DAC模块,通过I2S作为DAC的数据源,LOL和LOR作为输出。测试过程中发现输入正弦波时,启动传输瞬间,波形叠加了一个渐变的直流分量(如图),然后才趋于稳定。请问怎么解决启动传输时存在的这个直流分量?
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong… |
你好,我们使用的3104EVM-K底板为AC-MODEVM,接usb上点后,MCLK一直为高电平,请问这是哪里的问题,如何调整让MCLK有信号,谢谢
另外一个问题,在打开pc软件 AIC310X EVM GUI后,其中register table中page 0没有register3,而这个寄存器在page 1中显示,同时这个寄存器通过command line interface无法修改。这个问题通过修改register map.csv中register3的register…
想要通过PCM2912A实现拥有PTT功能的USB麦克风,芯片的USER GUIDE给到的电路是将mute引脚通过开关连接到SSPND上,这样默认为是开启的,按下后静音,如果需要实现PTT功能,就需要信号是反向的,这个有办法实现吗,该怎么更改,或者有其他芯片能实现这个功能吗
我下载官方的OPA1622仿真模型,并使用TINA TI仿真,根据数据表,连接成单位增益,接入1nf负载然后并联2K负载电阻,发现相位裕度在25.6度而不是数据表中的0度,偏高25度,与数据表不符。
我们计划在产品中使用2个woofer和2个tweeter,共四个喇叭。其中,2个woofer用一个TAS5825M功放,2个tweeter用另一个TAS5825M功放。如下图所示:
我们手头硬件只有Purepath控制台母版1PCS 和TAS5825M-SB 1pcs。请问能否使用上面的硬件来调节整机系统?即先调节2个woofer,然后再调节2个tweeter。
以上,多谢!