• USB-TO-GPIO2: 与USB2ANY是一样的工具吗,能否同时用于电源和时钟芯片的配置

    Part Number: USB-TO-GPIO2
    Other Parts Discussed in Thread: LMK05318, TPS53667

    需要调试的有PMBUS的电源控制器比如TPS53667和时钟芯片如LMK05318,两者介绍中分别用了这两款,买其中一个行不行呢

  • RE: ADC12DJ5200-SP: 数据转换器论坛

    Other Parts Discussed in Thread: LMK04828, LMX2594, LMK04832, USB2ANY, TUSB3410

    谢谢,Danie!

    LMK04828输出时钟能实现上面的框图吗?有两路SDCLKoutput7和9输出40.625M,DCLKoutput输出260M,看规格书SDCLK和DCLK是一样的输出频率?

    TICS pro能导出功能文件直接烧录芯片吗?还是在线操作寄存器?

    时钟原理图帮忙review,能方便提供联系方式吗?我是上海橙科微王小秋,13917788754…

  • LMX2595EVM: FPGA控制外部spi设备

    Part Number:  LMX2595EVM
    Other Parts Discussed in Thread: USB2ANY, LMX2595

    如图,我想通过fpga控制lmx2595evm,其通讯协议是spi,众所周知,spi协议有四个端口:clk,miso,mosi,ss,但lmx2595evm的spi接口共有10个针脚,这10个针脚是一些什么信号?我该向这些针脚中发送什么数据?感谢回答。

  • LMX2595EVM: python控制usb2any

    Part Number: LMX2595EVM
    Other Parts Discussed in Thread: USB2ANY

    我想用python控制usb2any,在网上搜索后得到的关于usb2any的资料很少,是否有官方的usb2any函数库?

  • LMX2595EVM: python或FPGA控制lmx2595evm

    Part Number: LMX2595EVM
    Other Parts Discussed in Thread: USB2ANY

    控制lmx2595evm,写入寄存器值的常用方法是使用TICS Pro软件控制,请问我是否可以通过python或者FPGA直接与evm通信来控制

  • LMK05318B: LMK05318B 输出1PPS 信号 无法与参考输入跟随问题

    Part Number: LMK05318B
    Other Parts Discussed in Thread: USB2ANY,

    根据TICS-PRO 配置该芯片输出1PPS 输出,secRef输入1PPS信号,芯片一直无法锁定secRef输入,输出与输入无法跟随问题,应该如何解决?另外芯片OUT1 输出的 25MHz的时钟信号,波形较垃圾,不光滑

  • CDCE6214: 配置的软件和信息请教

    Part Number: CDCE6214
    Other Parts Discussed in Thread: USB2ANY, CDCI6214,

    工程师你好:

           我们想配置CDCE6214,使用的是USB2ANY,软件使用的是TICS Pro  v1.7.6.2,请问是否正确?

           因为在“Select Device”里,没有看到CDCE6214,是不是选CDCE6214-Q1代替呢?

           试了一下,输出不正确,请帮忙确认下,感谢!

  • LMX2595: deterioration in phase noise

    Part Number: LMX2595
    Other Parts Discussed in Thread: USB2ANY

    Hello

    I'm using an lmx2595 in my circuit and have made a evaluating module using the EVM as a reference. Some changes have also been made to simplify the module, and these changes have caused…

  • CDCE813-Q1: 用于PCLK jitter cleaner功能的寄存器配置

    Part Number: CDCE813-Q1
    Other Parts Discussed in Thread: CLOCKPRO, CDCE913-Q1, CDCE913, , USB2ANY

    你好

    我们在使用CDCE813 用于PCLK jitter cleaner功能时,需要修改哪些寄存器的值,请帮忙给出 感谢

    宏伟

  • LMK61E2: LKM61E2-EVM setting

    Part Number: LMK61E2
    Other Parts Discussed in Thread: USB2ANY, TICSPRO-SW,

    When I use 100MHz or 50MHz or 10MHz, it didn't have waveform output.

    But I  use 100.01MHz, it has waveform output.

    Please tell me the reason, thank you.

  • LMK04133EVAL: 关于锁相问题及与USB2ANY的连线问题。

    Part Number: LMK04133EVAL
    Other Parts Discussed in Thread: LMK04133, LMK04033, USB2ANY, , LMK05028

    TI相关工程师,您好!

    最近在使用LMK04133评估板进行功能测试,有如下疑问烦请答复:

    1.LMK04133是否有内部EEPROM可供程序烧写?如果没有,这款芯片常规是如何使用呢?外围电路都需要进行哪些配置?

    2.目前我在TICS上进行寄存器配置,使能POWERDOWN之后再重新给电,观察到输出信号频率是我设置的600kHz…

  • CDCE6214-Q1: CDCE6214-Q1工厂烧录问题

    Part Number: CDCE6214-Q1
    Other Parts Discussed in Thread: CDCE6214, USB2ANY

    你好! 这边买过CDCE6214-Q1_EVM验证完成了,但是这个demo板是通过USB烧录的,想问下工厂加工时CDCE6214-Q1如何烧录?

  • LMK05318BEVM: Tics pro无法识别到该开发板

    Part Number: LMK05318BEVM
    Other Parts Discussed in Thread: LMK05318, USB2ANY

    第一次usb连接时,tics提示升级开发板,升级过程中,vm虚拟机识别到了设备进行了打断,导致Tics pro再也无法识别到开发板,不知有何解决方法

  • LMX2820EVM: USB2ANY 固件升级问题

    Part Number: LMX2820EVM

    问题已解决。

  • CDCE6214-Q1: CDCE6214RGER

    Part Number: CDCE6214-Q1
    Other Parts Discussed in Thread: USB2ANY

    请问TICS Pro中,FTDI的这个模式可用嘛?我们的设计是用的FTDI的芯片实现USB与I2C通信的,谢谢

  • CDCE6214-Q1: CDCE6214RGER

    Part Number: CDCE6214-Q1
    Other Parts Discussed in Thread: USB2ANY,
    1. CDCE6214-Q1配置信息下载一定需要USB2ANY接口板嘛?是不是只要能正确识别I2C地址信息就可以用TICS Pro软件配置啦。
    2. CDCE6214-Q1在第一次用没有下载配置的情况,外部25M单端时钟输入,上电默认有时钟输出嘛?
  • LMX2592EVM: LMX2592重大漏洞

    Part Number: LMX2592EVM
    Other Parts Discussed in Thread: LMX2592, USB2ANY

    目前做项目用到LMX2592芯片,在网上买了第一块评估版,第一天都是好的,芯片也能出频率和幅度;第二天评估版就不能出频率和幅度;又从官网上买了第二块LMX2592的评估版,刚拿回来的时候,用不同电脑运行TICS PRO软件提示更新USB2ANY,更新了其中一台电脑,然后评估版能正常工作。上午都能正常工作,下午突然不能正常工作了,检查也无明显错误,用没有更新USB2ANY的电脑…