Dear team,
Customer TDK (sold to 186237) is claiming that they received Order Push data on 11/05 that they did not expect, but I cannot find log on our side.
Below is log on customer side.
Could you please investigate if we have sent data to them?
API Request Header1
Order push notification
https://iris-connect.jp/api/ti/order-push
・2024/11/05 11:56:34
・2024/11/05 14:53:19
・2024/11/05 16:03:42
・2024/11/05 16:03:56
・2024/11/05 16:03:58
Do you have the order number? The link can't be opened, thank you.
Hi Xiaonan, customer does not have order number either. They are saying it is erroring out so they cannot see the data. Could you please check the Push log for TDK?
hi Ayumi, may I confirm it's the test environment data?
Yes, it is test environment data.
Hi Xiaonan, Could you please check the raw data? Customer is claiming that they are getting data with GET by push API and it is erroring out.
Customer cannot receive the data due to request header error so they do not have the order#.