This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前在开发一款基于ATMEL ARM9的 9x35的应用,之前使用SDRAM 16-data 于8080接口的LCD公用信号,中间使用76lvth16245,信号两边均为3.3V, 功能这个正常。
后切换为DDR2,将buffer更换为 sn74alvc164245,实现1.8V 到 3.3V转换。 但发现数据无法正常转发到3.3V一侧。导致无法点亮 LCD.
说明:ATMEL 9x35支持SMC /SDRAM/DDR2 这些总线。 发送LCD数据时,会切换成SMC控制器。
sn74alvc164245应该的VCCA最小2.3V,VCCB最小为3V,所以通常使用这款是进行2.5V,3.3V和5V这几种常用电平转换的。
所以这款不能用在1.8V到其他电平转换上。