• ISO1050: TXD波形不正确,无法正常通信

    Part Number: ISO1050

    我使用280049和ISO1050DUBR进行CAN通信测试。

    在使用其他CAN芯片进行测试时可以正常通信,但使用ISO1050DUBR时无法正常通信。

    使用ISO1050DUBR测试时的TXD引脚波形

    测试电路原理图

    CAN通信的软件设置使用其他CAN芯片验证过,可以正常通信。

  • ISO7720-Q1: ISO7720 can't cooperate with TCAN1042

    Part Number: ISO7720-Q1
    Other Parts Discussed in Thread: ISO7720, ISO7721

    I want to use ISO7720 to transfer CAN signal with TCAN1042, but the TX signal cannot transfer right signal while the MCU's CAN signal works well with TCAN1042, yellow:TX    blue…

  • ISOW1412: 是否支持 MCU UART 转 CAN?或者哪个可以?

    Part Number: ISOW1412
    Other Parts Discussed in Thread: ISO1044, TCAN4550

    1、项目需要 UART 转 CAN 通讯,带隔离,查到 ISOW1412 有 MCU TXD/RXD,不确定是否是 UART 的 TXD/RXD 还是 CAN 的,规格书里边并没有描述。

    2、帮忙推荐 UART 转 CAN FD IC 或者 设计,最好 >=1Mbps。如果没有这么高的,也可以 500Kbps 。

  • ISO1042: CAN DC Bus Fault Protection Voltage: ±70 V

    Part Number: ISO1042

    规格书中的DC Bus Fault Protection Voltage: ±70 V,这具体的解释是什么?

  • ISO1042: 请问vcc1为5v,vcc2为3.3v,can收发器可以正常工作吗

    Part Number: ISO1042

    canl和canh是3.3v供电,能否转成5v供电的rx和tx呢,二者如果电压不同,会出现错误吗?

  • ISO1042-Q1: ISO1042-Q1

    Part Number: ISO1042-Q1

    hello:

    At present, there is a demand to be realized through the CAN bus. We use the standard can. We hope to make a switch by judging whether the can signal from the OBD port comes out. We can sample the level on can-h and can…