This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28379D:TMS320F28379D

Guru**** 2529080 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1313801/tms320f28379d-tms320f28379d

器件型号:TMS320F28379D

大家好、我的 ePWM 有问题、我同时启动它们、但 PWM1与 PWM2和 PWM3有异步、我没有发现 我的错误您知道我的错误在哪里吗?

图 Ehe PWM 应该是50/50的、黄色是 PWM1和绿色 PWM2。 PWM3与 PWM2相同;

GpioCtrlRegs.GPACSEL1.all = 0x00222222;
GpioCtrlRegs.GPACSEL2.all = 0x00000000;



CpuSysRegs.PCLKCR0.bit.GTBCLKSYNC = 0; // Stop all the TB clocks
EDIS;



ClkCfgRegs.PERCLKDIVSEL.bit.EPWMCLKDIV = 0;

// // EPWM Module 4 config
PWM1.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Up count mode
PWM1.TBPHS.bit.TBPHS = 0; // Set Phase register to zero
PWM1.TBCTL.bit.PHSEN = TB_DISABLE; // Master module
PWM1.TBCTL.bit.PRDLD = TB_SHADOW;
PWM1.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // Sync down-stream module
PWM1.TBCTL.bit.HSPCLKDIV = TB_DIV1; //(int) PWM_CLK_PRESCALER/4;// High Speed Time-base Clock Prescale Bits 1
PWM1.TBCTL.bit.FREE_SOFT = 2; // Emulation Mode Bits = Free run
PWM1.AQCTLA.all = AQ_NO_ACTION; // clear AQ events
PWM1.AQCTLB.all = AQ_NO_ACTION; // clear AQ events
PWM1.AQCTLA.bit.CAU = AQ_SET; // force EPWM1A HIGH when counter equals CMPA and counts up
PWM1.AQCTLA.bit.CBU = AQ_CLEAR; // force EPWM1A HIGH when counter equals CMPB and counts up
PWM1.AQCTLB.bit.CAU = AQ_SET; // force EPWM1B LOW when counter equals CMPA and counts up
PWM1.AQCTLB.bit.CBU = AQ_CLEAR; // force EPWM1B HIGH when counter equals CMPB and counts up
PWM1.DBFED.all = PWM_TOTZEIT_CNT; // Falling Edge Delay
PWM1.DBRED.all = PWM_TOTZEIT_CNT; // Rising Edge Delay
PWM1.DBCTL.bit.IN_MODE = 2;
PWM1.DBCTL.bit.POLSEL = 2; // Active high complementary (AHC) mode. EPWMxB is inverted
PWM1.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // Dead-band is fully enabled for both rising-edge delay on output EPWMxA and falling-edge delay on output EPWMxB
PWM1.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
PWM1.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
PWM1.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR=Zero
PWM1.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR=Zero
PWM1.TBPRD = (int) (periode_us * PWM_FREQUENZ_IN_MHz);

PWM1.ETSEL.all = 0x0009; // Interrupt für Kurz-Task
PWM1.ETPS.all = 0x0001; // Interrupt für Kurz-Task

// //========================
// // EPWM Module 5 config
PWM2.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Up count mode
PWM2.TBPHS.bit.TBPHS = 0; // Set Phase register to zero
PWM2.TBCTL.bit.PHSEN = TB_ENABLE; // Slave module
PWM2.TBCTL.bit.PRDLD = TB_SHADOW;
PWM2.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
PWM2.TBCTL.bit.HSPCLKDIV = TB_DIV1;// (int) PWM_CLK_PRESCALER/4;// High Speed Time-base Clock Prescale Bits 1
PWM2.TBCTL.bit.FREE_SOFT = 2; // Emulation Mode Bits = Free run
PWM2.AQCTLA.all = AQ_NO_ACTION; // clear AQ events
PWM2.AQCTLB.all = AQ_NO_ACTION; // clear AQ events
PWM2.AQCTLA.bit.CAU = AQ_SET; // force EPWM2A HIGH when counter equals CMPA and counts up
PWM2.AQCTLA.bit.CBU = AQ_CLEAR; // force EPWM2A HIGH when counter equals CMPB and counts up
PWM2.AQCTLB.bit.CAU = AQ_SET; // force EPWM2B LOW when counter equals CMPA and counts up
PWM2.AQCTLB.bit.CBU = AQ_CLEAR; // force EPWM2B HIGH when counter equals CMPB and counts up
PWM2.DBFED.all = PWM_TOTZEIT_CNT; // Falling Edge Delay
PWM2.DBRED.all = PWM_TOTZEIT_CNT; // Rising Edge Delay
PWM2.DBCTL.bit.IN_MODE = 2;
PWM2.DBCTL.bit.POLSEL = 2; // Active high complementary (AHC) mode. EPWMxB is inverted
PWM2.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // Dead-band is fully enabled for both rising-edge delay on output EPWMxA and falling-edge delay on output EPWMxB
PWM2.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
PWM2.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
PWM2.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR=Zero
PWM2.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR=Zero
PWM2.TBPRD = (int) (periode_us * PWM_FREQUENZ_IN_MHz);


// //========================
// // EPWM Module 6 config
PWM3.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Up count mode
PWM3.TBPHS.bit.TBPHS = 0; // Set Phase register to zero
PWM3.TBCTL.bit.PHSEN = TB_ENABLE; // Slave module
PWM3.TBCTL.bit.PRDLD = TB_SHADOW;
PWM3.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
PWM3.TBCTL.bit.HSPCLKDIV = TB_DIV1;// (int) PWM_CLK_PRESCALER/4;// High Speed Time-base Clock Prescale Bits 1
PWM3.TBCTL.bit.FREE_SOFT = 2; // Emulation Mode Bits = Free run
PWM3.AQCTLA.all = AQ_NO_ACTION; // clear AQ events
PWM3.AQCTLB.all = AQ_NO_ACTION; // clear AQ events
PWM3.AQCTLA.bit.CAU = AQ_SET; // force EPWM3A HIGH when counter equals CMPA and counts up
PWM3.AQCTLA.bit.CBU = AQ_CLEAR; // force EPWM3A HIGH when counter equals CMPB and counts up
PWM3.AQCTLB.bit.CAU = AQ_SET; // force EPWM3B LOW when counter equals CMPA and counts up
PWM3.AQCTLB.bit.CBU = AQ_CLEAR; // force EPWM3B HIGH when counter equals CMPB and counts up
PWM3.DBFED.all = PWM_TOTZEIT_CNT; // Falling Edge Delay
PWM3.DBRED.all = PWM_TOTZEIT_CNT; // Rising Edge Delay
PWM3.DBCTL.bit.IN_MODE = 2;
PWM3.DBCTL.bit.POLSEL = 2; // Active high complementary (AHC) mode. EPWMxB is inverted
PWM3.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // Dead-band is fully enabled for both rising-edge delay on output EPWMxA and falling-edge delay on output EPWMxB
PWM3.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
PWM3.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
PWM3.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR=Zero
PWM3.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR=Zero
PWM3.TBPRD = (int) (periode_us * PWM_FREQUENZ_IN_MHz);



// ##### set to CPU2 ################

EALLOW;
DevCfgRegs.CPUSEL0.bit.EPWM1 = 1;
DevCfgRegs.CPUSEL0.bit.EPWM2 = 1;
DevCfgRegs.CPUSEL0.bit.EPWM3 = 1;
EDIS;

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Raphael、

    我看到您在配置 ePWM 之前将 GTBCLKSYNC 位设置为0。 配置 ePWM 后、您是否也将此位设置为1? 这应该会同时启动 ePWM 时钟。

    您也可以按照 F2837xD TRM 时基时钟同步部分中所述、执行相同的使用 TBCLKSYNC 位(如果这用于一个 CPU 子系统):

    以下是 TRM 中针对这些位的寄存器说明、以供参考:

    此致、

    艾里森