This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
根据 DP83867IS 数据表、所有 starp 引脚都具有9K 下拉电阻器。
在定制电路板中、我们将 PHY 地址配置为3 (0011)。我们将 RXD0引脚连接到 Rhi-2.49K 和 RLo-Open (用于配置模式4)、并将 RXD2引脚连接到 Rhi-Open 和 RLo-Open (用于配置模式0)。
当我们在 RXD0线另一端 Rhi 处测量电压时、预期电压为1.958V。我们在该引脚处测量了0。如果我们读取0X006E 寄存器、它始终保持为零。
请引导我解决此问题。