This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
仿真环境为matlab2018a,CCS9.3.
Simulink配置参数如下:
Build结束时,报错如下:
<Linking>
"### Created: ../CF_4wD_VCU_0513.out"
"### Invoking postbuild tool "Hex Converter" on "../CF_4wD_VCU_0513.out"..."
C:/PROGRA~3/MATLAB/SUPPOR~1/R2018a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/hex2000 -i "../CF_4wD_VCU_0513.out" -o "../CF_4wD_VCU_0513.hex" -order MS -romwidth 16 -q
"### Done Invoking postbuild tool "Hex Converter" ..."
"### Successfully generated all binary outputs."
D:\03_Project\CF_VCU\0513Test\CF_4wD_VCU_0513_ert_rtw>exit /B 0
"### Invoking postbuild tool "Download" ..."
C:/ti/ccs930/ccs/ccs_base/SCRIPT~1/bin/dss.bat C:\PROGRA~3\MATLAB\SUPPOR~1\R2018a\toolbox\target\SUPPOR~1\tic2000/CCS_CO~1/RUNPRO~1.JS C:\PROGRA~3\MATLAB\SUPPOR~1\R2018a\toolbox\target\SUPPOR~1\tic2000/CCS_CO~1/F28335~2.CCX ../CF_4wD_VCU_0513.out
*** User inputs:
Target Configuration: C:\PROGRA~3\MATLAB\SUPPOR~1\R2018a\toolbox\target\SUPPOR~1\tic2000/CCS_CO~1/F28335~2.CCX
Program Name: ../CF_4wD_VCU_0513.out
Board Name: unspecified (connect to first board)
CPU Name: unspecified (connect to first CPU)
*** Starting debug session...
*** Debug Session Name: Texas Instruments XDS100v1 USB Emulator_0/C28xx
*** Board Name: Texas Instruments XDS100v1 USB Emulator_0
*** CPU Name: C28xx
*** Connecting to target...
SEVERE: C28xx: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may be one or more of: no XDS100 is plugged in, invalid XDS100 serial number, blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the XDS100 can be located. (Emulation package 8.4.0.00006)
SEVERE: emulation failure occurred
SEVERE: Error connecting to the target: emulation failure occurred
SEVERE: Cannot perform operation, target is not connected.
SEVERE: Error reseting target: Cannot perform operation, target is not connected.
org.mozilla.javascript.WrappedException: Wrapped com.ti.ccstudio.scripting.environment.ScriptingException: Error reseting target: Cannot perform operation, target is not connected. (C:\PROGRA~3\MATLAB\SUPPOR~1\R2018a\toolbox\target\SUPPOR~1\tic2000/CCS_CO~1/RUNPRO~1.JS#93)
at org.mozilla.javascript.Context.throwAsScriptRuntimeEx(Context.java:1693)
at org.mozilla.javascript.MemberBox.invoke(MemberBox.java:160)
at org.mozilla.javascript.NativeJavaMethod.call(NativeJavaMethod.java:204)
at org.mozilla.javascript.optimizer.OptRuntime.callProp0(OptRuntime.java:119)
at org.mozilla.javascript.gen.c1._c0(C:\PROGRA~3\MATLAB\SUPPOR~1\R2018a\toolbox\target\SUPPOR~1\tic2000/CCS_CO~1/RUNPRO~1.JS:93)
at org.mozilla.javascript.gen.c1.call(C:\PROGRA~3\MATLAB\SUPPOR~1\R2018a\toolbox\target\SUPPOR~1\tic2000/CCS_CO~1/RUNPRO~1.JS)
at org.mozilla.javascript.ContextFactory.doTopCall(ContextFactory.java:340)
at org.mozilla.javascript.ScriptRuntime.doTopCall(ScriptRuntime.java:2758)
at org.mozilla.javascript.gen.c1.call(C:\PROGRA~3\MATLAB\SUPPOR~1\R2018a\toolbox\target\SUPPOR~1\tic2000/CCS_CO~1/RUNPRO~1.JS)
at org.mozilla.javascript.gen.c1.exec(C:\PROGRA~3\MATLAB\SUPPOR~1\R2018a\toolbox\target\SUPPOR~1\tic2000/CCS_CO~1/RUNPRO~1.JS)
at org.mozilla.javascript.tools.shell.Main.evaluateScript(Main.java:503)
at org.mozilla.javascript.tools.shell.Main.processFileSecure(Main.java:425)
at org.mozilla.javascript.tools.shell.Main.processFile(Main.java:391)
at org.mozilla.javascript.tools.shell.Main.processSource(Main.java:382)
at org.mozilla.javascript.tools.shell.Main.processFiles(Main.java:179)
at org.mozilla.javascript.tools.shell.Main$IProxy.run(Main.java:100)
at org.mozilla.javascript.Context.call(Context.java:528)
at org.mozilla.javascript.ContextFactory.call(ContextFactory.java:450)
at org.mozilla.javascript.tools.shell.Main.exec(Main.java:162)
at com.ti.ccstudio.apps.internal.scripting.RunScript$1.run(RunScript.java:89)
Caused by: com.ti.ccstudio.scripting.environment.ScriptingException: Error reseting target: Cannot perform operation, target is not connected.
at com.ti.debug.engine.scripting.Target.reset(Target.java:641)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
at java.lang.reflect.Method.invoke(Unknown Source)
at org.mozilla.javascript.MemberBox.invoke(MemberBox.java:145)
... 18 more
"### Done invoking postbuild tool."
### Successful completion of build procedure for model: CF_4wD_VCU_0513
### Creating HTML report file CF_4wD_VCU_0513_codegen_rpt.html
(1): error: generic lexer error: invalid character '\034' in input stream
(1): error: generic lexer error: invalid character '\000' in input stream
...(中间省略几十行)
下午检查了下,CCS9里不带XDS100v1仿真器驱动(ccs9自带XDS110),在网上搜索ccs3版本才带XDS100。
在CCS9中把项目的编译器改成了XDS110,但是回到simulink中build,依然报XDS100V1的错误。
报错代码如下:
*** Starting debug session... *** Debug Session Name: Texas Instruments XDS100v1 USB Emulator_0/C28xx *** Board Name: Texas Instruments XDS100v1 USB Emulator_0 *** CPU Name: C28xx
CCS9中设置如下:
任然迷茫中。。。