Part Number: TMS320F28335
使用f28335的SCIA通过USB-TTL向电脑的串口助手发送数据,结果能够正常接收到数据,但是每个发送的数据都与电脑接收到的数据不一致;
波特率为9600,采用fifo查询方式,配置代码如下:
void InitSciA(Uint32 baud)
{
Uint16 scibaud = 0;
unsigned char scihbaud=0;
unsigned char scilbaud=0;
scibaud=37500000/(8*baud)-1;
scihbaud=scibaud>>8;
scilbaud=scibaud&0xff;
// Initialize SCI-A:
//tbd...
/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled disabled by the user.
// This will enable the pullups for the specified pins.
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO28 = 0; // Enable pull-up for GPIO28 (SCIRXDA)
GpioCtrlRegs.GPAPUD.bit.GPIO29 = 0; // Enable pull-up for GPIO29 (SCITXDA)
/* Set qualification for selected pins to asynch only */
// Inputs are synchronized to SYSCLKOUT by default.
// This will select asynch (no qualification) for the selected pins.
GpioCtrlRegs.GPAQSEL2.bit.GPIO28 = 3; // Asynch input GPIO28 (SCIRXDA)
/* Configure SCI-A pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be SCI functional pins.
GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1; // Configure GPIO28 for SCIRXDA operation
GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 1; // Configure GPIO29 for SCITXDA operation
EDIS;
SciaRegs.SCIFFTX.all=0xE040;
SciaRegs.SCIFFRX.all=0x204f;
SciaRegs.SCIFFCT.all=0x0;
SciaRegs.SCICCR.all =0x0007;
SciaRegs.SCICTL1.all =0x0003;
SciaRegs.SCICTL2.all =0x0003;
SciaRegs.SCICTL2.bit.TXINTENA =1;
SciaRegs.SCICTL2.bit.RXBKINTENA =1;
SciaRegs.SCIHBAUD =scihbaud; // 9600 baud @LSPCLK = 37.5MHz.
SciaRegs.SCILBAUD =scilbaud;
SciaRegs.SCICCR.bit.LOOPBKENA = 1; // Enable loop back
SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
}
//scia发送单个字节
void SCIA_sendbyte(int byte)
{
while(SciaRegs.SCIFFTX.bit.TXFFST != 0)
{
}
SciaRegs.SCITXBUF = byte;
// while(SciaRegs.SCICTL2.bit.TXRDY != 1)
// {
//
// }
// SciaRegs.SCITXBUF = byte;
}
//sci发送字符串
void SCIA_sendstring(char *msg)
{
int i=0;
while(msg[i] != '\0')
{
SCIA_sendbyte(msg[i]);
i++;
}
}
//sci接收单个字节
Uint16 SCIA_recievebyte(void)
{
Uint16 byte;
while(SciaRegs.SCIFFRX.bit.RXFFST !=1)
{
}
byte = SciaRegs.SCIRXBUF.all;
return byte;
}
然后在100ms的定时中断里面发送数据
interrupt void TINT0_ISR(void) // CPU-Timer 0
{
// char *msg;
// Insert ISR Code here
// To receive more interrupts from this PIE group, acknowledge this interrupt
// PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
// Next two lines for debug only to halt the processor here
// Remove after inserting ISR Code
// asm (" ESTOP0");
// for(;;);
if(CpuTimer0.InterruptCount == 0){
CpuTimer0.InterruptCount++;
LED1 = 1;
}
else{
CpuTimer0.InterruptCount--;
LED1 = 0;
}
temp1 = TMP100_Read();
// msg = "Hello World!\r\n";
// Fot(temp1, 0, 0);
// SCIA_sendstring(msg);
SCIA_sendbyte(0x41);
CpuTimer0Regs.TCR.bit.TIF = 1; //清定时器中断标志位
PieCtrlRegs.PIEACK.bit.ACK1 = 1; //可响应同组其他中断
EINT; //开全局中断
}
发送的明明是0x41,接收到的却是0x5F,换了其他串口助手软件也是这样

通过仿真器调试,寄存器里的数据都正确

请教各位大佬,到底是什么原因呢?