This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用f28335的SCIA通过USB-TTL向电脑的串口助手发送数据,结果能够正常接收到数据,但是每个发送的数据都与电脑接收到的数据不一致;
波特率为9600,采用fifo查询方式,配置代码如下:
void InitSciA(Uint32 baud) { Uint16 scibaud = 0; unsigned char scihbaud=0; unsigned char scilbaud=0; scibaud=37500000/(8*baud)-1; scihbaud=scibaud>>8; scilbaud=scibaud&0xff; // Initialize SCI-A: //tbd... /* Enable internal pull-up for the selected pins */ // Pull-ups can be enabled or disabled disabled by the user. // This will enable the pullups for the specified pins. EALLOW; GpioCtrlRegs.GPAPUD.bit.GPIO28 = 0; // Enable pull-up for GPIO28 (SCIRXDA) GpioCtrlRegs.GPAPUD.bit.GPIO29 = 0; // Enable pull-up for GPIO29 (SCITXDA) /* Set qualification for selected pins to asynch only */ // Inputs are synchronized to SYSCLKOUT by default. // This will select asynch (no qualification) for the selected pins. GpioCtrlRegs.GPAQSEL2.bit.GPIO28 = 3; // Asynch input GPIO28 (SCIRXDA) /* Configure SCI-A pins using GPIO regs*/ // This specifies which of the possible GPIO pins will be SCI functional pins. GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1; // Configure GPIO28 for SCIRXDA operation GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 1; // Configure GPIO29 for SCITXDA operation EDIS; SciaRegs.SCIFFTX.all=0xE040; SciaRegs.SCIFFRX.all=0x204f; SciaRegs.SCIFFCT.all=0x0; SciaRegs.SCICCR.all =0x0007; SciaRegs.SCICTL1.all =0x0003; SciaRegs.SCICTL2.all =0x0003; SciaRegs.SCICTL2.bit.TXINTENA =1; SciaRegs.SCICTL2.bit.RXBKINTENA =1; SciaRegs.SCIHBAUD =scihbaud; // 9600 baud @LSPCLK = 37.5MHz. SciaRegs.SCILBAUD =scilbaud; SciaRegs.SCICCR.bit.LOOPBKENA = 1; // Enable loop back SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset } //scia发送单个字节 void SCIA_sendbyte(int byte) { while(SciaRegs.SCIFFTX.bit.TXFFST != 0) { } SciaRegs.SCITXBUF = byte; // while(SciaRegs.SCICTL2.bit.TXRDY != 1) // { // // } // SciaRegs.SCITXBUF = byte; } //sci发送字符串 void SCIA_sendstring(char *msg) { int i=0; while(msg[i] != '\0') { SCIA_sendbyte(msg[i]); i++; } } //sci接收单个字节 Uint16 SCIA_recievebyte(void) { Uint16 byte; while(SciaRegs.SCIFFRX.bit.RXFFST !=1) { } byte = SciaRegs.SCIRXBUF.all; return byte; }
然后在100ms的定时中断里面发送数据
interrupt void TINT0_ISR(void) // CPU-Timer 0 { // char *msg; // Insert ISR Code here // To receive more interrupts from this PIE group, acknowledge this interrupt // PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Next two lines for debug only to halt the processor here // Remove after inserting ISR Code // asm (" ESTOP0"); // for(;;); if(CpuTimer0.InterruptCount == 0){ CpuTimer0.InterruptCount++; LED1 = 1; } else{ CpuTimer0.InterruptCount--; LED1 = 0; } temp1 = TMP100_Read(); // msg = "Hello World!\r\n"; // Fot(temp1, 0, 0); // SCIA_sendstring(msg); SCIA_sendbyte(0x41); CpuTimer0Regs.TCR.bit.TIF = 1; //清定时器中断标志位 PieCtrlRegs.PIEACK.bit.ACK1 = 1; //可响应同组其他中断 EINT; //开全局中断 }
发送的明明是0x41,接收到的却是0x5F,换了其他串口助手软件也是这样
通过仿真器调试,寄存器里的数据都正确
请教各位大佬,到底是什么原因呢?