DSP双核IPC通信,CPU1同样一个数组readData,我把他放在MSGRAM_CPU1_TO_CPU2里面,传输给CPU2,CPU2读取到的readData地址正确,但是我把数组readData放在RAMGS0中,CPU2读取到的readData地址错误,本来地址应该是0x00C000,现在是0x8000C000,这是为什么呢?我CPU1和CPU2的CMD文件都定义了RAMGS0的起始位置和长度,RAMGS0由CPU1控制。
此外我还有一个问题,就是我在CPU1和CPU2都定义了GSRAM0的话,他们是共享这一片GSRAM0还是说CPU1有一块GSRAM0,CPU2有另外的GSRAM0呢?
CPU1代码如下
// // Included Files // #include "driverlib.h" #include "device.h" #include "board.h" #include "F2837xD_device.h" // F2837xD Headerfile Include File // // Defines // #define IPC_CMD_READ_MEM 0x1001 #define IPC_CMD_RESP 0x2001 #define TEST_PASS 0x5555 #define TEST_FAIL 0xAAAA #pragma DATA_SECTION(readData, "readDataRAM") uint32_t readData[10]; uint16_t IPCpass; uint32_t pass; IPC_MessageQueue_t messageQueue; IPC_Message_t TxMsg, RxMsg; // // Main // void main(void) { int i; // // Initialize device clock and peripherals // Device_init(); // // Initialize PIE and clear PIE registers. Disables CPU interrupts. // Interrupt_initModule(); // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // Interrupt_initVectorTable(); // // Initialize settings from SysConfig // Board_init(); // // Give Memory Access to GS0/ GS14 SARAM to CPU02 //必须在CPU2启动前分配 // while( !(MemCfgRegs.GSxMSEL.bit.MSEL_GS0 & // MemCfgRegs.GSxMSEL.bit.MSEL_GS14)) while( !(MemCfgRegs.GSxMSEL.bit.MSEL_GS14))//GS14未分配给CPU02则循环 { EALLOW; MemCfgRegs.GSxMSEL.bit.MSEL_GS0 = 0;// 将 GS0 分配给 CPU01 MemCfgRegs.GSxMSEL.bit.MSEL_GS14 = 1;// 将 GS14 分配给 CPU02 EDIS; } // // Give memory access to GS0 and GS14 RAM to CPU2 // driverlib库开发写法 // MemCfg_setGSRAMMasterSel((MEMCFG_SECT_GS0 | MEMCFG_SECT_GS14), // MEMCFG_GSRAMMASTER_CPU2); // MemCfg_setGSRAMMasterSel((MEMCFG_SECT_GS14), // MEMCFG_GSRAMMASTER_CPU2); // // Initialize GPIO and configure the GPIO pin as a push-pull output // Device_initGPIO(); GPIO_setPadConfig(99, GPIO_PIN_TYPE_STD); GPIO_setDirectionMode(99, GPIO_DIR_MODE_OUT); GPIO_setMasterCore(99, GPIO_CORE_CPU1); GPIO_setPadConfig(133, GPIO_PIN_TYPE_STD); GPIO_setDirectionMode(133, GPIO_DIR_MODE_OUT); GPIO_setMasterCore(133, GPIO_CORE_CPU2); // // Clear any IPC flags if set already // IPC_clearFlagLtoR(IPC_CPU1_L_CPU2_R, IPC_FLAG_ALL); // // Initialize message queue // IPC_initMessageQueue(IPC_CPU1_L_CPU2_R, &messageQueue, IPC_INT1, IPC_INT1); // // Synchronize both the cores // IPC_sync(IPC_CPU1_L_CPU2_R, SYNC_FLAG); // // Enable Global Interrupt (INTM) and realtime interrupt (DBGM) // EINT; ERTM; // // Fill in the data to be sent // for(i=0; i<10; i++) { readData[i] = i; } // // Update the message // TxMsg.command = IPC_CMD_READ_MEM; TxMsg.address = (uint32_t)readData; // TxMsg.address = (uint32_t)readData; TxMsg.dataw1 = 10; // Using dataw1 as data length TxMsg.dataw2 = 1; // Message identifier // // End of example. Loop forever // while(1) { DEVICE_DELAY_US(1000000); // GPIO_togglePin(133); GPIO_togglePin(99); IPC_sendMessageToQueue(IPC_CPU1_L_CPU2_R, &messageQueue, IPC_ADDR_CORRECTION_ENABLE, &TxMsg, IPC_BLOCKING_CALL); IPC_readMessageFromQueue(IPC_CPU1_L_CPU2_R, &messageQueue, IPC_ADDR_CORRECTION_DISABLE, &RxMsg, IPC_BLOCKING_CALL); if((RxMsg.command == IPC_CMD_RESP) && (RxMsg.dataw1 == TEST_PASS) && (RxMsg.dataw2 == 1)) { pass = 1; IPCpass++; } else pass = 0; } }
CPU2代码如下
#include "driverlib.h" #include "device.h" #include "board.h" #include "F2837xD_device.h" // F2837xD Headerfile Include File // // Defines // #define IPC_CMD_READ_MEM 0x1001 #define IPC_CMD_RESP 0x2001 #define TEST_PASS 0x5555 #define TEST_FAIL 0xAAAA #define GS0_Start 0x00C000 #define ARRAY_LENGTH 10 // 假设数组长度为 10 IPC_MessageQueue_t messageQueue; IPC_Message_t TxMsg, RxMsg; uint16_t IPCCount; uint32_t command, addr, data; bool status = false; uint32_t readData2[10]; #pragma DATA_SECTION(readData2, "readData2") // // Function prototypes // __interrupt void IPC_1_ISR(void); // // Main // void main(void) { int j=0; // // Initialize device clock and peripherals // Device_init(); // // Initialize PIE and clear PIE registers. Disables CPU interrupts. // Interrupt_initModule(); // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // Interrupt_initVectorTable(); Board_init(); // // Clear any IPC flags if set already // IPC_clearFlagLtoR(IPC_CPU2_L_CPU1_R, IPC_FLAG_ALL); // // Initialize message queue // IPC_initMessageQueue(IPC_CPU2_L_CPU1_R, &messageQueue, IPC_INT1, IPC_INT1); // // Enable Global Interrupt (INTM) and realtime interrupt (DBGM) // EINT; ERTM; // // Synchronize both the cores. // IPC_sync(IPC_CPU2_L_CPU1_R, SYNC_FLAG); while(1); } // // IPC ISR for Flag 1 // C28x core sends data with message queue using Flag 0 // __interrupt void IPC_1_ISR(void) { int i,j; // IPC_Message_t TxMsg, RxMsg; // bool status = false; IPCCount++; //利用GS0基地址读取 for(j=0; j<ARRAY_LENGTH; j++) { readData2[j]=*((uint32_t *)GS0_Start+j); } // // Read the message from the message queue // IPC_readMessageFromQueue(IPC_CPU2_L_CPU1_R, &messageQueue, IPC_ADDR_CORRECTION_ENABLE, &RxMsg, IPC_NONBLOCKING_CALL); if(RxMsg.command == IPC_CMD_READ_MEM) { status = true; // // Read and compare data // for(i=0; i<RxMsg.dataw1; i++) { if(*((uint32_t *)RxMsg.address + i) != i) status = false; } } // // Send response message // TxMsg.command = IPC_CMD_RESP; TxMsg.address = 0; // Not used TxMsg.dataw1 = status ? TEST_PASS : TEST_FAIL; TxMsg.dataw2 = RxMsg.dataw2; // Use the message identifier from the received message IPC_sendMessageToQueue(IPC_CPU2_L_CPU1_R, &messageQueue, IPC_ADDR_CORRECTION_DISABLE, &TxMsg, IPC_NONBLOCKING_CALL); DEVICE_DELAY_US(1000000); GPIO_togglePin(133); // uint32_t command, addr, data; // bool status = false; // // Acknowledge the flag // IPC_ackFlagRtoL(IPC_CPU2_L_CPU1_R, IPC_FLAG1); // // Acknowledge the PIE interrupt. // Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1); } // // End of File //
您好
CPU1和 CPU2在物理上没有不同的 GSRAM0、它是相同的存储器。 根据 GSxMSEL 寄存器的配置、任一 CPU 拥有该寄存器。 您是否还可以说明将此部分"readData2"映射到了哪个存储器? 在您共享的代码中、在 CPU2中、您对 GS0_Start 进行硬编码并直接读取 readData2[]。 我希望这可以正常工作。 运行代码时、我观察到 CPU1将地址0xC000放入消息队列(不考虑 IPC_sendMessageToQueue 中设置的 addrCorrEnable 参数)、当 CPU2读取队列时、它会转换地址。 既然我们使用的是 GSRAM、您可以尝试使用 IPC_ADDR_CORRECTION_DISABLE 吗?
readData2我放在了RAMGS14,我设置RAMGS14的主核是CPU2,可以对其读写。在CPU1我把数组放在RAMGS0中,我把RAMGS0的起始地址定义为GS0_Start ,在CPU2中直接用GS0_Start 读取数据是没有问题的。意思就是如果我在CPU1中把数组放在GSRAM而不是MSGRAM的话,不用地址校正就可以吗?我去尝试一下。另外这个地址校正是什么意思我还没弄明白,为什么会需要地址校正呢?相关的资料在哪里查呢?
非常感谢,刚刚我尝试了一下使用GSRAM的话采用IPC_ADDR_CORRECTION_DISABLE,现在地址就正确了,为什么用GSRAM就不用地址校正,用MSGRAM就需要呢?麻烦你再给我解释一下。
是的,对于GSRAM来说采用IPC_ADDR_CORRECTION_DISABLE 就可行了,但是为什么利用MSGRAM的时候需要IPC_ADDR_CORRECTION_ENABLE呢?可以为我解答一下吗?
还有一个疑问呀。为什么数组存放在GSRAM采用IPC_ADDR_CORRECTION_DISABLE,存放在MSGRAM的时候需要IPC_ADDR_CORRECTION_ENABLE呢?只有这一个疑问了。
您好
应在 sendMessage 和 readMessage 函数调用中禁用地址校正(IPC_ADDR_CORRECTION_DISABLE)。
您好
这是因为 API 实现假定使用 MSGRAM。 如果启用了地址校正、它会将地址发送到 MSGRAM 基址。 当您将其与 GSRAM 一同使用时、地址将损坏。
我的理解是因为GSRAM对于CPU1和CPU2是一个地址,但是MSGRAM具有指向性,若是CPU1TOCPU2RAM,是否可以认为同一块区域在CPU1和CPU2的地址不一样呢?
您好
是的、GSRAM 地址同时适用于 CPU1和 CPU2。 CPU1TOCPU2RAM 在 CPU1和 CPU2中也是相同的地址、没有什么不同、只是访问权限不同。 MSGRAM 具有来自其自身 CPU 子系统的 CPU/DMA 读取/写入访问权限、以及来自其他子系统的 CPU/DMA 只读权限。