MSPM0G3507外接OLED使用内部温度传感器测量温度并显示在OLED显示屏上
When using the CLI tool to compile and build sysconfig, the following error occurs:
Running script...
Error: cannot set 'compiler' to 'ticlang'
The command to be executed…
报错提示:Unable to download component ECLIPSE: File not found
在官网的下载链接下载多次依然是这样
本以为时中文路径问题切换英文账户后依旧无法解决
MSP Zero Code Studio cannot compile and run. I was connected to mspm0g3507 and the CCS showed that my development board was successfully connected to the computer.Please tell me how to solve it, thank you very much.
请问MSPM0G3507如何配置内部温度传感器,SysConfig应该如何配置
20.1.1.008版本的CCS对于一些代码它不提示 例如DL_GPIO_readPins它不提示 而且当我打开例程文件我也无法跳转(not go to define)
使用JliNK和UNIFLash烧录文件,中途突然中断,后续通过CCS不能更改或调试程序
你好:
我在使用SPI作为通信方式,我将从主机(MSPM0G3507)发送数据,在从机(ADS8688)接收数据后,将采集到的数据回传到主机;我使用示波器在POCI引脚的波形检测是循环连续的。我设置了接收中断,接收中断一直在触发,但Rxdata中没有数据传出,这是什么情况,下面是代码
请问,MSPM0G3507可以在在100KV以上的高压环境下工作吗?
MSPM0G3507扩展板上的LCD如何使用啊?需要发送什么指令?
MSPM0G3507做为IIC从机,主机进行数据读取出现问题,我这边I2C协议的头数据应该为EE,但是在极低概率(300次可能出现1-2次)中读取的头字节变为了00,第二个字节变成了EE,通过逻辑分析仪抓取的数据如下:
应该如何解决?
正常数据:
异常数据:
When I turn it on again, it stops at DL_SYSCTL_getClockStatus(void)
The following is the location where I met
/* Check that SYSPLL is disabled before configuration */
while ((DL_SYSCTL_getClockStatus() & (DL_SYSCTL_CLK_STATUS_SYSPLL_OFF…
我对开发板进行二次设计,连接RS485芯片。在编程时,在主函数内,我自己编写了A函数,在A函数内,我配置了DMA的传输配置,包括源地址,终地址,数据大小,也在config里面配置了uart的DMA传输完成中断,我的期望情况是,在A函数内进行DMA传输,在传输完成之后触发中断,在中断内,我再进行其他操作。现在遇到的问题是,DMA触发不了传输完成中断,进入不了中断函数,请问这种情况怎么处理
Dears
MSPM0G3507使用MSP-FET可以仿真吗?IAR环境