• BQ76952: EMC Test(RS-Radio Sensitivity) failure

    Part Number: BQ76952
    Other Parts Discussed in Thread: BQ76930

    In Radio Sensitivity test ,we found the voltage collect is failure. In fact, the cell voltage is 3.6V, but the AFE voltage collect is 4.4V,the test frequency band is 80 MHz.

  • BQ76930: 主动均衡和被动均衡

    Part Number: BQ76930

    BQ76930是否有主动均衡功能?如果有的话如何进行配置?

  • BQ76930: BQ76930

    Part Number: BQ76930

    你好,我使用了TI的BQ76930电源管理芯片设计我的电路。目前手册Datasheet和EVM板里面都是采用充电与放电在同一个接口Pack+-。我现在想要设计为充电与放电分开的两个接口,我认为需要将Discharge和Charge的两个PMOS控制管放在不同的回路,但是我不知道应该如何设计,麻烦您对我做出指导,谢谢!

  • BQ76930: BQ76930这颗BMS芯片能关闭欠压保护吗?

    Part Number: BQ76930

    TI的BMS芯片BQ76930能把他的欠压保护功能给关闭吗?如果可以如何关闭呢?因为我这个项目是应用到无人机上面的,如果飞机在飞行的过程中,飞机触发欠压保护,那飞机就掉下来了,飞机比电池贵,这样会得不偿失,所以我想求助如何能关闭欠压保护。

  • BQ76930: 两片BQ76930串联做20S电池管理系统,第十一串采样异常。

    Part Number: BQ76930

    val 0:3445 val 1:3454 val 2:3448 val 3:3447 val 4:3441 val 5:3420 val 6:3446 val 7:3461 val 8:3446 val 9:3449 val 10:72 val 11:3383 val 12:3371 val 13:3383 val 14:3344 val 15:3329 val 16:3377 val 17:3389 val 18:3395 val 19:3365

    第二片bq76930的vc1采样异常…

  • BQ76920: The battery voltage can be read, but the configuration register can not be read, may I ask if the chip can only read data register.

    Part Number: BQ76920

    As shown in the figure,SYS_CTRL1 register  can be written correctly, but it cannot be read correctly. The data register can read the battery voltage normally. Therefore, whether the bit configuration register cannot be read or needs…

  • BQ76930: 级联怎么平衡功耗

    Part Number: BQ76930

    使用BQ76930级联时(20S),出现高压部分功耗大于低压部分功耗导致电池用久了出现分层现象(11-20串电池电压小于1-10电池电压),该怎么平衡这两个功耗

  • BQ76930: 共地问题

    Part Number: BQ76930

    我用BQ76930设计了一个BMS板,所有功能都正常,但是有一个问题,我安装到电池组(6节4.2V电池)上,在断开BMS的充放电MOS管后,我测量BMS的输出口的电压,会存在一个20V左右的电压。由于MOS管是控制负极接通的,如果此时MOS管没有导通,系统没有共地,所以我怀疑是这个原因,产生这个20V的压差。原理图如下:

    如何解决这个浮地的问题呢?

  • BQ78350: BQ78350 + BQ76930

    Part Number: BQ78350
    Other Parts Discussed in Thread: BQ76930, BQSTUDIO,

    有个新项目准备用BQ78350搭配BQ76930使用,有两个问题想请教一下:

    1. 通过BQStudio可以设置BQ78350,BQ76930还需要单独设置吗?

    2. MOSFET推荐是放在负极回路,为了不影响通讯,SMBus的GND是不是要接到电芯负极?这样接会有什么影响吗?

    谢谢。

  • BQ76930: DEV_XD 在终端用户使用时被置位

    Part Number: BQ76930

    通过TI工具确认BQ异常无法掉电原因为IC内部异常故障标志位置1,想了解下是什么原因会导致此标志位置起。

  • BQ76930: 如果要测六节电池,如何连接VC引脚

    Part Number: BQ76930

    该芯片手册原理图测的是十节电池,如果要测六节电池,如何连接VC引脚

  • BQ76930: 电流计异常诊断

    Part Number: BQ76930

    对于电流的读取,程序内的策略是先读取电流计的Ready位(300ms),根据Ready位的结果决定是否读取电流值,若Ready == 0,则软件保持上次的数据。

    现在,我有个疑问,Ready位是否会连续的出现为0的情况?若芯片内电流计损坏,对于软件来说该做什么处理?

  • BQ76930: 在低温-40℃时,会触发硬件短路保护

    Part Number: BQ76930

    在低温-40℃,待机时,没接负载和充电,会触发硬件短路保护,但读到的电流是正常的,常温下不会出现这个现象

  • BQ76930: BQ76930温度采样异常

    Part Number: BQ76930

    你好,我在使用BQ76930的过程中,如果通过I2C初始化外部热敏电阻温度测量,会引起电池电压采样跳变,把温度测量屏蔽以后,电压采样就不会跳变,请问是什么原因呢?原理图如下

  • BQ76930: 电压和电流采样如何保证250ms读取的数据是准确的?

    Part Number: BQ76930

    尊敬的TI专家:

    您好!

    BQ76930手册上说每250ms完成一次电压的完整更新,想请问下250ms里每个cell采样多少次?采样频率是多少?用了什么算法?如何保证结果的正确性?

    另外16位CC在ALWAYS ON模式也是250ms完成一次更新,请问采样了多少次电流?采样率是多少?用了什么算法?如何保证结果的正确性?

    期盼得到您的回复,谢谢!

  • BQ76930: 用做20S三元锂电池设计时,第一串和第十一串掉电厉害

    Part Number: BQ76930

    从AFE读到数据,第一串和第十一串电池电压掉电明显,其它串电池只是几mV掉电,第一和第十一串20mV的掉电,但我硬件上测到的电压是没有掉电的,这是什么原因,下面是我的原理图

  • BQ78350: 参数如何配置来降低保护板功耗?

    Part Number: BQ78350
    Other Parts Discussed in Thread: BQ76200, BQ76930

    我们用BQ78350、BQ76930和BQ76200三款芯片做了一款7串锂电池保护板。但是发现该静态自耗电很大,在0.4mA左右。电池容量放光后,存放一个月左右进入了Shutdown(电压低于1.75V)模式,导致电池无法使用,需拆壳,激活保护板才能充电。

    保护板外围电路为官方推荐电路,无异常耗电。

  • BQ76930: BQ76930读取电芯电压、温度值失败

    Part Number: BQ76930

    当前版本为第个各版本原理图种采取了LDO转12V芯片,替代了推荐方案里的供电方案;

    检测:

    ①I2C是正常的;

    ②BQ76930的REGOUT输出有3.3V;

    ③可以更改部分寄存器的值;

    ④线路连接正常;

    ⑤不能读取电芯电压、温度值;

    请问:导致不能读取电芯电压、温度值的原因是否是供电问题????

  • BQ76930: 关于REG0x00 中的DEVICE_XREADY位,手册中的介绍很模棱两可

    Part Number: BQ76930

    DEVICE_XREADY 位在何种情况下被置位?

    DEVICE_XREADY 位在何种情况下不能被清除?

  • BQ76200: BQ76200

    Part Number: BQ76200
    Other Parts Discussed in Thread: BQ76930

    现在VDDCP~B+仅为9.4V,DSG和CHG电压为0V。 DSG_EN和CHG_EN与GND的电压始终为10.9V

  • BQ76930: 两片BQ76930串联做20S电池管理系统,插拔排线过程中第6、7串概率损坏问题

    Part Number: BQ76930

    两片BQ76930串联做20S电池管理系统,插拔排线过程中第6、7串概率损坏问题,表现为如图示情况

    相关原理图如下

  • BQ76930: bq76930如何关闭保护功能

    Part Number: BQ76930

    我想关闭BQ76930的两个保护功能:过流和短路(OCD、SCD),请问该怎么做,感激不尽

  • BQ76930: BQ78350-R1+BQ76930组合

    Part Number: BQ76930
    Other Parts Discussed in Thread: BQ78350-R1,

    你好 ,BQ78350-R1+BQ76930组合的电路,想请教一下误 解除过充保护问题

    BQstdio中设置COV Threshold 3.55V, Delay 2S Recovery3.3V

    触发过充保护后MOS关断,并进行放电一段时间,再充电后达到3.55V COV保护值后切断MOS几秒又打开再切断,打开和切断的过程中没有触发到Recovery3.3V(磷酸铁锂电芯)…

  • BQ76930: 这部分参考设计的作用是什么

    Part Number: BQ76930

    你好,我用BQ76930做20串电池设计,参考你们的设计时,有一部分电路不懂,请教一下

  • BQ76930: BQ76930这部分参考设计作用是什么

    Part Number: BQ76930

    用BQ76930做20s电池保护板时的参考设计,请教红框这部分电路的作用是什么,谢谢

1 2 3 4 5 »