This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2015年达芬奇精华帖汇总(DM8127/DM814x)-软件问题



1. ipnc_rdk启动脚本?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/78513.aspx


2. 想问一下 DCC在调试RGB2RGB时是否需要将 awb 关闭?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/78969.aspx


3. DM8127 的mcasp0 寄存器访问不了?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/79594.aspx


4. DM8148的MCASP2配置
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/79597.aspx


5. mcfw link 疑问
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/81080.aspx


6. 3D 去噪 中 vnflink中去噪强度是否可以开到最强,有什么负效果吗??
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/81127.aspx


7. DM8127的MP SCALR模块无法create,提示“pObj->scCreateStatus.retVal” 为FVID2_EALLOC
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/81209.aspx


8. DM8148 uboot 网络正常,Linux 起来后网络不通
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/81275.aspx


9. 图像处理嵌入式平台选择问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/82514.aspx


10. DM8147调试时遇到错误编码1180
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/84185.aspx


11. NFS挂载故障
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/84660.aspx


12. DM8127第二部分U-BOOT不运行的问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/84844.aspx


13. Live555获得的帧数据是否可以通过IPC bits links
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/85448.aspx


14. Appro DM8127 IPNC
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/87454.aspx


15. Appro DM8127 IPNC
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/87586.aspx


16. TI DM8148支持2000万像素及以上的jpeg编码吗
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/87869.aspx


17. DCC抓的RAW图片不正常
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/87958.aspx


18. M3Video 跳帧问题 ?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/90440.aspx


19. 8127可不可以保存一幅raw图片呢?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/90567.aspx


20. 请教814x DVRRDK 编译后map文件在哪里?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/91404.aspx


21. dm8148 vpss 下JPEG编码(MJPEG)和VideoM3上的JPEG有什么区别吗?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/91710.aspx


22. DM8148求助 案例
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/92320.aspx


23. dm8148 init.sh load.sh?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/92705.aspx


24. DM8148 为什么我无法生成KO文件
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/95349.aspx


25. ezsdk中是不是不包含两个M3和dsp的code?如果要修改生成新的xe文件只能用rdk版本进行开发?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/95749.aspx


26. DM8148 启动到## Starting application at 0x81000000 ...就停止了,并且Hit any...
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/96046.aspx


27. DM8127 接YUYV 16bit 模组
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/96861.aspx


28. 请教:DM8127 link.cmd编译修改问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/97507.aspx


29. DM8127 百兆phy问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/97907.aspx


30. DM8127 IPNC capture-->display usecase
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/98075.aspx