Hello,
I am using Yocto to build tisdk-adas-image
and tisdk-default-image
, and I noticed that the process requires downloading more than 13,000 intermediate components. However, my build environment has only 200GB of storage…
Hello,
I am using Yocto to build tisdk-adas-image
and tisdk-default-image
, and I noticed that the process requires downloading more than 13,000 intermediate components. However, my build environment has only 200GB of storage…
TDA4vm和TDA4vh下使用QNX SDK还需要购买商业许可吗?包括开发阶段和商用阶段。如果需要购买,许可可以通过那些渠道获取?
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hungarian | Russian |
Chinese… |
Hi TI,
请问AM6202的内部RTC在深度睡眠时,是否还能继续工作计时,在睡眠一段时间,醒来时能得到一个较精准一点的时间。
WKUP_LFOSC0_XI/XO已有接32.768Khz
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplif… |
您好,现在基于TMS320C6670 EVM评估板进行软件开发,通过网络boot的方式加载程序,通过抓包软件捕获bootp协议包,可以看出拨码开关设置成功,程序是基于ti的ndk实现DSP与上位机网络通信的回环,EVM评估板上只有一个网口,现在测试发现例程不起作用,请问可能是什么原因?会不会是方案设计有问题,网口有冲突?
Arabic | Hebrew | Polish |
Bulg… |
we need add frame number in the h264 video.
Arabic | Hebre… |
Hello,
I referred to the demo and used PDK for functional development, and I have some problems of using the Main domain uart3 (using rx levle interrupt triger,DMA was not used) in mcu1_0. (Note: It is possible to read data using…
1.DSS supports two types of display interfaces(Display parallel interface & Two low-voltage differential signaling (LVDS) interfaces):could this two interfaces work simultaneously(same display content),or just one of them at the same…
您好,
我在看用户手册的时候,看到两个概念:PKTDMA和PDMA,如下图所示:
请问这是一样的吗?如果不一样的话,PDMA如何使用SysCfg来设置?
谢谢!
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hungarian | Ru… |
I'm on Windows and the version I am using is CCS 5.3, I would like to know if this version comes with a gcc package, if so how should I enter it in the include path, and if it does not come with a gcc package what version of…
当前eth0和eth1为cpsw switch模式的网口,如何在驱动中进行设置,使
(1)两网口内部的switch数据传输速率不限速
(2)但是两网口进入mpu的速率限制到10M?
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hun… |
从去年11月下旬开始使用CCS 12.8.1版本
到目前为止,遇到过多次workspace目录下文件读取异常的情况,表现为文件系统错误导致部分文件无法读取也无法删除,从而有时候导致工程导入错误,或者无法编译
尝试过在新的硬盘分区重新建立工程,开发一段时间后,在新的硬盘分区依然会遇到上述问题
不知道大家有没有遇到过这个问题
Arabic | Hebrew | Polish |
Bulgari… |
Hello,I want to use Uart3 in main domain(baudRate is 460800,use interrupt mode). Is it possible to use it in the following way?
1、Set Pinmux V28 UART3_RXD,V29 UART3_TXD
2、use UART_socSetInitCfg()function set operMode is UART13x_OPER_MODE…
Hello,I want to use Main domain I2c(CSL_I2C2 bitRate 400khz) in Mcu domain. Is it possible to use it in the following way?
1、Set pinmux U23 as I2c SCL, U26 as I2c SDA
2、Preventing access to I2c2 by changing the base address
#define…
Hi TI
After power on about 13 minutes,
device's UART is no response, it can not input command or output log.
u-boot shell "=>" or "kernel shell "root@j721s2-evm:~#" have the same problem
Is there…
os : RTOS
icssg dirver: porting from uboot in sdk9.0
test method: phy internal loopback
compile chain: gcc
When testing RAW data, send 1024 bytes of data every 1ms, receive the data, and check the receive length, which can sometimes…
Hi support,
We're doing LPDDR4 layout for AM62D.
After reading this version of the DDR design guide https://www.ti.com/lit/an/sprad66b/sprad66b.pdf, I have several confusions.
1. According to LP4_DRS6 in Table 2-7, the propagation…
Hi TI expert,
I am working with qnx on am62px.
I would like to know if TI has a feature for memory fragmentation and organization in the QNX system.
or other measures to prevent or reduce memory fragmentation.
thanks
SDK Ver: 10_00_00
I modify tests/app_tiovx_linux_decode_display_test.c and try to capture and display my sensor video. The block diagram is as follows.
The main function is as follows
你好:
想请教一下关于mcu domain和main domain单独复位的问题,由于设计需要使用software方式实现m4与a53相互复位的功能,我查看了文档《spruiv7b.pdf》的6.3.5.2.3 SW_MAIN_WARMRSTz Reset和6.3.5.2.4 MCU_RESETz Reset章节,但未查找到文中所说的寄存器地址,能说明一下这几个寄存器的地址,以及软复位的具体操作方法吗?
硬件平台:am625sip
SDK:ti-processor-sdk-linux-am62xxsip-evm-09.02.01.10-Linux-x86-Install
尊敬的TI支持团队您好!
我们在做一款音频相关的产品,现在我们可以使用ALSA库实现8声道的音频播放和2声道音频的录制,但不能实现8声道的录制,如题,我的问题是am625sip在当前版本下是否支持8声道的音频录制…
你好,
请问一下DRA829 两个A72 是否可以运行AMP,就是运行两个QNX系统?
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hungarian | Russian |
Chinese Traditional | Indo… |
官方的MCAN loopback demo修改 app_mcanConfig(false)后,一直无法外发CAN数据成功,lastErrCode一直为5,loopback模式是可以的,按照文档介绍重写也是这样,请问这是什么问题?要怎么解决?用的是官方的板子。
有没有相关的可以外发的DEMO?