• CC2640R2L: Power consumption anomaly

    Part Number: CC2640R2L
    Other Parts Discussed in Thread: CC2640

    The CC2640R2L enters low-power sleep with a normal current of 1.5ua, the same procedure and operation, batch TI 368, TI 388 power consumption of 100ua+

    TRANSLATE with x
    English
  • LAUNCHXL-CC26X2R1: 影响最大连接数量(主/从)的因素有哪些?

    Part Number: LAUNCHXL-CC26X2R1

          麻烦您帮忙解答下,十分感谢!

           BLEcc2642)作为主从一体时,最多连接几个主设备?几个从设备?(能稳定做业务,如数字钥匙场景的最大连接数分别是多少?)

           影响最大连接数量(/)的因素有哪些?

     

     

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw Romanian
  • LP-EM-CC2745R10-Q1: LP-EM-CC2745R10-Q1开发板,导入basic_ble例程跑不起,看起来是BLE协议栈未正确完成初始化

    Part Number: LP-EM-CC2745R10-Q1
    Other Parts Discussed in Thread: SYSCONFIG

    LP-EM-CC2745R10-Q1开发板,导入basic_ble例程跑不起,看起来是BLE协议栈未正确完成初始化,如何解决?

    描述:

    1.  使用最近2个SDK版本都存在该现象...f3_sdk_8_40_00_61版本 和...f3_sdk_8_40_02_01

    2.  基于最新CCS 12.8.1 Version: 12.8.1.00005,(sy…

  • CC2340R2: 使用2m phy时的速率和丢包率

    Part Number: CC2340R2

    我想了解使用2m phy下能实现的最高的有效数据传输速率是多少,这个速率下在理想环境中丢包率有多少。

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw Romanian
    Chinese Simplified Hungarian Russian
    Chinese Traditional I…
  • CC2652RB: BLE蓝牙连接不稳定,超出5m范围连接就会断开

    Part Number: CC2652RB

    一款嵌入式产品带有蓝牙连接功能,MCU采用CC2652RB(带BLE功能、RF_P/RF_N管脚)方案,BLE蓝牙Balun电路设计如下图;

    PCB Layout布线如下图;

    *上述电路设计和PCB Layout设计方案以前均做过P板实机测试过,结果OK,BLE蓝牙连接距离可达25m以上稳定性没问题)

    近期试作P板时,为了控制Balun电路阻抗保持在50Ω,PCB工厂对Balun电流走线线宽做了调整[13mil(0.33mm)→4.3mil(0.1mm…

  • CC2340R5: 當配對時不需要輸入Pin Code

    Part Number: CC2340R5
    Other Parts Discussed in Thread: SYSCONFIG

    Hi.

    當使用 Android 10 以上版本,同時使用設定/藍芽 進行配對,或需要輸入 Pin code 才能配對完成,要如何移除輸入 Pin code 步驟,直接配對完成?

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan
  • LAUNCHXL-CC26X2R1: 两个手机同时连接蓝牙,同时给同一个UUID写和读数据,会出现问题吗?

    Part Number: LAUNCHXL-CC26X2R1
    Other Parts Discussed in Thread: SYSCONFIG

     两个手机同时连接蓝牙,同时给同一个UUID写和读数据,会出现问题吗?

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw Romanian
    Chinese Simplified Hungar…
  • CC2640R2F: LESC安全连接手机适配

    Part Number: CC2640R2F

    hello,everyone:

        目前在蓝牙手机适配的问题上卡住了,希望大家能提供一下帮助,具体信息为:

              蓝牙SDK:simplelink_cc2640r2_sdk_4_10_00_10

              由于使用了LESC,ram不够,当时的项目打开了CACHE

              具体的配置为:

    uint8_t pairMode = GAPBOND_PAIRING_MODE_INITIATE;

    uint8_t mitm = TRUE;

    uint8_t…
  • CC2642R: 从机主动notify会卡住

    Part Number: CC2642R

    主机打开notify enable,然后写char1,从机调用上面的notify函数响应数据,这个是没有问题的。

    但是,如果是主机没有写,从机主动notify一次数据就会导致BLE超时了,搜不到信号了。

  • CC2642R: CC2642R

    Part Number: CC2642R

    Hello, I want to get the name of the broadcast device when the device is scanned but not connected,How it can be done

    Thank you

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong…
  • CC2340R5: Do Not Print BLE ID Address

    Part Number: CC2340R5

    When I use basic_ble in SimpleLink Low Power F3 SDK (8.20.00.119), the Terminal has no print about BLE ID Address.

  • CC2640R2F: 需要进行KC认证,需要跳频发射,间接发射,改如何实现。

    Part Number: CC2640R2F

    如题,实现

    之前做FCC认证,定频实现是 HCI_EXT_ModemTestTxCmd(HCI_EXT_TX_UNMODULATED_CARRIER,0);

    不知道KC咋实现的,希望告知下。

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw Romanian
    Chinese Simpl…
  • CC2340R5: 無法Debug

    Part Number: CC2340R5
    Other Parts Discussed in Thread: UNIFLASH

    當我使用.out檔進行燒錄時,Console會顯示以下的:

    Cortex_M0P: File Loader: Memory write failed: Error occurred when erasing the chip - Command is not allowed due to restrictions
    Cortex_M0P: GEL: File: C:\ti…

  • CC2640R2L: 串口“部分返回”功能,返回方式疑问

    Part Number: CC2640R2L

    在使用2640串口时,配置为回调方式并开启部分返回功能接收不定长字符串,正常情况下2640串口收到一个字符串,可以一包收到,但是当发送方发送的字符之间延时稍大,2640的接收就会分包,这个应该是部分返回功能导致的,我想知道部分返回功能是什么原理,是超过一定时间没有接收到下一个字节就会返回吗?还是有其他判断方式进行部分返回?

    代码如下:

    Fullscreen
    1
    2
    // Callback function
    static void UartreadCallback(UART_Handle…
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • CC2340R5: TX Power Index

    Part Number: CC2340R5

    关于CC2340R5的TX_Power_Index问题,我逛论坛发现七八个月前就已经修复好了这个问题,我现在使用的SDK版本是7.20.0.29,发现仍然不可以调用,最新的7.20.1.10也是一样的?请问我需要修改时,应该怎样操作?

    Fullscreen
    1
    2
    3
    4
    5
    6
    /**
    * @defgroup TX_Power_Index TX Power Index
    * @{
    */
    #ifndef CC23X0
    #if defined( CC26XX ) || defined…
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • CC2640R2F: 多任务的创建

    Part Number: CC2640R2F

    你好,我想问一下多任务的创建中遇到了一些问题

    在APP程序ble5_simple_peripheral_cc2640r2lp_app_FlashROM_StackLibrary.opt设置的ICALL_MAX_NUM_ENTITIES=6   ICALL_MAX_NUM_TASKS=3,

    1.ICALL_MAX_NUM_TASKS=3是stack任务,gap任务和用户自定义的任务,一共是三个,但ICALL_MAX_NUM_ENTITIES为什么是6?(…

  • LP-EM-CC2340R5: oad-onchip示例合并data-stream

  • RE: LP-EM-CC2340R5: 功耗問題 , 與 RTC WAKEUP 範例.

    嗨~ 再請教.

    (1) 要達到低功耗, 能滿足大部分是進入STANDBY狀態. 又能常態的固定時間醒來.(比如每5秒鐘醒來)

    在FREE RTOS環境下. 除了加上 TIMER TASK 之外,還有甚麼方法可以實現?

    我目前,測試 功耗過程發現. 透過 TIMER TASK .每次WAKEUP 瞬間電流高達2mA...如下圖))

    下圖是.開發版實測, 每5秒 wakeup. 起來甚麼事都不做.也沒任何GPIO輸出.

    測1分鐘平均電流就達 8.5uA了. 

    (2) 我讓廣播1筆,就停止. 如下圖設定…

  • CC2642R: 守护时间

    Part Number: CC2642R
    Other Parts Discussed in Thread: SYSCONFIG

    您好!请给我一份蓝牙守护时间(goard time)的说明,谢谢

  • LAUNCHXL-CC26X2R1: SDK:simple_peripheral project 任务间运行和消息事件传递问题

    Part Number: LAUNCHXL-CC26X2R1
    Other Parts Discussed in Thread: SYSCONFIG, ENERGYTRACE

    在DEBUG这个工程的时候遇到一些问题:

    1、当APP  task任务执行到设置GapAdv_create #2时,会跳转执行SimplePeripheral_advCallback(此函数是向BLE stack传入的回调)将APP_ADV_EVT入队。

    关于这一步我的理解是:BLE stack的优先级高于APP  task,所以当GapAdv_enable之后…

  • CC2652P: CC2652P: zigbee传输速度较快时丢包

    Part Number: CC2652P

    说明:这是一个关于zigbee的问题,因论坛选择框只有“bluetooth forum”可选项,所以被划分至蓝牙论坛了。

    芯片: CC2652P

    协议栈版本号:simplelink_cc13xx_cc26xx_sdk_6_40_00_13

    应用场景:一个协调器,一个子设备,当作透传模块使用。测试速率:每间隔30ms发送一包数据,zcl payload携带64字节数据。测试过程中,发现丢包的情况。发送端的打印LOG显示,所有数据发送成功…

  • CC2652RSIP: 关于定时器Timer的API Timer_control 的一些疑问

    Part Number: CC2652RSIP

    我有一个需求,需要查看指定的定时器的运行状态(停止、运行中等)。

    查看Timer的API,感觉Timer_control可能能够实现此功能,但只在Timer.h文件中看到它的声明extern int_fast16_t Timer_control(Timer_Handle handle, uint_fast16_t cmd, void *arg);但并未对其支持的cmd命令进行详细的描述,能否有更详细的资料对其进行描述?谢谢

  • LP-EM-CC2340R5: 16碼UUID 變更後,SIMPLE LINK CONNECT 無法執行OAD 更新,怎麼解?

    Part Number: LP-EM-CC2340R5

    你好!

         我使用 LP-EM-CC2340R5 開發板.  跑 OAD 範例程式. 再配合 Simple Link Connect  APP 來更新FW.

    一切都正常。

    但是. 當我嘗試把 16 碼 UUID 替換成自家指定的 UUID後, 雖然  Simple Link Connect  一樣能掃描的到我的裝置.

    但連線進入之後, 卻無 " Update FW" 的 ICON 可以執行 OAD動作了.

    下圖的紅圈處為正常顯示…

  • CC2642R: CC2642 的SKD 13xx_cc26xx_sdk_6_20_00_29 public mac 的主机 发起配对绑定后,然后主机端删除配对信息,再次发起配对,然后主机跟从机断开,主机发起扫描请求,从机收不到

    Part Number: CC2642R

    Hello TI 的工程师:

    使用 CC2642 的SKD 13xx_cc26xx_sdk_6_20_00_29 SDK,遇到这样的情况,主机是华为的手表是 public mac 的地址,CC2642做从机,华为手表跟CC2642 配对绑定后,然后由于业务原因,华为手表在本地将配对信息删除了,当再次连接时,重新跟CC2642发起了配对绑定,配对绑定完成后,华为手表与CC2462连接断开,此时华为手表发送 scan request 到 CC2642, CC2642…

  • LAUNCHXL-CC2640R2: TIDA-01580: 使用application软件中的vi文件生成exe文件后出错

    Part Number: LAUNCHXL-CC2640R2
    Other Parts Discussed in Thread: TIDA-01580, SIMPLELINK-CC2640R2-SDK, CC2640R2F

    我使用launchpad-cc2640r2板子与TIDA-01580进行心电与脉搏检测,安装成功ccs10.4.0后并未打开该软件,安装成功TIDA-01580application后使用labview2016其中名为TIDA-01580application的vi文件生成了exe可执行文件…

1 2 3 4 5 »