Other Parts Discussed in Thread: LMX2572
请问LMX2594设置从1GHZ扫到1.5GHZ,步进1MHZ,10秒扫完,扫描6个周期,每个地方要如何选择,怎么设置,怎么计算,有没有相应的指南,谢谢!
我们在用LMX2572时,出现一个很奇怪的现象,LMX2572在上电后,使用spi成功锁定一个频率,然后把参考信号(Oscin)断开,再配另一个频率字,写入一次R0寄存器,寄存器操作结束以后,再把参考信号(Oscin)加上,此时会随机出现两种现象:
1、一种是锁相环失锁,但重新配一次频率字以后,能够恢复锁定,后面继续跳频也都能工作正常;
2、另一种是芯片的电流比正常工作时,电流大了30mA,失锁,并且从这以后不管怎么操作频率字,都没有办法恢复锁定了,这个时候…
鉴相频率Fpd=100Mhz
起始频率902.5MHz, 要求在890-915MHz之间往返扫频,步进50KHz,
测试了几天,输出依然不对,能否帮我检查一下,或者能给予一个寄存器数值表?
按照我的理解,
Fstep = 0.05*4=0.2;
Fmax = 915*4=3660;
Fmin = 890*4=3560;
Fstart = 3610;
RAMP_LIMIT_HIGH…
目前用2颗LMX2572 在同一个小的PCB内,请问布局需要怎么处理才能减少相互的串扰,特别是电源和GND的布线,PCB叠层是否有推荐,谢谢 ,
补充一下项目中要求频率输出6.4G和6.398GHz
LMX2572的评估板上晶振的位置是空着的。查阅数据手册,发现LMX2572对差分晶振的输入电平有要求。有推荐的晶振型号吗?
器件能够正常锁定,VCO直接输出没有问题,但是使用分频输出时,部分频率正常,但有好几段频率输出不正常,类似失锁状态,但是锁定检测脚是正常,我怀疑是分频器没有工作正常,想知道有没解决办法
Hello:
I have a question about LMX2572. LMX2572 is configured with sysref_REFEAT mode of SYSREF (signal frequency is 976.5625KHz), and an abnormally narrow pulse appears at the falling edge of output waveform, as shown below:
When I was using CPLD to configure LMX2572, I encountered the following problem: I was able to switch frequencies below 3.2GHz, but when I tried to switch frequencies above 3.2GHz, I got a Divider output of the frequency I wanted…
When I was using CPLD to configure LMX2572, I encountered the following problem: I was able to switch frequencies below 3.2GHz, but when I tried to switch frequencies above 3.2GHz, I got a Divider output of the frequency I wanted…
R125 0x7D2288
R124 0x7C0000
R123 0x7B0000
R122 0x7A0000
R121 0x790000
R120 0x780000
R119 0x770000
R118 0x760000
R117 0x750000
R116 0x740000
R115 0x730000
R114 0x727802
R113 0x710000
R112 0x700000
R111 0x6F0000
R110 0x6E0000
R109 0x6D0000
R108 0x…
LMX2572配置SYSREF_REPEAT模式时,输出SYSREF异常
R125 0x7D2288
R124 0x7C0000
R123 0x7B0000
R122 0x7A0000
R121 0x790000
R120 0x780000
R119 0x770000
R118 0x760000
R117 0x750000
R116 0x740000
R115 0x730000
R114 0x727802
R113 0x710000
R112 0x700000
R111 0x6F0…
关于手册中相关参数的计算不是看的很明白,手册中的参数 与TICSPRO中没有对应上。烦请将样例中的50MHz改为20Mhz(与鉴相器频率区分开,便于理解),提供一下automatic ramping 8GHz到10GHz在2ms内完成的TICSPRO中的配置截图,如果参数存在计算,麻烦帮忙说明一下计算公式,谢谢
我们想从1G频率开始每1ms步进1kHz,按照数据手册试过操作各种寄存器都无法实现,现在只能实现输出一种频率,只要重新设置相同或不同的频率输出都会直接没有输出了。我们是用单片机通过SPI口操作芯片,希望能提供扫频输出的C语言代码就最好了。谢谢
经过测试,LMX2572的自动锁定测试发现,最长的锁定时间在520us左右,而较短在15us左右,相差甚大,请教下怎么将LMX2572的锁定时间能否稳定的固定下来,或者通过手动锁相模式操作;
1、如何让锁定的时间能够控制在50us左右或者以内?
2、如果自动锁相模式达不到这个指标,能否通过手动锁相模式操作,手动锁相模式如何操作,请将步骤给详细描述下(手册里面没有这块描述);
你好,我们使用的是LMX2572,当配置为1.5G时,频偏很小,只有10几K,但当配置为1.6G时,测得的频率为1.594GHz,偏差了有6M多,
使用的参考时钟是38.4MHz,麻烦帮分析下频偏这么大的原因?配置如下,多谢:
R125 0x7D2288
R124 0x7C0000
R123 0x7B0000
R122 0x7A0000
R121 0x790000
R120 0x780000
R119 0x770000
R118 0x760000
R117 0x7500…
HI,
我再在使用LMK2572 时,遇到一个问题,输出有很多谐波信号,在我们的应用中,使用38.4M 单端时钟信号输入,输出124.8M时钟,用TICS Pro 软件生成的配置 导入到LMK2572中, 出来的信号除了124.8M时钟,还有其他很多频点的时钟,如下图:
以下是配置:
ADDR DATA
R125 0x2288
R124 0x0000
R123 0x0000
R122 0x0000
R121 0x0000
R120 0x0000
R119 0x0…